summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'rootdir/init.rc')
-rw-r--r--rootdir/init.rc5
1 files changed, 4 insertions, 1 deletions
diff --git a/rootdir/init.rc b/rootdir/init.rc
index 424dbee75..901d06636 100644
--- a/rootdir/init.rc
+++ b/rootdir/init.rc
@@ -321,7 +321,6 @@ on post-fs
321 # Make sure /sys/kernel/debug (if present) is labeled properly 321 # Make sure /sys/kernel/debug (if present) is labeled properly
322 # Note that tracefs may be mounted under debug, so we need to cross filesystems 322 # Note that tracefs may be mounted under debug, so we need to cross filesystems
323 restorecon --recursive --cross-filesystems /sys/kernel/debug 323 restorecon --recursive --cross-filesystems /sys/kernel/debug
324 chmod 0755 /sys/kernel/debug/tracing
325 324
326 # We chown/chmod /cache again so because mount is run as root + defaults 325 # We chown/chmod /cache again so because mount is run as root + defaults
327 chown system cache /cache 326 chown system cache /cache
@@ -359,6 +358,10 @@ on post-fs
359 mkdir /cache/lost+found 0770 root root 358 mkdir /cache/lost+found 0770 root root
360 359
361on late-fs 360on late-fs
361 # Ensure that tracefs has the correct permissions.
362 # This does not work correctly if it is called in post-fs.
363 chmod 0755 /sys/kernel/debug/tracing
364
362 # HALs required before storage encryption can get unlocked (FBE/FDE) 365 # HALs required before storage encryption can get unlocked (FBE/FDE)
363 class_start early_hal 366 class_start early_hal
364 367