diff options
Diffstat (limited to 'storaged')
-rw-r--r-- | storaged/EventLogTags.logtags | 4 | ||||
-rw-r--r-- | storaged/include/storaged.h | 2 | ||||
-rw-r--r-- | storaged/include/storaged_uid_monitor.h | 6 | ||||
-rw-r--r-- | storaged/storaged_service.cpp | 8 | ||||
-rw-r--r-- | storaged/storaged_uid_monitor.cpp | 31 |
5 files changed, 25 insertions, 26 deletions
diff --git a/storaged/EventLogTags.logtags b/storaged/EventLogTags.logtags index 71fda25e5..2e25d4a29 100644 --- a/storaged/EventLogTags.logtags +++ b/storaged/EventLogTags.logtags | |||
@@ -36,6 +36,4 @@ | |||
36 | 36 | ||
37 | 2732 storaged_disk_stats (type|3),(start_time|2|3),(end_time|2|3),(read_ios|2|1),(read_merges|2|1),(read_sectors|2|1),(read_ticks|2|3),(write_ios|2|1),(write_merges|2|1),(write_sectors|2|1),(write_ticks|2|3),(o_in_flight|2|1),(io_ticks|2|3),(io_in_queue|2|1) | 37 | 2732 storaged_disk_stats (type|3),(start_time|2|3),(end_time|2|3),(read_ios|2|1),(read_merges|2|1),(read_sectors|2|1),(read_ticks|2|3),(write_ios|2|1),(write_merges|2|1),(write_sectors|2|1),(write_ticks|2|3),(o_in_flight|2|1),(io_ticks|2|3),(io_in_queue|2|1) |
38 | 38 | ||
39 | 2733 storaged_emmc_info (mmc_ver|3),(eol|1),(lifetime_a|1),(lifetime_b|1) | 39 | 2733 storaged_emmc_info (mmc_ver|3),(eol|1),(lifetime_a|1),(lifetime_b|1) \ No newline at end of file |
40 | |||
41 | 2734 storaged_uid_io_alert (name|3),(read|2),(write|2),(interval|2) \ No newline at end of file | ||
diff --git a/storaged/include/storaged.h b/storaged/include/storaged.h index c6cdd81c7..41bdf9744 100644 --- a/storaged/include/storaged.h +++ b/storaged/include/storaged.h | |||
@@ -250,7 +250,7 @@ public: | |||
250 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_UNIT ( 60 ) | 250 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_UNIT ( 60 ) |
251 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_DISK_STATS_PUBLISH ( 3600 ) | 251 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_DISK_STATS_PUBLISH ( 3600 ) |
252 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_EMMC_INFO_PUBLISH ( 86400 ) | 252 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_EMMC_INFO_PUBLISH ( 86400 ) |
253 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_UID_IO ( 3600 ) | 253 | #define DEFAULT_PERIODIC_CHORES_INTERVAL_UID_IO ( 86400 ) |
254 | 254 | ||
255 | // UID IO threshold in bytes | 255 | // UID IO threshold in bytes |
256 | #define DEFAULT_PERIODIC_CHORES_UID_IO_THRESHOLD ( 1024 * 1024 * 1024ULL ) | 256 | #define DEFAULT_PERIODIC_CHORES_UID_IO_THRESHOLD ( 1024 * 1024 * 1024ULL ) |
diff --git a/storaged/include/storaged_uid_monitor.h b/storaged/include/storaged_uid_monitor.h index fffed6f19..9101767e5 100644 --- a/storaged/include/storaged_uid_monitor.h +++ b/storaged/include/storaged_uid_monitor.h | |||
@@ -44,8 +44,10 @@ struct uid_info { | |||
44 | 44 | ||
45 | struct uid_event { | 45 | struct uid_event { |
46 | std::string name; | 46 | std::string name; |
47 | uint64_t read_bytes; | 47 | uint64_t fg_read_bytes; |
48 | uint64_t write_bytes; | 48 | uint64_t fg_write_bytes; |
49 | uint64_t bg_read_bytes; | ||
50 | uint64_t bg_write_bytes; | ||
49 | uint64_t interval; | 51 | uint64_t interval; |
50 | }; | 52 | }; |
51 | 53 | ||
diff --git a/storaged/storaged_service.cpp b/storaged/storaged_service.cpp index 2799c3933..86a2b219b 100644 --- a/storaged/storaged_service.cpp +++ b/storaged/storaged_service.cpp | |||
@@ -90,9 +90,11 @@ status_t Storaged::dump(int fd, const Vector<String16>& /* args */) { | |||
90 | 90 | ||
91 | const std::vector<struct uid_event>& events = storaged.get_uid_events(); | 91 | const std::vector<struct uid_event>& events = storaged.get_uid_events(); |
92 | for (const auto& event : events) { | 92 | for (const auto& event : events) { |
93 | dprintf(fd, "%s %llu %llu %llu\n", event.name.c_str(), | 93 | dprintf(fd, "%s %llu %llu %llu %llu %llu\n", event.name.c_str(), |
94 | (unsigned long long)event.read_bytes, | 94 | (unsigned long long)event.fg_read_bytes, |
95 | (unsigned long long)event.write_bytes, | 95 | (unsigned long long)event.fg_write_bytes, |
96 | (unsigned long long)event.bg_read_bytes, | ||
97 | (unsigned long long)event.bg_write_bytes, | ||
96 | (unsigned long long)event.interval); | 98 | (unsigned long long)event.interval); |
97 | } | 99 | } |
98 | return NO_ERROR; | 100 | return NO_ERROR; |
diff --git a/storaged/storaged_uid_monitor.cpp b/storaged/storaged_uid_monitor.cpp index fd30f5f5b..5f664e4e2 100644 --- a/storaged/storaged_uid_monitor.cpp +++ b/storaged/storaged_uid_monitor.cpp | |||
@@ -145,23 +145,20 @@ void uid_monitor::report() | |||
145 | 145 | ||
146 | for (const auto& it : uids) { | 146 | for (const auto& it : uids) { |
147 | const struct uid_info& uid = it.second; | 147 | const struct uid_info& uid = it.second; |
148 | uint64_t bg_read_delta = uid.io[UID_BACKGROUND].read_bytes - | 148 | struct uid_event event; |
149 | last_uids[uid.uid].io[UID_BACKGROUND].read_bytes; | 149 | |
150 | uint64_t bg_write_delta = uid.io[UID_BACKGROUND].write_bytes - | 150 | event.name = uid.name; |
151 | last_uids[uid.uid].io[UID_BACKGROUND].write_bytes; | 151 | event.fg_read_bytes = uid.io[UID_FOREGROUND].read_bytes - |
152 | 152 | last_uids[uid.uid].io[UID_FOREGROUND].read_bytes;; | |
153 | if (bg_read_delta + bg_write_delta >= adjusted_threshold) { | 153 | event.fg_write_bytes = uid.io[UID_FOREGROUND].write_bytes - |
154 | struct uid_event event; | 154 | last_uids[uid.uid].io[UID_FOREGROUND].write_bytes;; |
155 | event.name = uid.name; | 155 | event.bg_read_bytes = uid.io[UID_BACKGROUND].read_bytes - |
156 | event.read_bytes = bg_read_delta; | 156 | last_uids[uid.uid].io[UID_BACKGROUND].read_bytes;; |
157 | event.write_bytes = bg_write_delta; | 157 | event.bg_write_bytes = uid.io[UID_BACKGROUND].write_bytes - |
158 | event.interval = uint64_t(ts_delta / NS_PER_SEC); | 158 | last_uids[uid.uid].io[UID_BACKGROUND].write_bytes;; |
159 | add_event(event); | 159 | event.interval = uint64_t(ts_delta / NS_PER_SEC); |
160 | 160 | ||
161 | android_log_event_list(EVENTLOGTAG_UID_IO_ALERT) | 161 | add_event(event); |
162 | << uid.name << bg_read_delta << bg_write_delta | ||
163 | << uint64_t(ts_delta / NS_PER_SEC) << LOG_ID_EVENTS; | ||
164 | } | ||
165 | } | 162 | } |
166 | 163 | ||
167 | set_last_uids(std::move(uids), curr_ts); | 164 | set_last_uids(std::move(uids), curr_ts); |