summaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* disable console in user buildsandroid-2.3_r1android-2.3.2_r1android-2.3.1_r1Brian Swetland2010-10-271-2/+8
* add rules to set perms for input device sysfs attributesBrian Swetland2010-10-261-0/+5
* init: support owner/permission setting for sysfs attributes of devicesBrian Swetland2010-10-264-33/+62
* add sdcard access permission to ril daemonBrian Swetland2010-10-231-1/+1
* adb: Add support for Philips's USB vendor IDMike Lockwood2010-10-151-0/+3
* Merge "Add AID_NFC for use by the NFC service." into gingerbreadNick Pelly2010-10-151-0/+2
|\
| * Add AID_NFC for use by the NFC service.Nick Pelly2010-10-151-0/+2
* | Add Asus USB vendor ID to adb.Xavier Ducrohet2010-10-151-0/+3
* | Set PROT_EXEC on the whole pixelflinger code cache.Jean-Baptiste Queru2010-10-141-1/+1
|/
* Merge "Define HAVE_STAT_ST_MTIM and disable it under MinGW/Cygwin." into ging...Raphael Moll2010-10-147-0/+69
|\
| * Define HAVE_STAT_ST_MTIM and disable it under MinGW/Cygwin.Raphael Moll2010-10-137-0/+69
* | Fix KT Tech's usb vendor ID.Xavier Ducrohet2010-10-141-1/+1
|/
* Print out the signal code along with signal number and address.Carl Shapiro2010-10-081-2/+48
* Add HAVE_PREAD definition to platformsKenny Root2010-10-047-0/+35
* init: Add support for SOCK_SEQPACKET socket typeMike Lockwood2010-10-013-6/+8
* netstat should include /proc/net/tcp6 and /proc/net/udp6 dataBrian Carlstrom2010-09-292-50/+84
* Qualify the source argument of atomic loads as a const pointer.Carl Shapiro2010-09-284-14/+22
* Add new USB vendor IDs.Xavier Ducrohet2010-09-281-0/+6
* Add AID_GPS user ID for GPS daemonMike Lockwood2010-09-271-0/+2
* Make netd restart when system server hangs on it.Brad Fitzpatrick2010-09-211-0/+1
* add /vendor supportBrian Swetland2010-09-193-11/+26
* add graphics events to the eventlog definitionsMathias Agopian2010-09-141-0/+18
* Merge "Fetch peer credentials for local sockets" into gingerbreadKenny Root2010-09-142-2/+31
|\
| * Fetch peer credentials for local socketsKenny Root2010-09-142-2/+31
* | Add dvm_lock_sample's new fields.Brad Fitzpatrick2010-09-141-1/+1
|/
* Merge "Add missing lock in SocketListener." into gingerbreadBrad Fitzpatrick2010-09-141-0/+1
|\
| * Add missing lock in SocketListener.Brad Fitzpatrick2010-09-141-0/+1
* | Return false on socket read errorKenny Root2010-09-141-1/+1
|/
* make df more readableBrian Swetland2010-09-111-8/+24
* Merge "remount / as read-only only on post-fs to allow per-target config of /...Brian Swetland2010-09-081-2/+3
|\
| * remount / as read-only only on post-fs to allow per-target config of /Brian Swetland2010-09-081-2/+3
* | Use makedev helper for device major and minor numbersColin Cross2010-09-031-4/+1
* | It seems that Windows actually does have a header for <stdbool.h>.Dan Bornstein2010-09-011-1/+1
* | Merge "get rid of compile time warning: "warning: ‘android_ids’ defined b...Nick Kralevich2010-08-311-1/+1
|\ \
| * | get rid of compile time warning: "warning: ‘android_ids’ defined but not ...Nick Kralevich2010-08-311-1/+1
* | | am 2ad6067c: (-s ours) do not merge: cherry-picked 44db990d3a4ce0edbdd16fa7ac...Nick Kralevich2010-08-300-0/+0
|\ \ \ | |/ / |/| |
| * | do not merge: cherry-picked 44db990d3a4ce0edbdd16fa7ac20693ef601b723 from mas...Nick Kralevich2010-08-301-4/+12
* | | Fix bug 2950316. Check return values.Nick Kralevich2010-08-271-4/+12
* | | Fix the pagesize argument parsingMaarten Hooft2010-08-241-2/+2
* | | Fix usage string.Ying Wang2010-08-231-0/+1
* | | Including dl heap stubs for the dalvikvm host buildJesse Wilson2010-08-181-1/+1
* | | Fix a long standing bug in the output buffer size computation.Carl Shapiro2010-08-171-1/+1
* | | sdcard: Implement statfs, stat time values and change mount point to /mnt/sdcardMike Lockwood2010-08-161-5/+36
| |/ |/|
* | fix up permissionsBrian Swetland2010-08-121-3/+15
* | sdcard: a program to create a "virtual" /sdcard pointed at a pathBrian Swetland2010-08-123-0/+1340
* | handle 4096 byte pages if requested via --pagesizeBrian Swetland2010-08-111-1/+7
* | Tracking merge of dalvik-dev to gingerbreadBrian Carlstrom2010-08-043-1/+18
* | Merge "Add basic lsof command" into gingerbreadKenny Root2010-07-272-1/+225
|\ \
| * | Add basic lsof commandKenny Root2010-07-272-1/+225
* | | Correct copyright header for uptime and NOTICEKenny Root2010-07-272-12/+89
|/ /