| Commit message (Collapse) | Author | Age | Files | Lines |
|\ |
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
The backtrace offline code uses these error codes to diagnose errors.
In addtion, I've had cases where seeing these errors would help diagnose
failures.
This also allows us to add a few features to indicate why an unwind
terminated (such as max frames exceeded).
Bug: 65682279
Test: Updated unit tests pass.
Change-Id: If82b5092698e8a194016d670efff1320f9b44d50
|
|\ \ |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
The library isn't intented to be exposed to vendors. It is a platform
private library.
Bug: 72471487
Test: Pixel 2016/2017 boots to the UI. Photo editing works.
Change-Id: Ib0479a43d66d988c2f882688240746bed3213dad
|
|\ \ \ |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This CL will enable reading /product/build.prop and add product paths
into ld.config.txt.in.
Bug: 64195575
Test: tested with 'PRODUCT_PRODUCT_PROPERTIES := ro.product.abc=abc' on
sailfish
Change-Id: Ie996def20e25dc1afe0c74af2096af844934b2dc
|
|\ \ \ \
| |_|_|/
|/| | | |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Bug: N/A
Test: N/A
Change-Id: I91c07531ba8a2da0187b7411b9c11dc3191dcede
|
|\ \ \ \
| |_|/ /
|/| | | |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
- Be a little more lenient when reading the cies/fdes. If next entry data
winds up incorrect, don't fail, simply stop processing the entries. This
only applies when reading all of the cies/fdes at once.
- Fail to init an eh_frame with no entries and fallback to assuming the
eh_frame has no header instead.
- Change the step to always try debug_frame first which has the most
accurate information.
- Add small unit tests and a couple of offline unit tests to verify
this behavior.
These changes are needed to support offline unwinding since it depends
on this new behavior.
Bug: 65682279
Test: Ran new unit tests.
Change-Id: I3529f1b0c8e14cd7409494e5de2f3c9e78d0855e
|
|\ \ \ \
| |/ / /
|/| | | |
|
| |/ /
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
This way, we don't fault in the entirety of our DSOs immediately;
instead, used pages are "sticky" in memory. Works only on kernel 4.4
and up: downlevel, we ignore the mlockall failure.
Once we get statically-linked lmkd in better shape, we'll just switch
to that.
Change-Id: I07a75ee3bc1264a1db41635c2acf611fede99b91
|
|\ \ \ |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Use the art dex file library to read the dex data.
Add unit tests for the UnwindDexFile code.
Bug: 72070049
Test: All unit tests continue to pass.
Test: Dumped the backtrace of the 137-cfi test while running in interpreter
Test: mode and verified that the stack trace is correct. Did this on host
Test: and for arm/arm64.
Change-Id: Ia6f343318c5dd6968a954015a7d59fdf101575b0
|
|\ \ \ \
| |_|/ /
|/| | | |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
auditd : type=1400 audit(0.0:9): avc: denied { dac_override } for comm="usbd" capability=1 scontext=u:r:usbd:s0 tcontext=u:r:usbd:s0 tclass=capability permissive=
auditd : type=1400 audit(0.0:9): avc: denied { dac_override } for comm="usbd" capability=1 scontext=u:r:usbd:s0 tcontext=u:r:usbd:s0 tclass=capability permissive=0
Bug: 72397740
Test: booted the device to make sure that the denials are no longer
seen.
Change-Id: Ie276103ba261fd762fb8c24234904e3f3ce3d2f1
|
|\ \ \ \
| |/ / /
|/| | | |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
vendor_init doesn't have permissions to read rootfs labeled files, but
needs to read /vendor_file_contexts to do restorecon correctly. This
file is a file_contexts file, so labeling it as such seems appropriate.
Test: bullhead + vendor_init doesn't hit this audit
Change-Id: I475e9735616c2426b9c7073700272f878ced2135
|
|\ \ \ \
| |/ / /
|/| | | |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
32-bit devices still exist...
Bug: http://b/72335947
Test: builds
Change-Id: Ia644640f19ad9d9160554e3fe329b3ce8e585c66
|
|\ \ \ \
| |_|/ /
|/| | | |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Finishing a TODO from vendor_init, check SELinux permissions before
setting properties in vendor_init.
Bug: 62875318
Test: N/A
Change-Id: I3cb6abadd2613ae083705cc6b9c970587b6c6b19
|
|\ \ \ \ |
|
| | |_|/
| |/| |
| | | |
| | | |
| | | | |
Test: No crash when a jit debug object is not instantiated.
Change-Id: Ic4350a10258459ead7c5679ceb84372f1084f0ad
|
|\ \ \ \ |
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
usbd checks whether adb is enabled by default, if yes,
would start adbd and would call into usb hal to configure
usb gadget stack.
Bug: 63669128
Test: Verify that adb gets configured when enabled
Change-Id: If6d06cdadd6d93f181d56619142cbbb04d39a5cd
|
|\ \ \ \ \ |
|
| | |/ / /
| |/| | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
This commit moves /{odm,vendor}/lib[64]/vndk[-sp] to vndk namespace so
that vndk extension can override vndk libs from
/system/lib[64]/vndk[-sp].
Bug: 69824336
Test: Create libutils_ext locally and it can be called from
android.hardware.nfc@1.0-service.
Change-Id: Id63e58d665fa41eda85950ee1d16fe06c35cd7d3
|
|\ \ \ \ \
| |_|_|_|/
|/| | | | |
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
This CL implements a simple force_suspend(). This function takes a
timeoutMs argument that is currently ignored. It also uses a two-stage
init process that spawns the suspend_thread when autosuspend is in use.
Follow-up CLs will:
- Implement file locking to prevent multiple libsuspend instances from
starting multiple suspend threads in the system.
- Fully implement timout for force_suspend.
- Integrate force_suspend with suspend_thred.
Bug: 70669809
Test: autosuspend still works
Change-Id: I6b2c72d0c61d1bec6db0f0b28481ffe0e20ec615
|
|\ \ \ \ \
| |_|_|_|/
|/| | | | |
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
These are halified. Instead launch blank_screen which
does the same task w/o init itself having binder
dependencies.
Bug: 70846424
Test: manual + reboot appears similar
Change-Id: If8b2a56cbc31077122ea81406721b06034e4498f
|
|\ \ \ \ \
| |_|_|/ /
|/| | | | |
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
I'd be not doing this for a while since some of this code doesn't
compile on host and libinit previously did. But after realizing
the property_service.cpp (libinit) references symbols in init.cpp
(init) and seeing a new linker error crop up due to that, it's time to
make the fix.
My only hold out previously was that libinit compiled on host bionic
and some of init (builtins.cpp, etc) do not, however given that we
don't actually have host bionic support or host bionic init tests,
that isn't a good reason. We can and should mock out the libraries
that aren't available with host bionic when ready.
Test: build, unit tests, boot
Change-Id: Ie49362ddb637924efc272540a4f32b693643fcdc
|
|\ \ \ \ \ |
|
|/ / / / /
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
The stack dump was not printing leading zeros for data after the
change to remove uintptr_t types from the libbacktrace API.
Bug: 65682279
Test: Created an arm tombstone and an arm64 tombstone and verified
Test: that the stack data has leading zeros.
Change-Id: I1fbec2c4fa7c8b0fab18894c5628d18c5a580299
|
|\ \ \ \ \ |
|
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | | |
Bug: http://b/38508369
Test: debuggerd_test32/64 on walleye and aosp_x86_64
Change-Id: I7e69e37bcd1823d271b9f2b0a13b8c9cba9a8e84
|
|\ \ \ \ \ \ |
|
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | | |
Traceur app is being split out of shell user. Previously it logged to
shell's bugreports directory. It no longer has access, so it needs a
new, user-friendly file location to store trace data.
Bug:68126425
Test: Traceur can write and shell can read from this directory
Change-Id: I9e344973fd43eb5699f7a848524e20b06458fb77
|
|\ \ \ \ \ \ \ |
|
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | | |
In order to support the offline unwinding properly, get rid of the
usage of non-fixed type uintptr_t from all API calls.
In addition, completely remove the old local and remote unwinding code
that used libunwind.
The next step will be to move the offline unwinding to the new unwinder.
Bug: 65682279
Test: Ran unit tests for libbacktrace/debuggerd.
Test: Ran debuggerd -b on a few arm and arm64 processes.
Test: Ran crasher and crasher64 and verified tombstones look correct.
Change-Id: Ib0c6cee3ad6785a102b74908a3d8e5e93e5c6b33
|
|\ \ \ \ \ \ \ \ |
|
| | | | | | | | |
| | | | | | | | |
| | | | | | | | |
| | | | | | | | |
| | | | | | | | |
| | | | | | | | | |
Bug: http://b/68664649
Test: echo 'ANDROID!' > fake.img ; fastboot -c `python -c "print 'A'*4000"` boot fake.img
Change-Id: I3299e0fba24a6c1f6178c994731a94cea68f7254
|
|\ \ \ \ \ \ \ \ \
| |_|_|_|_|/ / / /
|/| | | | | | | | |
|
|/ / / / / / / /
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | |
| | | | | | | | |
Revert "Remove obsolete workaround."
This reverts commit 1f3ac7583feaf591ee23fcc69d56d29613020b4f.
Bug: 72143978
Bug: 24465209
Test: Tested failing case on sailfish, reverted back all CL's since
Test: 3471433 for b/24465209 and apps open
|
|\ \ \ \ \ \ \ \
| |_|_|_|_|/ / /
|/| | | | | | | |
|
| | |/ / / / /
| |/| | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | |
| | | | | | | |
Prevent future cyclic dependency from libunwind changes.
Bug: 66919073
Test: make -j 50
Change-Id: I2a4fa5b7c2c3a82db2073d0fa51940da6603be1f
|
|\ \ \ \ \ \ \
| |/ / / / / /
|/| | | | | | |
|
|/ / / / / /
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | | |
Changes:
- Change the register type from int16_t to uint32_t for the location data
and the Eval processing. This is because the special dex pc is > 65535.
- Add the ability for Dwarf register location information to point to a
register that is itself a Dwarf location register.
- Add dex_pc to the frame information.
- Modify the unwind tool to print the dex pc if non-zero.
This does not implement the printing of the dex information in anything
but the unwind tool. It's not the final form of this printing.
Bug: 72070049
Test: Ran new unit tests.
Test: Dumped stack while in interpreter running 137-cfi art test and
Test: verified dex pc is set to non-zero.
Change-Id: I6ce8a6b577fb4f92abacbd433b1f68977e272542
|