| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
| |
Realloc can return null pointer which
will cause a crash then. Patch introduces
check for controlled 'die' in case memory is
not available
Change-Id: I279028339b1fe756d8a511834e164e59d4cab110
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
CL in [1] fixed the wrong mode for the root directory from 0644 to 0755.
However it only handles the path by calling mkbootfs with canned
fs_config (i.e. with -f flag). When calling mkbootfs without -f flag, it
still treats the root directory as a file. This renders the generated
boot/recovery images w/ and w/o -f being different, and leads to the
incorrect checksums in /system/bin/install-recovery.sh.
[1] commit aa8f2f65a030f71506277e2a8d64d83a099e9feb.
Bug: 31988535
Test: `make dist` and verify the checksums in /system/bin/install-recovery.sh.
Change-Id: Ib50fadb23367da0b46944ae0579093da21412593
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Using a getenv('OUT') in such a deep down function is a wrong design
choice. Replacing with explicit parameter that may be NULL in case
device specific files can be accessed from /.
Since TARGET_COPY_OUT_SYSTEM may be defined to something different than
system we also ensure that we use a path relative to TARGET_OUT to
compute path to fs_config_* files.
Bug: 21989305
Bug: 22048934
Change-Id: Id91bc183b29beac7379d1117ad83bd3346e6897b
Signed-off-by: Thierry Strudel <tstrudel@google.com>
|
|
|
|
|
|
|
|
|
|
|
| |
- move to libcutils.so as shared now that they are
in DISTTOOL.
- liblog dependency is part of libcutils, and need not be
called out explicitly now. liblog is in DISTTOOL.
- libcutils fs_config has the right to add Android logging
Bug: 19908228
Change-Id: I915503f64389b59075620578601f98fc0756bd7a
|
|
|
|
|
|
| |
Bug: 19908228
Change-Id: Ic843b32f575825dc89cd9fa15dc0619bc397ce82
|
|
|
|
|
|
|
| |
- Solve st_mode is uint16_t on MAC
- Turn on -Werror
Change-Id: I67b62424245545099ed283c56dae544153b85425
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Missing frees in:
adb/file_sync_client.c
fastboot/fastboot.c
libsparse/output_file.c
Missing closedirs in:
adb/file_sync_service.c
cpio/mkbootfs.c
libcutils/dir_hash.c
Potential buffer overrun in:
gpttool/gpttool.c
Incorrect NULL check in:
libsparse/backed_block.c
Bug: https://code.google.com/p/android/issues/detail?id=61564
Change-Id: If97838a9e73a77aef7f416c31c237ce1fca4ce21
|
|
|
|
|
|
|
|
| |
Modify android_filesystem_config.h and add a capabilities
field. This field can be used to add filesystem capabilities
to a particular file.
Change-Id: If8953a322457ea7275aa6df75660b714e6dc678a
|
|
|
|
| |
Change-Id: I1b841bde6de6c8e762c5fba35e6d6d701f18bb05
|
|
|
|
|
|
|
|
|
|
|
| |
mkbootfs uses the compiled in fs_config() function to set the mode
(but not the uid or gid) of the files in the filesystem it is
building. Give it an optional "-f filename" flag to allow loading the
list of file permissions from a file, so we can continue to accurately
recreate old filesystems even when the current fs_config() has changed.
Bug: 6435132
Change-Id: Ife6b25e989301e78e22c34a544738436c96caf6f
|
|
|
|
| |
Change-Id: I665572a2212f1239b02b7816e37ada210afbdb48
|
| |
|
| |
|
| |
|
| |
|
|
|