summaryrefslogtreecommitdiffstats
path: root/fs_mgr
Commit message (Expand)AuthorAgeFilesLines
* Merge "fs_mgr: don't log error messages when missing fstab"Christopher Morin2018-01-081-5/+8
|\
| * fs_mgr: don't log error messages when missing fstabChris Morin2018-01-051-5/+8
* | Merge changes from topic "resgidz"Jeff Sharkey2018-01-081-5/+7
|\ \ | |/ |/|
| * Set reserved GID when setting reserved blocks.Jeff Sharkey2018-01-071-5/+7
* | fs_mgr: fix memory leakChris Morin2018-01-041-3/+4
|/
* Merge "first stage mount: support mount points like /vendor/abc"Treehugger Robot2017-12-142-16/+37
|\
| * first stage mount: support mount points like /vendor/abcBowgo Tsai2017-12-132-16/+37
* | Merge changes from topic "sload_f2fs"Jaegeuk Kim2017-12-071-8/+36
|\ \
| * | fs_mgr: format f2fs with length=xx fstabJaegeuk Kim2017-12-071-8/+36
| |/
* | Merge "Add OWNERS."Elliott Hughes2017-12-071-0/+2
|\ \ | |/ |/|
| * Add OWNERS.Elliott Hughes2017-12-071-0/+2
* | Merge "Remove dead code."Elliott Hughes2017-12-062-155/+0
|\ \
| * | Remove dead code.Elliott Hughes2017-12-062-155/+0
| |/
| * Merge "DO NOT MERGE ANYWHERE Add comments and code about ro.boot.slot back"Treehugger Robot2017-11-131-3/+10
| |\
| | * DO NOT MERGE ANYWHERE Add comments and code about ro.boot.slot backSandeep Patil2017-11-101-3/+10
* | | Merge commit 'a63ccea6abc7ea02e2d98e41c80793ca97237bd3' fromXin Li2017-11-141-5/+3
|\ \ \ | |/ / |/| |
| * | Merge "fs_mgr: removing is_device_secure()" am: af54c27e1b am: 6353d514e8Bowgo Tsai2017-10-144-22/+3
| |\ \
| * \ \ Merge "Move some properties users to __system_property_read_callback()" am: 4...Tom Cherry2017-10-122-26/+16
| |\ \ \
| * \ \ \ Merge "fs_mgr: removing __BEGIN_DECLS and __END_DECLS" am: 85b80dc18d am: a4b...Bowgo Tsai2017-10-102-17/+1
| |\ \ \ \
| * \ \ \ \ Merge "fs_mgr_fstab: removing fs_mgr_get_entry_for_mount_point_after()" am: 1...Bowgo Tsai2017-09-292-31/+5
| |\ \ \ \ \
| * \ \ \ \ \ Merge "fs_mgr_fstab: do an exact match when searching a mount point" am: a0dd...Bowgo Tsai2017-09-261-7/+8
| |\ \ \ \ \ \
| * \ \ \ \ \ \ Merge "Reland "Remove comments and code about ro.boot.slot"" am: dea5e081ac a...Tom Cherry2017-09-251-10/+3
| |\ \ \ \ \ \ \
| * \ \ \ \ \ \ \ Merge "Revert "Remove comments and code about ro.boot.slot"" am: eb00b1f3aa a...Tom Cherry2017-09-211-3/+10
| |\ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ Merge "Remove comments and code about ro.boot.slot" am: 7dcf076700 am: bf6168...Tom Cherry2017-09-201-10/+3
| |\ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ Merge "Allow the use of a custom Android DT directory" am: 6fa0884188 am: 8b2...Bo Hu2017-07-294-17/+48
| |\ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ Merge "Remove LOCAL_CLANG and clang: true" am: 80ec81cf4b am: f7b315c985 am: ...Lennart Wieboldt2017-07-251-1/+0
| |\ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr:Add filter condition to make sure that the super block is corre...Keun-young Park2017-07-211-3/+9
| |\ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr_verity: allow verification error when the device is unlocked" a...Bowgo Tsai2017-07-191-1/+7
| |\ \ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ \ Merge changes from topic 'ext4_encryption_flag' am: 5be05733c2 am: 5a6226929e...Tom Cherry2017-07-143-211/+210
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr: trim the terminating '\0' when reading from device tree" am: b...Bowgo Tsai2017-07-141-2/+6
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr: Adding logs when failing to wait for a device file" am: 4ca2a3...Jinguang Dong2017-07-055-54/+39
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr: allow no verity metadata when the device is unlocked." am: cd0...Bowgo Tsai2017-07-054-13/+14
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr: report errno string for __mount errors" am: 6333cd0938 am: eef...Mark Salyzyn2017-07-051-2/+3
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ Merge "fs_mgr: add libfstab for vendor"TreeHugger Robot2017-06-273-89/+134
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| | * | | | | | | | | | | | | | | | | | | fs_mgr: add libfstab for vendorJiyong Park2017-06-273-89/+134
| * | | | | | | | | | | | | | | | | | | | Merge changes Ibe1feb39,I05be83e4,If1422e4d am: a4f086ab20 am: 3a156e6c2b am:...Mark Salyzyn2017-06-271-1/+4
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ | | |/ / / / / / / / / / / / / / / / / / / | |/| | | | | | | | | | | | | | | | | | |
| * | | | | | | | | | | | | | | | | | | | Merge "AVB: allow no metadata in the generic system.img for project Treble" a...Bowgo Tsai2017-06-234-65/+114
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * | | | | | | | | | | | | | | | | | | | | fs_mgr: properly propagate exec child errorsBen Fennema2017-06-221-5/+3
| * | | | | | | | | | | | | | | | | | | | | Merge changes from topic 'eng_first_stage_mount' am: b7e2f272ee am: e5341cf56...Sandeep Patil2017-06-213-3/+8
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * | | | | | | | | | | | | | | | | | | | | | fs_mgr: replace make_ext4 api with e2fsprogsJin Qian2017-06-203-63/+35
* | | | | | | | | | | | | | | | | | | | | | | first stage mount: abort when failed to parse fstab in device-treeBowgo Tsai2017-11-091-1/+1
| |_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|/ |/| | | | | | | | | | | | | | | | | | | | |
* | | | | | | | | | | | | | | | | | | | | | Merge "fs_mgr: support reading fstab based on ro.boot.hardware.platform"Treehugger Robot2017-11-011-11/+30
|\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| * | | | | | | | | | | | | | | | | | | | | | fs_mgr: support reading fstab based on ro.boot.hardware.platformOleg Matcovschi2017-11-011-11/+30
| | |_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|/ | |/| | | | | | | | | | | | | | | | | | | |
* / | | | | | | | | | | | | | | | | | | | | Use -Werror in system/coreChih-Hung Hsieh2017-11-011-1/+5
|/ / / / / / / / / / / / / / / / / / / / /
* | | | | | | | | | | | | | | | | | | | | Merge "fs_mgr: removing is_device_secure()"Bowgo Tsai2017-10-144-22/+3
|\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ | |_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|/ |/| | | | | | | | | | | | | | | | | | | |
| * | | | | | | | | | | | | | | | | | | | fs_mgr: removing is_device_secure()Bowgo Tsai2017-10-124-22/+3
* | | | | | | | | | | | | | | | | | | | | Merge "Move some properties users to __system_property_read_callback()"Tom Cherry2017-10-122-26/+16
|\| | | | | | | | | | | | | | | | | | | | | |_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|/ |/| | | | | | | | | | | | | | | | | | |
| * | | | | | | | | | | | | | | | | | | Merge "Move some properties users to __system_property_read_callback()"Tom Cherry2017-10-122-26/+16
| |\ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \ \
| | * | | | | | | | | | | | | | | | | | | Move some properties users to __system_property_read_callback()Tom Cherry2017-10-102-26/+16
* | | | | | | | | | | | | | | | | | | | | Merge "fs_mgr: removing __BEGIN_DECLS and __END_DECLS"Bowgo Tsai2017-10-102-17/+1
|\| | | | | | | | | | | | | | | | | | | | | |_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|_|/ |/| | | | | | | | | | | | | | | | | | |