| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Just the minimial changes to get this to actually build, because otherwise
we always bog down trying to rewrite everything (when the real answer
is usually "stop using libcutils, it's awful").
This doesn't move a handful of files: two are basically just BSD libc
source, a couple have outstanding code reviews, and one can be deleted
(but I'll do that in a separate change).
I'm also skipping the presubmit hooks because otherwise clang-format
wants to reformat everything. I'll follow up with that...
Bug: N/A
Test: builds
Change-Id: I06403f465b67c8e493bad466dd76b1151eed5993
|
|
|
|
|
|
|
|
| |
Every little helps...
Bug: N/A
Test: builds
Change-Id: Ibcac5cda1619420c95903211ed0b96af81351f9e
|
|
|
|
|
|
|
|
|
|
|
|
| |
Some of Android componets e.g. init have migrated to use base/logging to get rid
of klog utilities. However, without explicit initilization, the default
klog_level is set to 3 which masks the logwrap output.
This patch sets default klog_level to KLOG_INFO_LEVEL to make
android_fork_execvp_ext log available.
Bug: 34256270
Test: manual
Change-Id: Ibe74707a92c954053cd0e6828a984fbd72b4acae
|
|
|
|
|
|
|
|
|
|
| |
files.[h|cpp] is bound to be abused with junk, replace with
android_get_control_file.[h|cpp]. Plus some sundry cleanup.
Test: gTest libcutils-tests, logd-unit-tests, liblog-unit-tests,
logcat-unit-tests and init_tests
Bug: 32450474
Change-Id: Ibd4a7aa4624ea19a43d1f98a3c71ac37805d36b5
|
|
|
|
|
|
|
|
| |
If the file descriptor is in the environment, use it.
Test: compile
Bug: 32450474
Change-Id: Id208b11b727a44dc861a141130a644d7d8009c5f
|
|
|
|
|
|
|
|
|
|
|
| |
Remove the /dev/__kmsg__ workarounds (which can then be removed
from sepolicy), and fix confusion in the translation between
android-base logging and kernel logging priorities (in particular,
where 'notice' comes in the hierarchy).
Bug: http://b/30317429
Change-Id: I6eaf9919904b6b55bc402c20bf1a4ae269014bc7
Test: adb shell dmesg | grep init
|
|
|
|
| |
Change-Id: I467edad1d004ac16647f4aa1f0eead04e808efa0
|
|
I'll come back and remove klog_init when I've removed other calls to it.
Change-Id: Iad7fd26d853b4ddc54e9abd44516b6f138cbbfcb
Test: booted N9, looked at "adb shell dmesg" output.
|