Commit message (Collapse) | Author | Age | Files | Lines | |
---|---|---|---|---|---|
* | Move libcutils source to C++. | Elliott Hughes | 2017-11-10 | 1 | -1/+2 |
| | | | | | | | | | | | | | | | | | Just the minimial changes to get this to actually build, because otherwise we always bog down trying to rewrite everything (when the real answer is usually "stop using libcutils, it's awful"). This doesn't move a handful of files: two are basically just BSD libc source, a couple have outstanding code reviews, and one can be deleted (but I'll do that in a separate change). I'm also skipping the presubmit hooks because otherwise clang-format wants to reformat everything. I'll follow up with that... Bug: N/A Test: builds Change-Id: I06403f465b67c8e493bad466dd76b1151eed5993 | ||||
* | Redirect qtaguid native call to netd fwmark client | Chenbo Feng | 2017-11-09 | 1 | -0/+125 |
In order to replace qtaguid module with new eBPF network monitoring module. We firstly move the current qtaguid userspace implementation into netd and hide the detail from other processes. The current API will talk to netd fwmark client to pass down the qtaguid related request from high level framework and netd will use the proper method to complete the request. Test: Current TrafficStats CTS tests should not fail. Bug: 30950746 Change-Id: Ie90c28f3594ab2877746b2372a1b6944768bfb18 |
index : android/platform-system-core | ||
Stable Android distribution for TI processors; Supported SoCs: Jacinto (DRA7xx, J721E), Sitara (AM43xx, AM57xx, AM65x) - fork of https://android.googlesource.com/platform/system/core/. | Scott (ITS) Allen |
summaryrefslogtreecommitdiffstats |