summaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* More SOCK_CLOEXECNick Kralevich2015-02-261-1/+1
* Remove loghack.h.Narayan Kamath2015-02-212-121/+1
* Libcutils: Remove unused variableAndreas Gampe2015-02-191-1/+0
* Use mkstemp for host ashmem.Elliott Hughes2015-02-091-43/+7
* android_reboot should take a const char*.Elliott Hughes2015-02-031-1/+1
* Kill HAVE_PTHREADS.Yabin Cui2015-01-271-18/+16
* Move 32 bit/64 bit check into debuggerd.Christopher Ferris2015-01-201-53/+5
* Remove unused cruft from libcutils.Elliott Hughes2015-01-152-83/+0
* Merge "Extend to receive NFLOG packets."Jeff Sharkey2015-01-151-9/+17
|\
| * Extend to receive NFLOG packets.Jeff Sharkey2015-01-151-9/+17
* | Add timed versions of stack dumping functions.Christopher Ferris2015-01-151-3/+29
|/
* Remove HAVE_LIBC_SYSTEM_PROPERTIES and HAVE_SYSTEM_PROPERTY_SERVER.Elliott Hughes2015-01-121-184/+2
* Use getmntent when accessing /proc/mounts.Yabin Cui2015-01-051-24/+9
* Fix references to HAVE_PRCTL.Elliott Hughes2014-12-151-2/+2
* HAVE_ANDROID_OS implies that you have <pthread.h> and <sched.h>.Elliott Hughes2014-12-141-1/+1
* Libcutils: Remove unused variableAndreas Gampe2014-11-241-1/+0
* Kill LOCAL_SOCKET_NAMESPACE.Elliott Hughes2014-11-222-4/+4
* Remove the error-prone TARGET_CPU_SMP from system/core.Elliott Hughes2014-11-171-10/+2
* Disable the static libcutils tests.Dan Albert2014-11-141-15/+17
* Second attempt to "Rewrite atomic.h to use stdatomic.h."Hans Boehm2014-11-131-1/+8
* Revert "Move some tests to libc++."Dan Albert2014-11-111-3/+1
* Move some tests to libc++.Dan Albert2014-11-111-1/+3
* Remove dead code.Elliott Hughes2014-11-081-8/+0
* am 07f1300c: am 7979f1ce: Merge "Do not inline rarely used trace function bod...Chih-Hung Hsieh2014-10-151-0/+57
|\
| * Do not inline rarely used trace function bodies.Chih-Hung Hsieh2014-10-141-0/+57
* | am ad0ff1d9: am 4fceda2b: Merge "Add -no-integrated-as at local level."Chih-Hung Hsieh2014-10-061-0/+3
|\|
| * Add -no-integrated-as at local level.Chih-Hung Hsieh2014-10-061-0/+3
* | am 072877af: am 41198eea: Merge "Revert "Rewrite atomic.h to use stdatomic.h.""Hans Boehm2014-10-031-8/+1
|\|
| * Revert "Rewrite atomic.h to use stdatomic.h."Hans Boehm2014-10-031-8/+1
* | am f5204549: am 028928fe: Merge "Rewrite atomic.h to use stdatomic.h."Hans Boehm2014-10-031-1/+8
|\|
| * Rewrite atomic.h to use stdatomic.h.Hans Boehm2014-10-011-1/+8
* | am be0d295d: am 19d686ee: Merge "Don\'t manually link stlport."Dan Albert2014-09-261-1/+1
|\|
| * Don't manually link stlport.Dan Albert2014-09-261-1/+1
* | am 6c03b85f: am 32e2f1be: Merge "Clean up memset[16,32] routines: unify files...Elliott Hughes2014-09-179-1275/+1209
|\|
| * Clean up memset[16,32] routines: unify files names, remove redundant wrapperVarvara Rainchik2014-09-179-1275/+1209
| * Use the correct debuggerd given the tid.Christopher Ferris2014-09-131-57/+119
* | am 07dda6b5: Merge "Use the correct debuggerd given the tid." into lmp-devChristopher Ferris2014-09-131-57/+119
|\ \
| * | Use the correct debuggerd given the tid.Christopher Ferris2014-09-121-57/+119
| * | Remove invalid 64-bit host objects.Stephen Hines2014-07-251-13/+0
* | | am 522c1d34: am e18ed89e: Merge "Remove makefile cruft."Dan Albert2014-09-121-0/+2
|\ \ \ | | |/ | |/|
| * | Remove makefile cruft.Dan Albert2014-09-121-0/+2
* | | am a66532e7: am 91baad56: Merge "Fix some clang compilation issues."Dan Albert2014-09-111-1/+1
|\| |
| * | Fix some clang compilation issues.Dan Albert2014-09-111-1/+1
* | | am 4592d73e: am a59b6ac6: Merge "Only the Mac doesn\'t have open_memstream."Elliott Hughes2014-08-201-2/+2
|\| |
| * | Only the Mac doesn't have open_memstream.Elliott Hughes2014-08-201-2/+2
* | | am 3859029a: am 7fb0ee0c: Merge "Remove androidGetTid."Elliott Hughes2014-08-181-4/+0
|\| |
| * | Remove androidGetTid.Elliott Hughes2014-08-181-4/+0
* | | am e07a6e63: am 6d9a5ac3: Merge "[MIPSR6] Skip pixelflinger, memset assembler...Elliott Hughes2014-08-051-1/+9
|\| |
| * | [MIPSR6] Skip pixelflinger, memset assembler code on mips32r6Duane Sand2014-07-311-1/+9
* | | am 31dc191b: am 73290cd1: Merge "Remove invalid 64-bit host objects."Stephen Hines2014-07-221-13/+0
|\| | | |/ |/|