| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
| |
Bug: 110127913
Test: boots
Change-Id: I0c1efacfb5ac0407e896ddde0bcc63927edc0525
|
|
|
|
|
|
|
|
|
|
|
|
| |
This change removes the call to prctl(PR_SET_KEEPCAPS, 1), because now
that logd is being run with ambient capabilities, init will set the
KEEP_CAPS / KEEP_CAPS_LOCKED securebits.
Bug: 110127913
Test: liblog-unit-tests, logd-unit-tests, logcat-unit-tests
(on an aosp_sailfish-userdebug)
Change-Id: I72b6a49c5cd1552085f9ad44cb19a7333a13eeea
|
|
|
|
|
|
| |
Bug: N/A
Test: builds
Change-Id: I794cd28667c6c65b38940d8f443315ad116b7ac3
|
|
|
|
|
|
|
|
| |
Prevent a possible DOS of the kernel logs because the runtime result
could differ from the boottime result.
Test: adb bugreport, then examine kernel log
Change-Id: I140fd465f2e691c751d92af50dbdf95e23c121d8
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Refine DAC security surrounding logd.daemon worker thread and add a
positive test for logd failure to access /data/system/packages.list.
- Add AID_PACKAGE_INFO to groups of worker thread.
- Move AID_SYSTEM to groups, setgid to AID_LOGD.
- Do not drop capabilities until after setting the uid and gids.
- Add a test that is part of logd.statistics test to check when
packagelistparser appears broken.
- If /data/system/packages.list is encrypted, ensure we do not pick
up the existing inode to ensure strong positive when finding access
problems.
- Replace all occurrences of NULL with nullptr in gTest code for
compliance with best practices.
Test: gTest logd-unit-tests --gtest_filter=logd.statistics
(expect consistent failure, later CLs fix)
Bug: 37751120
Bug: 36645158
Change-Id: I01b26fe5e25203246ae432d272c8daa9c07cab54
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
(cherry picked from commit c27f12a3d396f113c5ae09d2f2c8ff7de3f8b551)
logd assumes that it is running in UTC time zone.
However, if persist.sys.timezone is set at some point later,
that affects and confuses logd behavior.
To avoid such a case, this CL sets TZ to UTC, which overrides
the property's behavior.
Test: Ran CtsOsTestCases.
Test: gTest liblog-unit-tests, logd-unit-tests and logcat-unit-tests
Bug: 33566779
Change-Id: Ib9edd4cb06f019a33aaf8d77d33bd82fdbbda480
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
A mixture of fixes and cleanup for LogKlog.cpp and friends.
- sscanf calls strlen. Check if the string is missing a nul
terminator, if it is, do not call sscanf.
- replace NULL with nullptr for stronger typechecking.
- pass by reference for simpler code.
- Use ssize_t where possible to check for negative values.
- fix FastCmp to add some validity checking since ASAN reports that
callers are not making sure pre-conditions are met.
- add fasticmp templates for completeness.
- if the buffer is too small to contain a meaningful time, do not
call down to log_time::strptime() because it does not limit its
accesses to the buffer boundaries, instead stopping at a
terminating nul or invalid match.
- move strnstr to LogUtils.h, drop size checking of needle and
clearly report the list of needles used with android::strnstr
- replace 'sizeof(static const char[]) - 1' with strlen.
Test: gTest liblog-unit-test, logd-unit-tests & logcat-unit-tests
Bug: 30792935
Bug: 36536248
Bug: 35468874
Bug: 34949125
Bug: 34606909
Bug: 36075298
Bug: 36608728
Change-Id: I161bf03ba029050e809b31cceef03f729d318866
|
|
|
|
|
|
|
|
|
| |
Switch _all_ file's coding style to match to ease all future changes.
SideEffects: None
Test: compile
Bug: 35373582
Change-Id: I470cb17f64fa48f14aafc02f574e296bffe3a3f3
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Will register a new event tag by name and format, and return an
event-log-tags format response with the newly allocated tag.
If format is not specified, then nothing will be recorded, but
a pre-existing named entry will be listed. If name and format are
not specified, list all dynamic entries. If name=* list all
event log tag entries.
Stickiness through logd crash will be managed with the tmpfs file
/dev/event-log-tags and through a reboot with add_tag entries in
the pmsg last logcat event log. On debug builds we retain a
/data/misc/logd/event-log-tags file that aids stickiness and that
can be picked up by the bugreport.
If we detect truncation damage to /dev/event-log-tags, or to
/data/misc/logd/event-log-tags, rebuild file with a new first line
signature incorporating the time so mmap'd readers of the file can
detect the possible change in shape and order.
Manual testing:
Make sure nc (netcat) is built for the target platform on the host:
$ m nc
Then the following can be used to issue a request on the platform:
$ echo -n 'getEventTag name=<name> format="<format>"\0EXIT\0' |
> nc -U /dev/socket/logd
Test: gTest logd-unit-test --gtest_filter=getEventTag*
Bug: 31456426
Change-Id: I5dacc5f84a24d52dae09cca5ee1a3a9f9207f06d
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
log selinux audit messages boolean (true or false, default true)
selection for logging destinations:
ro.logd.auditd - turn on logd.auditd to pick up violations.
ro.logd.auditd.dmesg - to the kernel log.
ro.logd.auditd.main - to the "main" log buffer.
ro.logd.auditd.events - to the "events" log buffer.
We used to also read logd.auditd.dmesg and persist.logd.auditd.dmesg
which do not get refreshed when /data mounts internally. This is a
confusing state as these properties will be read after a logd crash
and restart, adjusting the behavior of the logger. Same can be said
for logd.auditd as well. Drop reading these other parameters.
Test: manual set r/o parameters, stop/start logd to confirm behavior
Bug: 33969000
Bug: 27878170
Change-Id: I1a6bb4a903074c9aa7b227cf583a0094d49cbefd
|
|
|
|
|
|
|
|
|
|
| |
NULL represents system default. In the future, NULL could represent
static and dynamic tags, which can come from multiple files based on
implementation details in the liblog library.
Test: gTest logd-unit-tests & liblog-unit-tests
Bug: 31456426
Change-Id: I0e3d296de81ca299ae63d7b83781639ee67ec298
|
|
|
|
|
|
|
|
|
|
| |
files.[h|cpp] is bound to be abused with junk, replace with
android_get_control_file.[h|cpp]. Plus some sundry cleanup.
Test: gTest libcutils-tests, logd-unit-tests, liblog-unit-tests,
logcat-unit-tests and init_tests
Bug: 32450474
Change-Id: Ibd4a7aa4624ea19a43d1f98a3c71ac37805d36b5
|
|
|
|
|
|
|
|
|
| |
Allows us some leaway to investigate logd issues on eng builds
Test: gTests logd-unit-tests, liblog-unit-tests and logcat-unit-tests
Manual on eng builds, bad logd.rc to fake permission issues
Bug: 32450474
Change-Id: I432016e29e5601d67c502076ead941cecdcbebe7
|
|
|
|
|
|
| |
Test: gTest logd-unit-tests, liblog-unit-tests and logcat-unit-testsa
Bug: 32450474
Change-Id: Icdaf9e352e86c9e140928509201da743004aeedb
|
|
|
|
|
|
| |
Test: gTest logd-unit-tests, liblog-unit-tests and logcat-unit-tests
Bug: 32450474
Change-Id: I842a7a64f0ba695acef66caf54270f9475c9f9ac
|
|
|
|
|
|
|
|
|
| |
Use libcap instead of libminijail. Set CAP_SETGID before setgroups,
then clear it afterwards.
Test: gTest logd-unit-tests, liblog-unit-tests and logcat-unit-tests
Bug: 32450474
Change-Id: I2ed027fd5efd95f76b1dd4c5791bae5f2ea94c28
|
|
|
|
|
|
|
|
|
| |
Setup and then collect from the environment /proc/kmsg and /dev/kmsg
file descriptors. Do not do so for logcat --reinit.
Test: gTest logd-unit-tests, liblog-unit-tests and logcat-unit-tests
Bug: 32450474
Change-Id: Ied537ca561fcd4e71a9ad9c57398a23ba23f6ced
|
|
|
|
|
|
|
|
| |
Do not allow anyone to see logd memory.
Test: gTest logd-unit-tests, liblog-unit-tests and logcat-unit-tests
Bug: 32450474
Change-Id: Ic7377efcb7e1d3cd91b50741061037a0fb589045
|
|
|
|
|
|
| |
Test: gTest logd-unit-tests, liblog-unit-tests and logcat-unit-tests
Bug: 31750617
Change-Id: I692577cfdf4bf8c93616f32df4b56786918aef1c
|
|
|
|
|
|
|
| |
Test: gTest logd-unit-tests
Bug: 27566046
Bug: 31456426
Change-Id: I9faf88263fe62ce5bba80dc2cb928e6dbe73dbb2
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Allows us to mitigate the impact of MAP_PRIVATE and copy on write by
calling android_lookupEventTag_len instead of android_lookupEventTag,
and delaying the copy on write impact to the later. We return a
string length in a supplied location along with the string pointer
with android_lookupEventTag_len(const EventTagMap* map, size_t* len,
int tag). The string is not guaranteed to be nul terminated. Since
android_lookupEventTag() called even once can cause the memory
impact, we will mark it as deprecated, but we currently have no
timeframe for removal since this is a very old interface.
Add an API for __android_log_is_loggable_len() that accepts the non
null terminated content and fixup callers that would gain because the
length is known prior to the call either in the compiler or at
runtime. Tackle transition to android_lookupEventTag_len() and
fixup callers.
On any application that performs logging (eg: com.android.phone)
/proc/<pid>/smaps before:
xxxxxxxxxx-xxxxxxxxxx rw-p 00000000 fd:00 463 /system/etc/event-log-tags
Size: 20 kB
Rss: 20 kB
Pss: 1 kB
Shared_Clean: 0 kB
Shared_Dirty: 20 kB
Private_Clean: 0 kB
Private_Dirty: 0 kB
Referenced: 0 kB
Anonymous: 20 kB
AnonHugePages: 0 kB
Swap: 0 kB
SwapPss: 0 kB
KernelPageSize: 4 kB
MMUPageSize: 4 kB
Locked: 0 kB
VmFlags: rd wr mr mw me ac
/proc/<pid>/smaps after:
xxxxxxxxxx-xxxxxxxxxx rw-p 00000000 fd:00 1773 /system/etc/event-log-tags
Size: 20 kB
Rss: 20 kB
Pss: 1 kB
Shared_Clean: 20 kB (was 0kB)
Shared_Dirty: 0 kB (was 20kB)
Private_Clean: 0 kB
Private_Dirty: 0 kB
Referenced: 20 kB (was 0kB)
Anonymous: 0 kB (was 20kB)
AnonHugePages: 0 kB
Swap: 0 kB
SwapPss: 0 kB
KernelPageSize: 4 kB
MMUPageSize: 4 kB
Locked: 0 kB
VmFlags: rd wr mr mw me ac
Added liblog-unit-tests --gtest_filter=liblog.event_log_tags to
check for Shared_Clean: to not be 0 and Anonymous: to be 0 for
all processes referencing event-log-tags. Which can include multiple
references to /system/etc/event-log-tags and future possible refs to
/data/misc/logd/event-log-tags and /dev/event-log-tags. We want
failure messages to help point to errant code using the deprecated
interface.
This change saves 1/4MB of memory or more on a typical system.
Test: gTest liblog-unit-tests
Bug: 31456426
Change-Id: I9e08e44d9092bd96fe704b5709242e7195281d33
|
|\
| |
| |
| |
| |
| | |
am: d3dfd95728
Change-Id: I4ee161fac939c57f273e4af669c3e845b81a4b45
|
| |
| |
| |
| |
| |
| |
| |
| | |
Makes code smaller, removes duplication. Using Minijail also allows
adding further sandboxing down the road.
Bug: 30156807
Change-Id: I8fa242fba545049ee82f6655fe6ecc14c53fcab7
|
|\|
| |
| |
| |
| |
| | |
am: 7c50033e9f
Change-Id: Ie0fb615394eea100dbcc12519c52bbdba8fb8fe0
|
| |
| |
| |
| |
| |
| |
| | |
Makes the prdebug helper accessible for debugging
Bug: 30118730
Change-Id: Ieab60fd18221108ae27c54140a25061ab29ca1a3
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
The setgid() and setuid() call failure in logd.daemon thread
do not block overall functionality, so clearly tell static
analyzer and developers that we do not care to check their
return values.
SideEffects: None
Bug: 27434072
Change-Id: I6fdc87e8311ebc0173716080bbd72c86b3f00f78
|
|\ \
| | |
| | |
| | | |
Change-Id: Icf3257ee8a47f31ba812a5f47899b8022f4eedb7
|
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
This reverts commit 0bdad0f231103db89f2c0931616dd78309258d3b.
Bug: 26902605
Change-Id: I6ce8fa7bef63c45821628265c379970eb64963a2
|
|\| |
| |/
|/|
| |
| |
| |
| | |
am: 07522c6e9b
* commit '07522c6e9b8acba0f5cfb274d4514014749475e8':
logd: check return values
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
(cherry pick from commit bf7d0b887561929d22c8e2efa5d86cb0d7c50b51)
The setgid() and setuid() call failure in logd.daemon thread
do not block overall functionality, so clearly tell static
analyzer and developers that we do not care to check their
return values.
SideEffects: None
Bug: 27434072
Change-Id: I6fdc87e8311ebc0173716080bbd72c86b3f00f78
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
If a SELinux policy change or a switch to permissive mode is detected
on a user build, restart the device into safe mode, and keep it there
until an OTA is applied or user data is wiped.
This change deprecates the ro.logd.auditd property.
Needs matching changes from
I781c3059ea8d4fb2f0c923e4488b1932d69678d3
Ica825cf2af74f5624cf4091544bd24bb5482dbe7
Id3ca7889ede30b54b7af73dd50653ca1a20d59aa
Bug: 26902605
Change-Id: Idcdc5bff133f13c1267f0ec0a75cc8cf1ddbda0d
(cherry picked from commit d122ee65b66b5b33d51302dabbaa0d6c84597549)
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
If a SELinux policy change or a switch to permissive mode is detected
on a user build, restart the device into safe mode, and keep it there
until an OTA is applied or user data is wiped.
This change deprecates the ro.logd.auditd property.
Needs matching changes from
I781c3059ea8d4fb2f0c923e4488b1932d69678d3
Ica825cf2af74f5624cf4091544bd24bb5482dbe7
Id3ca7889ede30b54b7af73dd50653ca1a20d59aa
Bug: 26902605
Change-Id: Idcdc5bff133f13c1267f0ec0a75cc8cf1ddbda0d
|
| |
| |
| |
| | |
Change-Id: Ic644f1f78e68094f700834675f4acc63386a6b92
|
|/
|
|
|
|
|
|
|
|
| |
Usage: android::prdebug(const char *fmt, ...) __printflike(1, 2);
Will add logd prefix tag, log as debug priority in kernel logs,
and will suffix a newline if one is not supplied. To be used to
aid debugging of the logger only.
Change-Id: I217326ef34dc4eb0ea076bacb7a7a8b564c931c3
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
- enhance property_get_bool, drop property_get_bool_svelte
- enhance base properties with ro and persist variants
- update and fortify README.property
- primarily move auditd and kernel logger into a realm where
they can be controlled by build properties.
- Move logd.klogd to logd.kernel, and add ro.logd.kernel
and persist.logd.kernel.
- Add ro.logd.auditd and persist.logd.auditd.
- Document persist.logd.security
- Document log.tag and persist.logd.tag properties.
- Document ro.logd.size, persist.logd.size and logd.size
properties.
Bug: 26178938
Bug: 26029733
Bug: 17760225
Change-Id: Ibc1a497e45d69db5cf52133937f7ba6fb1d6cd21
|
|
|
|
|
| |
Bug: 25792367
Change-Id: Icae85a7de70b3a71f89b2bf8c80866649f727177
|
|
|
|
|
| |
Bug: 26115803
Change-Id: I6e8843ce9766756a40e6d176e0a822f62045c2af
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Add the following mount options to the /proc filesystem:
hidepid=2,gid=3009
This change blocks /proc access unless you're in group 3009
(aka AID_READPROC).
Please see
https://github.com/torvalds/linux/blob/master/Documentation/filesystems/proc.txt
for documentation on the hidepid option.
hidepid=2 is preferred over hidepid=1 since it leaks less information
and doesn't generate SELinux ptrace denials when trying to access
/proc without being in the proper group.
Add AID_READPROC to processes which need to access /proc entries for
other UIDs.
Bug: 23310674
Change-Id: I22bb55ff7b80ff722945e224845215196f09dafa
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
if ro.logd.timestamp or persist.logd.timestamp are set to the value
monotonic then liblog writer, liblog printing and logd all switch to
recording/printing monotonic time rather than realtime. If reinit
detects a change for presist.logd.timestamp, correct the older entry
timestamps in place.
ToDo: A corner case condition where new log entries in monotonic time
occur before logd reinit detects persist.logd.timestamp, there
will be a few out-of-order entries, but with accurate
timestamps. This problem does not happen for ro.logd.timestamp
as it is set before logd starts.
NB: This offers a nano second time accuracy on all log entries
that may be more suitable for merging with other system
activities, such as systrace, that also use monotonic time. This
feature is for debugging.
Bug: 23668800
Change-Id: Iee6dab7140061b1a6627254921411f61b01aa5c2
|
|
|
|
|
|
|
|
|
| |
- Add device (ro.logd.filter), persistent (persist.logd.filter)
properties to control the default filters
- Allow logcat -P default to produce expected results
- Allow logcat -P disable to produce expected results
Change-Id: I651cb705373ec1e88a99e4b9086da4f9668a468a
|
|
|
|
|
|
|
|
| |
Switch from the internal packages.list file parser
implementation to a common parser library.
Change-Id: I87a406802f95d8e7bfd8ee85f723f80e9e6b6c0c
Signed-off-by: William Roberts <william.c.roberts@intel.com>
|
|\
| |
| |
| |
| | |
* commit '72146b931ca61e942df91407b561f22648a70bf2':
logd: Add LogUtils.h
|
| |
| |
| |
| |
| |
| | |
Move prototypes from LogBufferElement.h to LogUtils.h
Change-Id: I55e42e17e6c997e35b2b78b87fd2f84f8f393282
|
|\|
| |
| |
| |
| |
| |
| |
| | |
* commit '1b2fb587eb7db6f9de1dda8663b33d87a2f5a27e':
logd: klogd deal with nuls in dmesg
logd: log_strtok_r deal with nuls
liblog: logprint: printable nul
logd: klogd: sniff for time correction on Mediatek
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Switch to using string and length in all transactions, treating
trailing nuls the same as spaces.
ToDo: change dumpstate (bugreport) to use logcat -b printable _regardless_
Bug: 23517551
Change-Id: I42162365e6bf8ed79d356e7b689a673902116fdb
|
| |
| |
| |
| |
| |
| |
| |
| | |
Rename to log_strntok_r and change from dealing with strings
to dealing with a string and an associated length.
Bug: 23517551
Change-Id: Ia72f1305a53f55eeef9861ac378fb8205fd2378e
|
|\|
| |
| |
| |
| | |
* commit '87122ce1d60dd6fbc18e747d976db734d502f2bf':
logd: increase dgram_max_qlen to 600
|
| |
| |
| |
| |
| |
| |
| |
| | |
Seeing liblog messages on system_server runtime restart
(too much system_server spam, 566 messages in 72ms)
Bug: 23788621
Change-Id: I5171f2c19a3538da190fc6c2b40e978d89bf0e20
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
- regression in log_strtok_r (part deux) In commit
'logd: fix kernel logline stutter'
2c3b300fd8307e8da13608197d0a89bc613de5fb we introduced log_strtok_r.
as a replacement for strtok_r that dealt with a problem with
some kernel log messages. Fix is to refine definition of
is_timestamp to not match on patterns like [0], requiring
a single period. Another fix is to refine definition of
is_prio to properly escape non-digit content.
- Missing content because SYSLOG_ACTION_SIZE_BUFFER with added logging
is too short for full read of SYSLOG_ACTION_READ_ALL dropping
initial content. Add a margin for additional 1024 bytes.
- Absolute _first_ log entry has sequence number of 1, which is
specifically dropped, start sequence count at 1 rather than 0.
- Remove trailing space for efficiency.
- If tag exists but no content, trick into kernel logging.
Bug: 21851884
Change-Id: I0867a555a3bca09bbf18d18e75e41dffffe57a23
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
(cherry pick from commit d98f4e8af5076e6a9dbd4ddc2c375cb7bcda8cd8)
sched_batch implies only a penalty to latency in scheduling, but
does not imply that the process will be given less cpu time. Increase
the nice level to 10 to prioritize it below ui threads.
Bug: 21696721
Change-Id: I075af059dc755402f7df9b0d7a66cca921ff04b2
|