From dd7bc3319deb2b77c5d07a51b7d6cd7e11b5beb0 Mon Sep 17 00:00:00 2001
From: The Android Open Source Project
Date: Tue, 3 Mar 2009 19:32:55 -0800
Subject: auto import from //depot/cupcake/@135843
---
libcutils/socket_local.h | 39 +++++++++++++++++++++++++++++++++++++++
1 file changed, 39 insertions(+)
create mode 100644 libcutils/socket_local.h
(limited to 'libcutils/socket_local.h')
diff --git a/libcutils/socket_local.h b/libcutils/socket_local.h
new file mode 100644
index 000000000..45b9856b6
--- /dev/null
+++ b/libcutils/socket_local.h
@@ -0,0 +1,39 @@
+/*
+ * Copyright (C) 2006 The Android Open Source Project
+ *
+ * Licensed under the Apache License, Version 2.0 (the "License");
+ * you may not use this file except in compliance with the License.
+ * You may obtain a copy of the License at
+ *
+ * http://www.apache.org/licenses/LICENSE-2.0
+ *
+ * Unless required by applicable law or agreed to in writing, software
+ * distributed under the License is distributed on an "AS IS" BASIS,
+ * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
+ * See the License for the specific language governing permissions and
+ * limitations under the License.
+ */
+
+#ifndef __SOCKET_LOCAL_H
+#define __SOCKET_LOCAL_H
+
+#define FILESYSTEM_SOCKET_PREFIX "/tmp/"
+#define ANDROID_RESERVED_SOCKET_PREFIX "/dev/socket/"
+
+/*
+ * Set up a given sockaddr_un, to have it refer to the given
+ * name in the given namespace. The namespace must be one
+ * of ANDROID_SOCKET_NAMESPACE_ABSTRACT
,
+ * ANDROID_SOCKET_NAMESPACE_RESERVED
, or
+ * ANDROID_SOCKET_NAMESPACE_FILESYSTEM
. Upon success,
+ * the pointed at sockaddr_un is filled in and the pointed at
+ * socklen_t is set to indicate the final length. This function
+ * will fail if the namespace is invalid (not one of the indicated
+ * constants) or if the name is too long.
+ *
+ * @return 0 on success or -1 on failure
+ */
+int socket_make_sockaddr_un(const char *name, int namespaceId,
+ struct sockaddr_un *p_addr, socklen_t *alen);
+
+#endif
--
cgit v1.2.3-54-g00ecf