# Copyright 2005 The Android Open Source Project # # Android.mk for adb # LOCAL_PATH:= $(call my-dir) ADB_CLANG := # libadb # ========================================================= # Much of adb is duplicated in bootable/recovery/minadb and fastboot. Changes # made to adb rarely get ported to the other two, so the trees have diverged a # bit. We'd like to stop this because it is a maintenance nightmare, but the # divergence makes this difficult to do all at once. For now, we will start # small by moving common files into a static library. Hopefully some day we can # get enough of adb in here that we no longer need minadb. https://b/17626262 LIBADB_SRC_FILES := \ adb.cpp \ adb_auth.cpp \ adb_io.cpp \ adb_listeners.cpp \ sockets.cpp \ transport.cpp \ transport_local.cpp \ transport_usb.cpp \ LIBADB_CFLAGS := \ -Wall -Werror \ -Wno-unused-parameter \ -Wno-missing-field-initializers \ -fvisibility=hidden \ LIBADB_darwin_SRC_FILES := \ fdevent.cpp \ get_my_path_darwin.c \ usb_osx.c \ LIBADB_linux_SRC_FILES := \ fdevent.cpp \ get_my_path_linux.cpp \ usb_linux.cpp \ LIBADB_windows_SRC_FILES := \ get_my_path_windows.cpp \ sysdeps_win32.c \ usb_windows.cpp \ include $(CLEAR_VARS) LOCAL_CLANG := $(ADB_CLANG) LOCAL_MODULE := libadbd LOCAL_CFLAGS := $(LIBADB_CFLAGS) -DADB_HOST=0 LOCAL_SRC_FILES := \ $(LIBADB_SRC_FILES) \ adb_auth_client.cpp \ fdevent.cpp \ jdwp_service.cpp \ qemu_tracing.cpp \ usb_linux_client.c \ include $(BUILD_STATIC_LIBRARY) include $(CLEAR_VARS) LOCAL_CLANG := $(ADB_CLANG) LOCAL_MODULE := libadb LOCAL_CFLAGS := $(LIBADB_CFLAGS) -DADB_HOST=1 LOCAL_SRC_FILES := \ $(LIBADB_SRC_FILES) \ $(LIBADB_$(HOST_OS)_SRC_FILES) \ adb_auth_host.cpp \ # Even though we're building a static library (and thus there's no link step for # this to take effect), this adds the SSL includes to our path. LOCAL_STATIC_LIBRARIES := libcrypto_static ifeq ($(HOST_OS),windows) LOCAL_C_INCLUDES += development/host/windows/usb/api/ endif include $(BUILD_HOST_STATIC_LIBRARY) LIBADB_TEST_SRCS := \ adb_io_test.cpp \ transport_test.cpp \ include $(CLEAR_VARS) LOCAL_CLANG := $(ADB_CLANG) LOCAL_MODULE := adbd_test LOCAL_CFLAGS := -DADB_HOST=0 $(LIBADB_CFLAGS) LOCAL_SRC_FILES := $(LIBADB_TEST_SRCS) LOCAL_STATIC_LIBRARIES := libadbd LOCAL_SHARED_LIBRARIES := liblog libbase libcutils include $(BUILD_NATIVE_TEST) include $(CLEAR_VARS) LOCAL_CLANG := $(ADB_CLANG) LOCAL_MODULE := adb_test LOCAL_CFLAGS := -DADB_HOST=1 $(LIBADB_CFLAGS) LOCAL_SRC_FILES := $(LIBADB_TEST_SRCS) services.cpp LOCAL_SHARED_LIBRARIES := liblog libbase LOCAL_STATIC_LIBRARIES := \ libadb \ libcrypto_static \ libcutils \ ifeq ($(HOST_OS),linux) LOCAL_LDLIBS += -lrt -ldl -lpthread endif include $(BUILD_HOST_NATIVE_TEST) # adb host tool # ========================================================= include $(CLEAR_VARS) ifeq ($(HOST_OS),linux) LOCAL_LDLIBS += -lrt -ldl -lpthread LOCAL_CFLAGS += -DWORKAROUND_BUG6558362 endif ifeq ($(HOST_OS),darwin) LOCAL_LDLIBS += -lpthread -framework CoreFoundation -framework IOKit -framework Carbon LOCAL_CFLAGS += -Wno-sizeof-pointer-memaccess -Wno-unused-parameter endif ifeq ($(HOST_OS),windows) EXTRA_STATIC_LIBS := AdbWinApi ifneq ($(strip $(USE_MINGW)),) # MinGW under Linux case LOCAL_LDLIBS += -lws2_32 -lgdi32 USE_SYSDEPS_WIN32 := 1 endif endif LOCAL_CLANG := $(ADB_CLANG) LOCAL_SRC_FILES := \ adb_main.cpp \ console.cpp \ commandline.cpp \ adb_client.cpp \ services.cpp \ file_sync_client.cpp \ LOCAL_CFLAGS += \ -Wall -Werror \ -Wno-unused-parameter \ -D_GNU_SOURCE \ -DADB_HOST=1 \ LOCAL_MODULE := adb LOCAL_MODULE_TAGS := debug LOCAL_STATIC_LIBRARIES := \ libadb \ libcrypto_static \ $(EXTRA_STATIC_LIBS) \ ifeq ($(USE_SYSDEPS_WIN32),) LOCAL_STATIC_LIBRARIES += libcutils endif include $(BUILD_HOST_EXECUTABLE) $(call dist-for-goals,dist_files sdk,$(LOCAL_BUILT_MODULE)) ifeq ($(HOST_OS),windows) $(LOCAL_INSTALLED_MODULE): \ $(HOST_OUT_EXECUTABLES)/AdbWinApi.dll \ $(HOST_OUT_EXECUTABLES)/AdbWinUsbApi.dll endif # adbd device daemon # ========================================================= include $(CLEAR_VARS) LOCAL_CLANG := $(ADB_CLANG) LOCAL_SRC_FILES := \ adb_main.cpp \ services.cpp \ file_sync_service.cpp \ framebuffer_service.cpp \ remount_service.cpp \ set_verity_enable_state_service.cpp \ LOCAL_CFLAGS := \ -DADB_HOST=0 \ -D_GNU_SOURCE \ -Wall -Werror \ -Wno-unused-parameter \ -Wno-deprecated-declarations \ ifneq (,$(filter userdebug eng,$(TARGET_BUILD_VARIANT))) LOCAL_CFLAGS += -DALLOW_ADBD_ROOT=1 endif ifneq (,$(filter userdebug eng,$(TARGET_BUILD_VARIANT))) LOCAL_CFLAGS += -DALLOW_ADBD_DISABLE_VERITY=1 endif LOCAL_MODULE := adbd LOCAL_FORCE_STATIC_EXECUTABLE := true LOCAL_MODULE_PATH := $(TARGET_ROOT_OUT_SBIN) LOCAL_UNSTRIPPED_PATH := $(TARGET_ROOT_OUT_SBIN_UNSTRIPPED) LOCAL_C_INCLUDES += system/extras/ext4_utils LOCAL_STATIC_LIBRARIES := \ libadbd \ libbase \ libfs_mgr \ liblog \ libcutils \ libc \ libmincrypt \ libselinux \ libext4_utils_static \ include $(BUILD_EXECUTABLE)