/* * Copyright (C) 2006 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef __FDEVENT_H #define __FDEVENT_H #include #include /* for int64_t */ #include /* events that may be observed */ #define FDE_READ 0x0001 #define FDE_WRITE 0x0002 #define FDE_ERROR 0x0004 typedef void (*fd_func)(int fd, unsigned events, void *userdata); struct fdevent { fdevent* next = nullptr; fdevent* prev = nullptr; int fd = -1; int force_eof = 0; uint16_t state = 0; uint16_t events = 0; fd_func func = nullptr; void* arg = nullptr; }; /* Allocate and initialize a new fdevent object * Note: use FD_TIMER as 'fd' to create a fd-less object * (used to implement timers). */ fdevent *fdevent_create(int fd, fd_func func, void *arg); /* Uninitialize and deallocate an fdevent object that was ** created by fdevent_create() */ void fdevent_destroy(fdevent *fde); /* Change which events should cause notifications */ void fdevent_set(fdevent *fde, unsigned events); void fdevent_add(fdevent *fde, unsigned events); void fdevent_del(fdevent *fde, unsigned events); void fdevent_set_timeout(fdevent *fde, int64_t timeout_ms); /* loop forever, handling events. */ void fdevent_loop(); void check_main_thread(); // Queue an operation to run on the main thread. void fdevent_run_on_main_thread(std::function fn); // The following functions are used only for tests. void fdevent_terminate_loop(); size_t fdevent_installed_count(); void fdevent_reset(); void set_main_thread(); #endif