/* * Copyright (C) 2017 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef _INIT_REBOOT_H #define _INIT_REBOOT_H #include namespace android { namespace init { // This is a wrapper around the actual reboot calls. DoReboot() should be preferred in most cases. void __attribute__((noreturn)) RebootSystem(unsigned int cmd, const std::string& rebootTarget); /* Reboot / shutdown the system. * cmd ANDROID_RB_* as defined in android_reboot.h * reason Reason string like "reboot", "shutdown,userrequested" * rebootTarget Reboot target string like "bootloader". Otherwise, it should be an * empty string. * runFsck Whether to run fsck after umount is done. */ void DoReboot(unsigned int cmd, const std::string& reason, const std::string& rebootTarget, bool runFsck) __attribute__((__noreturn__)); // Parses and handles a setprop sys.powerctl message. bool HandlePowerctlMessage(const std::string& command); // Determines whether the system is capable of rebooting. This is conservative, // so if any of the attempts to determine this fail, it will still return true. bool IsRebootCapable(); } // namespace init } // namespace android #endif