/* * Copyright (C) 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specic language governing permissions and * limitations under the License. */ #include "libappfuse/FuseBridgeLoop.h" #include #include #include #include #include #include "libappfuse/EpollController.h" namespace android { namespace fuse { namespace { enum class FuseBridgeState { kWaitToReadEither, kWaitToReadProxy, kWaitToWriteProxy, kClosing }; struct FuseBridgeEntryEvent { FuseBridgeEntry* entry; int events; }; void GetObservedEvents(FuseBridgeState state, int* device_events, int* proxy_events) { switch (state) { case FuseBridgeState::kWaitToReadEither: *device_events = EPOLLIN; *proxy_events = EPOLLIN; return; case FuseBridgeState::kWaitToReadProxy: *device_events = 0; *proxy_events = EPOLLIN; return; case FuseBridgeState::kWaitToWriteProxy: *device_events = 0; *proxy_events = EPOLLOUT; return; case FuseBridgeState::kClosing: *device_events = 0; *proxy_events = 0; return; } } } class FuseBridgeEntry { public: FuseBridgeEntry(int mount_id, base::unique_fd&& dev_fd, base::unique_fd&& proxy_fd) : mount_id_(mount_id), device_fd_(std::move(dev_fd)), proxy_fd_(std::move(proxy_fd)), state_(FuseBridgeState::kWaitToReadEither), last_state_(FuseBridgeState::kWaitToReadEither), last_device_events_({this, 0}), last_proxy_events_({this, 0}), open_count_(0) {} // Transfer bytes depends on availability of FDs and the internal |state_|. void Transfer(FuseBridgeLoopCallback* callback) { constexpr int kUnexpectedEventMask = ~(EPOLLIN | EPOLLOUT); const bool unexpected_event = (last_device_events_.events & kUnexpectedEventMask) || (last_proxy_events_.events & kUnexpectedEventMask); const bool device_read_ready = last_device_events_.events & EPOLLIN; const bool proxy_read_ready = last_proxy_events_.events & EPOLLIN; const bool proxy_write_ready = last_proxy_events_.events & EPOLLOUT; last_device_events_.events = 0; last_proxy_events_.events = 0; LOG(VERBOSE) << "Transfer device_read_ready=" << device_read_ready << " proxy_read_ready=" << proxy_read_ready << " proxy_write_ready=" << proxy_write_ready; if (unexpected_event) { LOG(ERROR) << "Invalid epoll event is observed"; state_ = FuseBridgeState::kClosing; return; } switch (state_) { case FuseBridgeState::kWaitToReadEither: if (proxy_read_ready) { state_ = ReadFromProxy(); } else if (device_read_ready) { state_ = ReadFromDevice(callback); } return; case FuseBridgeState::kWaitToReadProxy: CHECK(proxy_read_ready); state_ = ReadFromProxy(); return; case FuseBridgeState::kWaitToWriteProxy: CHECK(proxy_write_ready); state_ = WriteToProxy(); return; case FuseBridgeState::kClosing: return; } } bool IsClosing() const { return state_ == FuseBridgeState::kClosing; } int mount_id() const { return mount_id_; } private: friend class BridgeEpollController; FuseBridgeState ReadFromProxy() { switch (buffer_.response.ReadOrAgain(proxy_fd_)) { case ResultOrAgain::kSuccess: break; case ResultOrAgain::kFailure: return FuseBridgeState::kClosing; case ResultOrAgain::kAgain: return FuseBridgeState::kWaitToReadProxy; } if (!buffer_.response.Write(device_fd_)) { return FuseBridgeState::kClosing; } auto it = opcode_map_.find(buffer_.response.header.unique); if (it != opcode_map_.end()) { switch (it->second) { case FUSE_OPEN: if (buffer_.response.header.error == fuse::kFuseSuccess) { open_count_++; } break; case FUSE_RELEASE: if (open_count_ > 0) { open_count_--; } else { LOG(WARNING) << "Unexpected FUSE_RELEASE before opening a file."; break; } if (open_count_ == 0) { return FuseBridgeState::kClosing; } break; } opcode_map_.erase(it); } return FuseBridgeState::kWaitToReadEither; } FuseBridgeState ReadFromDevice(FuseBridgeLoopCallback* callback) { LOG(VERBOSE) << "ReadFromDevice"; if (!buffer_.request.Read(device_fd_)) { return FuseBridgeState::kClosing; } const uint32_t opcode = buffer_.request.header.opcode; LOG(VERBOSE) << "Read a fuse packet, opcode=" << opcode; switch (opcode) { case FUSE_FORGET: // Do not reply to FUSE_FORGET. return FuseBridgeState::kWaitToReadEither; case FUSE_LOOKUP: case FUSE_GETATTR: case FUSE_OPEN: case FUSE_READ: case FUSE_WRITE: case FUSE_RELEASE: case FUSE_FSYNC: if (opcode == FUSE_OPEN || opcode == FUSE_RELEASE) { opcode_map_.emplace(buffer_.request.header.unique, opcode); } return WriteToProxy(); case FUSE_INIT: buffer_.HandleInit(); break; default: buffer_.HandleNotImpl(); break; } if (!buffer_.response.Write(device_fd_)) { return FuseBridgeState::kClosing; } if (opcode == FUSE_INIT) { callback->OnMount(mount_id_); } return FuseBridgeState::kWaitToReadEither; } FuseBridgeState WriteToProxy() { switch (buffer_.request.WriteOrAgain(proxy_fd_)) { case ResultOrAgain::kSuccess: return FuseBridgeState::kWaitToReadEither; case ResultOrAgain::kFailure: return FuseBridgeState::kClosing; case ResultOrAgain::kAgain: return FuseBridgeState::kWaitToWriteProxy; } } const int mount_id_; base::unique_fd device_fd_; base::unique_fd proxy_fd_; FuseBuffer buffer_; FuseBridgeState state_; FuseBridgeState last_state_; FuseBridgeEntryEvent last_device_events_; FuseBridgeEntryEvent last_proxy_events_; // Remember map between unique and opcode in fuse_in_header so that we can // refer the opcode later. std::unordered_map opcode_map_; int open_count_; DISALLOW_COPY_AND_ASSIGN(FuseBridgeEntry); }; class BridgeEpollController : private EpollController { public: BridgeEpollController(base::unique_fd&& poll_fd) : EpollController(std::move(poll_fd)) {} bool AddBridgePoll(FuseBridgeEntry* bridge) const { return InvokeControl(EPOLL_CTL_ADD, bridge); } bool UpdateOrDeleteBridgePoll(FuseBridgeEntry* bridge) const { return InvokeControl( bridge->state_ != FuseBridgeState::kClosing ? EPOLL_CTL_MOD : EPOLL_CTL_DEL, bridge); } bool Wait(size_t bridge_count, std::unordered_set* entries_out) { CHECK(entries_out); const size_t event_count = std::max(bridge_count * 2, 1); if (!EpollController::Wait(event_count)) { return false; } entries_out->clear(); for (const auto& event : events()) { FuseBridgeEntryEvent* const entry_event = reinterpret_cast(event.data.ptr); entry_event->events = event.events; entries_out->insert(entry_event->entry); } return true; } private: bool InvokeControl(int op, FuseBridgeEntry* bridge) const { LOG(VERBOSE) << "InvokeControl op=" << op << " bridge=" << bridge->mount_id_ << " state=" << static_cast(bridge->state_) << " last_state=" << static_cast(bridge->last_state_); int last_device_events; int last_proxy_events; int device_events; int proxy_events; GetObservedEvents(bridge->last_state_, &last_device_events, &last_proxy_events); GetObservedEvents(bridge->state_, &device_events, &proxy_events); bool result = true; if (op != EPOLL_CTL_MOD || last_device_events != device_events) { result &= EpollController::InvokeControl(op, bridge->device_fd_, device_events, &bridge->last_device_events_); } if (op != EPOLL_CTL_MOD || last_proxy_events != proxy_events) { result &= EpollController::InvokeControl(op, bridge->proxy_fd_, proxy_events, &bridge->last_proxy_events_); } return result; } }; FuseBridgeLoop::FuseBridgeLoop() : opened_(true) { base::unique_fd epoll_fd(epoll_create1(/* no flag */ 0)); if (epoll_fd.get() == -1) { PLOG(ERROR) << "Failed to open FD for epoll"; opened_ = false; return; } epoll_controller_.reset(new BridgeEpollController(std::move(epoll_fd))); } FuseBridgeLoop::~FuseBridgeLoop() { CHECK(bridges_.empty()); } bool FuseBridgeLoop::AddBridge(int mount_id, base::unique_fd dev_fd, base::unique_fd proxy_fd) { LOG(VERBOSE) << "Adding bridge " << mount_id; std::unique_ptr bridge( new FuseBridgeEntry(mount_id, std::move(dev_fd), std::move(proxy_fd))); std::lock_guard lock(mutex_); if (!opened_) { LOG(ERROR) << "Tried to add a mount to a closed bridge"; return false; } if (bridges_.count(mount_id)) { LOG(ERROR) << "Tried to add a mount point that has already been added"; return false; } if (!epoll_controller_->AddBridgePoll(bridge.get())) { return false; } bridges_.emplace(mount_id, std::move(bridge)); return true; } bool FuseBridgeLoop::ProcessEventLocked(const std::unordered_set& entries, FuseBridgeLoopCallback* callback) { for (auto entry : entries) { entry->Transfer(callback); if (!epoll_controller_->UpdateOrDeleteBridgePoll(entry)) { return false; } if (entry->IsClosing()) { const int mount_id = entry->mount_id(); callback->OnClosed(mount_id); bridges_.erase(mount_id); if (bridges_.size() == 0) { // All bridges are now closed. return false; } } } return true; } void FuseBridgeLoop::Start(FuseBridgeLoopCallback* callback) { LOG(DEBUG) << "Start fuse bridge loop"; std::unordered_set entries; while (true) { const bool wait_result = epoll_controller_->Wait(bridges_.size(), &entries); LOG(VERBOSE) << "Receive epoll events"; { std::lock_guard lock(mutex_); if (!(wait_result && ProcessEventLocked(entries, callback))) { for (auto it = bridges_.begin(); it != bridges_.end();) { callback->OnClosed(it->second->mount_id()); it = bridges_.erase(it); } opened_ = false; return; } } } } } // namespace fuse } // namespace android