/* * Copyright (C) 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specic language governing permissions and * limitations under the License. */ #include "libappfuse/FuseBuffer.h" #include #include #include #include #include #include #include #include #include #include namespace android { namespace fuse { namespace { constexpr useconds_t kRetrySleepForWriting = 1000; // 1 ms template bool CheckHeaderLength(const FuseMessage* self, const char* name, size_t max_size) { const auto& header = static_cast(self)->header; if (header.len >= sizeof(header) && header.len <= max_size) { return true; } else { LOG(ERROR) << "Invalid header length is found in " << name << ": " << header.len; return false; } } template ResultOrAgain ReadInternal(FuseMessage* self, int fd, int sockflag) { char* const buf = reinterpret_cast(self); const ssize_t result = sockflag ? TEMP_FAILURE_RETRY(recv(fd, buf, sizeof(T), sockflag)) : TEMP_FAILURE_RETRY(read(fd, buf, sizeof(T))); switch (result) { case 0: // Expected EOF. return ResultOrAgain::kFailure; case -1: if (errno == EAGAIN) { return ResultOrAgain::kAgain; } PLOG(ERROR) << "Failed to read a FUSE message"; return ResultOrAgain::kFailure; } const auto& header = static_cast(self)->header; if (result < static_cast(sizeof(header))) { LOG(ERROR) << "Read bytes " << result << " are shorter than header size " << sizeof(header); return ResultOrAgain::kFailure; } if (!CheckHeaderLength(self, "Read", sizeof(T))) { return ResultOrAgain::kFailure; } if (static_cast(result) != header.len) { LOG(ERROR) << "Read bytes " << result << " are different from header.len " << header.len; return ResultOrAgain::kFailure; } return ResultOrAgain::kSuccess; } template ResultOrAgain WriteInternal(const FuseMessage* self, int fd, int sockflag, const void* data, size_t max_size) { if (!CheckHeaderLength(self, "Write", max_size)) { return ResultOrAgain::kFailure; } const char* const buf = reinterpret_cast(self); const auto& header = static_cast(self)->header; while (true) { int result; if (sockflag) { CHECK(data == nullptr); result = TEMP_FAILURE_RETRY(send(fd, buf, header.len, sockflag)); } else if (data) { const struct iovec vec[] = {{const_cast(buf), sizeof(header)}, {const_cast(data), header.len - sizeof(header)}}; result = TEMP_FAILURE_RETRY(writev(fd, vec, arraysize(vec))); } else { result = TEMP_FAILURE_RETRY(write(fd, buf, header.len)); } if (result == -1) { switch (errno) { case ENOBUFS: // When returning ENOBUFS, epoll still reports the FD is writable. Just usleep // and retry again. usleep(kRetrySleepForWriting); continue; case EAGAIN: return ResultOrAgain::kAgain; default: PLOG(ERROR) << "Failed to write a FUSE message: " << "fd=" << fd << " " << "sockflag=" << sockflag << " " << "data=" << data; return ResultOrAgain::kFailure; } } if (static_cast(result) != header.len) { LOG(ERROR) << "Written bytes " << result << " is different from length in header " << header.len; return ResultOrAgain::kFailure; } return ResultOrAgain::kSuccess; } } } static_assert(std::is_standard_layout::value, "FuseBuffer must be standard layout union."); bool SetupMessageSockets(base::unique_fd (*result)[2]) { base::unique_fd fds[2]; { int raw_fds[2]; if (socketpair(AF_UNIX, SOCK_SEQPACKET, 0, raw_fds) == -1) { PLOG(ERROR) << "Failed to create sockets for proxy"; return false; } fds[0].reset(raw_fds[0]); fds[1].reset(raw_fds[1]); } constexpr int kMaxMessageSize = sizeof(FuseBuffer); if (setsockopt(fds[0], SOL_SOCKET, SO_SNDBUFFORCE, &kMaxMessageSize, sizeof(int)) != 0 || setsockopt(fds[1], SOL_SOCKET, SO_SNDBUFFORCE, &kMaxMessageSize, sizeof(int)) != 0) { PLOG(ERROR) << "Failed to update buffer size for socket"; return false; } (*result)[0] = std::move(fds[0]); (*result)[1] = std::move(fds[1]); return true; } template bool FuseMessage::Read(int fd) { return ReadInternal(this, fd, 0) == ResultOrAgain::kSuccess; } template ResultOrAgain FuseMessage::ReadOrAgain(int fd) { return ReadInternal(this, fd, MSG_DONTWAIT); } template bool FuseMessage::Write(int fd) const { return WriteInternal(this, fd, 0, nullptr, sizeof(T)) == ResultOrAgain::kSuccess; } template bool FuseMessage::WriteWithBody(int fd, size_t max_size, const void* data) const { CHECK(data != nullptr); return WriteInternal(this, fd, 0, data, max_size) == ResultOrAgain::kSuccess; } template ResultOrAgain FuseMessage::WriteOrAgain(int fd) const { return WriteInternal(this, fd, MSG_DONTWAIT, nullptr, sizeof(T)); } void FuseRequest::Reset( uint32_t data_length, uint32_t opcode, uint64_t unique) { memset(this, 0, sizeof(fuse_in_header) + data_length); header.len = sizeof(fuse_in_header) + data_length; header.opcode = opcode; header.unique = unique; } template void FuseResponseBase::ResetHeader(uint32_t data_length, int32_t error, uint64_t unique) { CHECK_LE(error, 0) << "error should be zero or negative."; header.len = sizeof(fuse_out_header) + data_length; header.error = error; header.unique = unique; } template void FuseResponseBase::Reset(uint32_t data_length, int32_t error, uint64_t unique) { memset(this, 0, sizeof(fuse_out_header) + data_length); ResetHeader(data_length, error, unique); } void FuseBuffer::HandleInit() { const fuse_init_in* const in = &request.init_in; // Before writing |out|, we need to copy data from |in|. const uint64_t unique = request.header.unique; const uint32_t minor = in->minor; const uint32_t max_readahead = in->max_readahead; // Kernel 2.6.16 is the first stable kernel with struct fuse_init_out // defined (fuse version 7.6). The structure is the same from 7.6 through // 7.22. Beginning with 7.23, the structure increased in size and added // new parameters. if (in->major != FUSE_KERNEL_VERSION || in->minor < 6) { LOG(ERROR) << "Fuse kernel version mismatch: Kernel version " << in->major << "." << in->minor << " Expected at least " << FUSE_KERNEL_VERSION << ".6"; response.Reset(0, -EPERM, unique); return; } // We limit ourselves to minor=15 because we don't handle BATCH_FORGET yet. // Thus we need to use FUSE_COMPAT_22_INIT_OUT_SIZE. #if defined(FUSE_COMPAT_22_INIT_OUT_SIZE) // FUSE_KERNEL_VERSION >= 23. const size_t response_size = FUSE_COMPAT_22_INIT_OUT_SIZE; #else const size_t response_size = sizeof(fuse_init_out); #endif response.Reset(response_size, kFuseSuccess, unique); fuse_init_out* const out = &response.init_out; out->major = FUSE_KERNEL_VERSION; out->minor = std::min(minor, 15u); out->max_readahead = max_readahead; out->flags = FUSE_ATOMIC_O_TRUNC | FUSE_BIG_WRITES; out->max_background = 32; out->congestion_threshold = 32; out->max_write = kFuseMaxWrite; } void FuseBuffer::HandleNotImpl() { LOG(VERBOSE) << "NOTIMPL op=" << request.header.opcode << " uniq=" << request.header.unique << " nid=" << request.header.nodeid; // Add volatile as a workaround for compiler issue which removes the temporary // variable. const volatile uint64_t unique = request.header.unique; response.Reset(0, -ENOSYS, unique); } template class FuseMessage; template class FuseMessage; template class FuseMessage; template struct FuseResponseBase<0u>; template struct FuseResponseBase; } // namespace fuse } // namespace android