/* * Copyright (C) 2008 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include /* * Implementation of the user-space ashmem API for devices, which have our * ashmem-enabled kernel. See ashmem-sim.c for the "fake" tmp-based version, * used by the simulator. */ #define LOG_TAG "ashmem" #include #include #include #include #include #include #include #include #include #include #include #define ASHMEM_DEVICE "/dev/ashmem" /* ashmem identity */ static dev_t __ashmem_rdev; /* * If we trigger a signal handler in the middle of locked activity and the * signal handler calls ashmem, we could get into a deadlock state. */ static pthread_mutex_t __ashmem_lock = PTHREAD_MUTEX_INITIALIZER; /* logistics of getting file descriptor for ashmem */ static int __ashmem_open_locked() { int ret; struct stat st; int fd = TEMP_FAILURE_RETRY(open(ASHMEM_DEVICE, O_RDWR | O_CLOEXEC)); if (fd < 0) { return fd; } ret = TEMP_FAILURE_RETRY(fstat(fd, &st)); if (ret < 0) { int save_errno = errno; close(fd); errno = save_errno; return ret; } if (!S_ISCHR(st.st_mode) || !st.st_rdev) { close(fd); errno = ENOTTY; return -1; } __ashmem_rdev = st.st_rdev; return fd; } static int __ashmem_open() { int fd; pthread_mutex_lock(&__ashmem_lock); fd = __ashmem_open_locked(); pthread_mutex_unlock(&__ashmem_lock); return fd; } /* Make sure file descriptor references ashmem, negative number means false */ static int __ashmem_is_ashmem(int fd, int fatal) { dev_t rdev; struct stat st; if (fstat(fd, &st) < 0) { return -1; } rdev = 0; /* Too much complexity to sniff __ashmem_rdev */ if (S_ISCHR(st.st_mode) && st.st_rdev) { pthread_mutex_lock(&__ashmem_lock); rdev = __ashmem_rdev; if (rdev) { pthread_mutex_unlock(&__ashmem_lock); } else { int fd = __ashmem_open_locked(); if (fd < 0) { pthread_mutex_unlock(&__ashmem_lock); return -1; } rdev = __ashmem_rdev; pthread_mutex_unlock(&__ashmem_lock); close(fd); } if (st.st_rdev == rdev) { return 0; } } if (fatal) { if (rdev) { LOG_ALWAYS_FATAL("illegal fd=%d mode=0%o rdev=%d:%d expected 0%o %d:%d", fd, st.st_mode, major(st.st_rdev), minor(st.st_rdev), S_IFCHR | S_IRUSR | S_IWUSR | S_IRGRP | S_IWGRP | S_IROTH | S_IRGRP, major(rdev), minor(rdev)); } else { LOG_ALWAYS_FATAL("illegal fd=%d mode=0%o rdev=%d:%d expected 0%o", fd, st.st_mode, major(st.st_rdev), minor(st.st_rdev), S_IFCHR | S_IRUSR | S_IWUSR | S_IRGRP | S_IWGRP | S_IROTH | S_IRGRP); } /* NOTREACHED */ } errno = ENOTTY; return -1; } static int __ashmem_check_failure(int fd, int result) { if (result == -1 && errno == ENOTTY) __ashmem_is_ashmem(fd, 1); return result; } int ashmem_valid(int fd) { return __ashmem_is_ashmem(fd, 0) >= 0; } /* * ashmem_create_region - creates a new ashmem region and returns the file * descriptor, or <0 on error * * `name' is an optional label to give the region (visible in /proc/pid/maps) * `size' is the size of the region, in page-aligned bytes */ int ashmem_create_region(const char *name, size_t size) { int ret, save_errno; int fd = __ashmem_open(); if (fd < 0) { return fd; } if (name) { char buf[ASHMEM_NAME_LEN] = {0}; strlcpy(buf, name, sizeof(buf)); ret = TEMP_FAILURE_RETRY(ioctl(fd, ASHMEM_SET_NAME, buf)); if (ret < 0) { goto error; } } ret = TEMP_FAILURE_RETRY(ioctl(fd, ASHMEM_SET_SIZE, size)); if (ret < 0) { goto error; } return fd; error: save_errno = errno; close(fd); errno = save_errno; return ret; } int ashmem_set_prot_region(int fd, int prot) { return __ashmem_check_failure(fd, TEMP_FAILURE_RETRY(ioctl(fd, ASHMEM_SET_PROT_MASK, prot))); } int ashmem_pin_region(int fd, size_t offset, size_t len) { // TODO: should LP64 reject too-large offset/len? ashmem_pin pin = { static_cast(offset), static_cast(len) }; return __ashmem_check_failure(fd, TEMP_FAILURE_RETRY(ioctl(fd, ASHMEM_PIN, &pin))); } int ashmem_unpin_region(int fd, size_t offset, size_t len) { // TODO: should LP64 reject too-large offset/len? ashmem_pin pin = { static_cast(offset), static_cast(len) }; return __ashmem_check_failure(fd, TEMP_FAILURE_RETRY(ioctl(fd, ASHMEM_UNPIN, &pin))); } int ashmem_get_size_region(int fd) { return __ashmem_check_failure(fd, TEMP_FAILURE_RETRY(ioctl(fd, ASHMEM_GET_SIZE, NULL))); }