/* * Copyright (C) 2014 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include #include #include #include #include #include #include #include #include #include typedef struct { const char* path; unsigned uid; unsigned gid; unsigned mode; uint64_t capabilities; } Path; static Path* canned_data = NULL; static int canned_alloc = 0; static int canned_used = 0; static int path_compare(const void* a, const void* b) { return strcmp(((Path*)a)->path, ((Path*)b)->path); } int load_canned_fs_config(const char* fn) { char buf[PATH_MAX + 200]; FILE* f; f = fopen(fn, "r"); if (f == NULL) { fprintf(stderr, "failed to open %s: %s\n", fn, strerror(errno)); return -1; } while (fgets(buf, sizeof(buf), f)) { Path* p; char* token; char* line = buf; bool rootdir; while (canned_used >= canned_alloc) { canned_alloc = (canned_alloc+1) * 2; canned_data = (Path*) realloc(canned_data, canned_alloc * sizeof(Path)); } p = canned_data + canned_used; if (line[0] == '/') line++; rootdir = line[0] == ' '; p->path = strdup(rootdir ? "" : strtok(line, " ")); p->uid = atoi(strtok(rootdir ? line : NULL, " ")); p->gid = atoi(strtok(NULL, " ")); p->mode = strtol(strtok(NULL, " "), NULL, 8); // mode is in octal p->capabilities = 0; do { token = strtok(NULL, " "); if (token && strncmp(token, "capabilities=", 13) == 0) { p->capabilities = strtoll(token+13, NULL, 0); break; } } while (token); canned_used++; } fclose(f); qsort(canned_data, canned_used, sizeof(Path), path_compare); printf("loaded %d fs_config entries\n", canned_used); return 0; } static const int kDebugCannedFsConfig = 0; void canned_fs_config(const char* path, int dir, const char* target_out_path, unsigned* uid, unsigned* gid, unsigned* mode, uint64_t* capabilities) { Path key, *p; key.path = path; if (path[0] == '/') key.path++; // canned paths lack the leading '/' p = (Path*) bsearch(&key, canned_data, canned_used, sizeof(Path), path_compare); if (p == NULL) { fprintf(stderr, "failed to find [%s] in canned fs_config\n", path); exit(1); } *uid = p->uid; *gid = p->gid; *mode = p->mode; *capabilities = p->capabilities; if (kDebugCannedFsConfig) { // for debugging, run the built-in fs_config and compare the results. unsigned c_uid, c_gid, c_mode; uint64_t c_capabilities; fs_config(path, dir, target_out_path, &c_uid, &c_gid, &c_mode, &c_capabilities); if (c_uid != *uid) printf("%s uid %d %d\n", path, *uid, c_uid); if (c_gid != *gid) printf("%s gid %d %d\n", path, *gid, c_gid); if (c_mode != *mode) printf("%s mode 0%o 0%o\n", path, *mode, c_mode); if (c_capabilities != *capabilities) { printf("%s capabilities %" PRIx64 " %" PRIx64 "\n", path, *capabilities, c_capabilities); } } }