/* * Copyright (C) 2010 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #if defined(__APPLE__) /* * Implementation of the POSIX open_memstream() function, which Linux has * but BSD lacks. * * Summary: * - Works like a file-backed FILE* opened with fopen(name, "w"), but the * backing is a chunk of memory rather than a file. * - The buffer expands as you write more data. Seeking past the end * of the file and then writing to it zero-fills the gap. * - The values at "*bufp" and "*sizep" should be considered read-only, * and are only valid immediately after an fflush() or fclose(). * - A '\0' is maintained just past the end of the file. This is not included * in "*sizep". (The behavior w.r.t. fseek() is not clearly defined. * The spec says the null byte is written when a write() advances EOF, * but it looks like glibc ensures the null byte is always found at EOF, * even if you just seeked backwards. The example on the opengroup.org * page suggests that this is the expected behavior. The null must be * present after a no-op fflush(), which we can't see, so we have to save * and restore it. Annoying, but allows file truncation.) * - After fclose(), the caller must eventually free(*bufp). * * This is built out of funopen(), which BSD has but Linux lacks. There is * no flush() operator, so we need to keep the user pointers up to date * after each operation. * * I don't think Windows has any of the above, but we don't need to use * them there, so we just supply a stub. */ #include #include #include #include #include #include #include #include #if 0 # define DBUG(x) printf x #else # define DBUG(x) ((void)0) #endif /* * Definition of a seekable, write-only memory stream. */ typedef struct { char** bufp; /* pointer to buffer pointer */ size_t* sizep; /* pointer to eof */ size_t allocSize; /* size of buffer */ size_t eof; /* furthest point we've written to */ size_t offset; /* current write offset */ char saved; /* required by NUL handling */ } MemStream; #define kInitialSize 1024 /* * Ensure that we have enough storage to write "size" bytes at the * current offset. We also have to take into account the extra '\0' * that we maintain just past EOF. * * Returns 0 on success. */ static int ensureCapacity(MemStream* stream, int writeSize) { DBUG(("+++ ensureCap off=%d size=%d\n", stream->offset, writeSize)); size_t neededSize = stream->offset + writeSize + 1; if (neededSize <= stream->allocSize) return 0; size_t newSize; if (stream->allocSize == 0) { newSize = kInitialSize; } else { newSize = stream->allocSize; newSize += newSize / 2; /* expand by 3/2 */ } if (newSize < neededSize) newSize = neededSize; DBUG(("+++ realloc %p->%p to size=%d\n", stream->bufp, *stream->bufp, newSize)); char* newBuf = (char*) realloc(*stream->bufp, newSize); if (newBuf == NULL) return -1; *stream->bufp = newBuf; stream->allocSize = newSize; return 0; } /* * Write data to a memstream, expanding the buffer if necessary. * * If we previously seeked beyond EOF, zero-fill the gap. * * Returns the number of bytes written. */ static int write_memstream(void* cookie, const char* buf, int size) { MemStream* stream = (MemStream*) cookie; if (ensureCapacity(stream, size) < 0) return -1; /* seeked past EOF earlier? */ if (stream->eof < stream->offset) { DBUG(("+++ zero-fill gap from %d to %d\n", stream->eof, stream->offset-1)); memset(*stream->bufp + stream->eof, '\0', stream->offset - stream->eof); } /* copy data, advance write pointer */ memcpy(*stream->bufp + stream->offset, buf, size); stream->offset += size; if (stream->offset > stream->eof) { /* EOF has advanced, update it and append null byte */ DBUG(("+++ EOF advanced to %d, appending nul\n", stream->offset)); assert(stream->offset < stream->allocSize); stream->eof = stream->offset; } else { /* within previously-written area; save char we're about to stomp */ DBUG(("+++ within written area, saving '%c' at %d\n", *(*stream->bufp + stream->offset), stream->offset)); stream->saved = *(*stream->bufp + stream->offset); } *(*stream->bufp + stream->offset) = '\0'; *stream->sizep = stream->offset; return size; } /* * Seek within a memstream. * * Returns the new offset, or -1 on failure. */ static fpos_t seek_memstream(void* cookie, fpos_t offset, int whence) { MemStream* stream = (MemStream*) cookie; off_t newPosn = (off_t) offset; if (whence == SEEK_CUR) { newPosn += stream->offset; } else if (whence == SEEK_END) { newPosn += stream->eof; } if (newPosn < 0 || ((fpos_t)((size_t) newPosn)) != newPosn) { /* bad offset - negative or huge */ DBUG(("+++ bogus seek offset %ld\n", (long) newPosn)); errno = EINVAL; return (fpos_t) -1; } if (stream->offset < stream->eof) { /* * We were pointing to an area we'd already written to, which means * we stomped on a character and must now restore it. */ DBUG(("+++ restoring char '%c' at %d\n", stream->saved, stream->offset)); *(*stream->bufp + stream->offset) = stream->saved; } stream->offset = (size_t) newPosn; if (stream->offset < stream->eof) { /* * We're seeked backward into the stream. Preserve the character * at EOF and stomp it with a NUL. */ stream->saved = *(*stream->bufp + stream->offset); *(*stream->bufp + stream->offset) = '\0'; *stream->sizep = stream->offset; } else { /* * We're positioned at, or possibly beyond, the EOF. We want to * publish the current EOF, not the current position. */ *stream->sizep = stream->eof; } return newPosn; } /* * Close the memstream. We free everything but the data buffer. */ static int close_memstream(void* cookie) { free(cookie); return 0; } /* * Prepare a memstream. */ FILE* open_memstream(char** bufp, size_t* sizep) { FILE* fp; MemStream* stream; if (bufp == NULL || sizep == NULL) { errno = EINVAL; return NULL; } stream = (MemStream*) calloc(1, sizeof(MemStream)); if (stream == NULL) return NULL; fp = funopen(stream, NULL, write_memstream, seek_memstream, close_memstream); if (fp == NULL) { free(stream); return NULL; } *sizep = 0; *bufp = NULL; stream->bufp = bufp; stream->sizep = sizep; return fp; } #if 0 #define _GNU_SOURCE #include #include #include /* * Simple regression test. * * To test on desktop Linux with valgrind, it's possible to make a simple * change to open_memstream() to use fopencookie instead: * * cookie_io_functions_t iofuncs = * { NULL, write_memstream, seek_memstream, close_memstream }; * fp = fopencookie(stream, "w", iofuncs); * * (Some tweaks to seek_memstream are also required, as that takes a * pointer to an offset rather than an offset, and returns 0 or -1.) */ int testMemStream(void) { FILE *stream; char *buf; size_t len; off_t eob; printf("Test1\n"); /* std example */ stream = open_memstream(&buf, &len); fprintf(stream, "hello my world"); fflush(stream); printf("buf=%s, len=%zu\n", buf, len); eob = ftello(stream); fseeko(stream, 0, SEEK_SET); fprintf(stream, "good-bye"); fseeko(stream, eob, SEEK_SET); fclose(stream); printf("buf=%s, len=%zu\n", buf, len); free(buf); printf("Test2\n"); /* std example without final seek-to-end */ stream = open_memstream(&buf, &len); fprintf(stream, "hello my world"); fflush(stream); printf("buf=%s, len=%zu\n", buf, len); eob = ftello(stream); fseeko(stream, 0, SEEK_SET); fprintf(stream, "good-bye"); //fseeko(stream, eob, SEEK_SET); fclose(stream); printf("buf=%s, len=%zu\n", buf, len); free(buf); printf("Test3\n"); /* fancy example; should expand buffer with writes */ static const int kCmpLen = 1024 + 128; char* cmp = malloc(kCmpLen); memset(cmp, 0, 1024); memset(cmp+1024, 0xff, kCmpLen-1024); sprintf(cmp, "This-is-a-tes1234"); sprintf(cmp + 1022, "abcdef"); stream = open_memstream (&buf, &len); setvbuf(stream, NULL, _IONBF, 0); /* note: crashes in glibc with this */ fprintf(stream, "This-is-a-test"); fseek(stream, -1, SEEK_CUR); /* broken in glibc; can use {13,SEEK_SET} */ fprintf(stream, "1234"); fseek(stream, 1022, SEEK_SET); fputc('a', stream); fputc('b', stream); fputc('c', stream); fputc('d', stream); fputc('e', stream); fputc('f', stream); fflush(stream); if (memcmp(buf, cmp, len+1) != 0) { printf("mismatch\n"); } else { printf("match\n"); } printf("Test4\n"); stream = open_memstream (&buf, &len); fseek(stream, 5000, SEEK_SET); fseek(stream, 4096, SEEK_SET); fseek(stream, -1, SEEK_SET); /* should have no effect */ fputc('x', stream); if (ftell(stream) == 4097) printf("good\n"); else printf("BAD: offset is %ld\n", ftell(stream)); printf("DONE\n"); return 0; } /* expected output: Test1 buf=hello my world, len=14 buf=good-bye world, len=14 Test2 buf=hello my world, len=14 buf=good-bye, len=8 Test3 match Test4 good DONE */ #endif #endif /* __APPLE__ */