/* libs/cutils/strdup16to8.c ** ** Copyright 2006, The Android Open Source Project ** ** Licensed under the Apache License, Version 2.0 (the "License"); ** you may not use this file except in compliance with the License. ** You may obtain a copy of the License at ** ** http://www.apache.org/licenses/LICENSE-2.0 ** ** Unless required by applicable law or agreed to in writing, software ** distributed under the License is distributed on an "AS IS" BASIS, ** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. ** See the License for the specific language governing permissions and ** limitations under the License. */ #include /* for SIZE_MAX */ #include #include #include /** * Given a UTF-16 string, compute the length of the corresponding UTF-8 * string in bytes. */ extern size_t strnlen16to8(const char16_t* utf16Str, size_t len) { size_t utf8Len = 0; /* A small note on integer overflow. The result can * potentially be as big as 3*len, which will overflow * for len > SIZE_MAX/3. * * Moreover, the result of a strnlen16to8 is typically used * to allocate a destination buffer to strncpy16to8 which * requires one more byte to terminate the UTF-8 copy, and * this is generally done by careless users by incrementing * the result without checking for integer overflows, e.g.: * * dst = malloc(strnlen16to8(utf16,len)+1) * * Due to this, the following code will try to detect * overflows, and never return more than (SIZE_MAX-1) * when it detects one. A careless user will try to malloc * SIZE_MAX bytes, which will return NULL which can at least * be detected appropriately. * * As far as I know, this function is only used by strndup16(), * but better be safe than sorry. */ /* Fast path for the usual case where 3*len is < SIZE_MAX-1. */ if (len < (SIZE_MAX-1)/3) { while (len != 0) { len--; unsigned int uic = *utf16Str++; if (uic > 0x07ff) utf8Len += 3; else if (uic > 0x7f || uic == 0) utf8Len += 2; else utf8Len++; } return utf8Len; } /* The slower but paranoid version */ while (len != 0) { len--; unsigned int uic = *utf16Str++; size_t utf8Cur = utf8Len; if (uic > 0x07ff) utf8Len += 3; else if (uic > 0x7f || uic == 0) utf8Len += 2; else utf8Len++; if (utf8Len < utf8Cur) /* overflow detected */ return SIZE_MAX-1; } /* don't return SIZE_MAX to avoid common user bug */ if (utf8Len == SIZE_MAX) utf8Len = SIZE_MAX-1; return utf8Len; } /** * Convert a Java-Style UTF-16 string + length to a JNI-Style UTF-8 string. * * This basically means: embedded \0's in the UTF-16 string are encoded * as "0xc0 0x80" * * Make sure you allocate "utf8Str" with the result of strlen16to8() + 1, * not just "len". * * Please note, a terminated \0 is always added, so your result will always * be "strlen16to8() + 1" bytes long. */ extern char* strncpy16to8(char* utf8Str, const char16_t* utf16Str, size_t len) { char* utf8cur = utf8Str; /* Note on overflows: We assume the user did check the result of * strnlen16to8() properly or at a minimum checked the result of * its malloc(SIZE_MAX) in case of overflow. */ while (len != 0) { len--; unsigned int uic = *utf16Str++; if (uic > 0x07ff) { *utf8cur++ = (uic >> 12) | 0xe0; *utf8cur++ = ((uic >> 6) & 0x3f) | 0x80; *utf8cur++ = (uic & 0x3f) | 0x80; } else if (uic > 0x7f || uic == 0) { *utf8cur++ = (uic >> 6) | 0xc0; *utf8cur++ = (uic & 0x3f) | 0x80; } else { *utf8cur++ = uic; if (uic == 0) { break; } } } *utf8cur = '\0'; return utf8Str; } /** * Convert a UTF-16 string to UTF-8. * */ char * strndup16to8 (const char16_t* s, size_t n) { char* ret; size_t len; if (s == NULL) { return NULL; } len = strnlen16to8(s, n); /* We are paranoid, and we check for SIZE_MAX-1 * too since it is an overflow value for our * strnlen16to8 implementation. */ if (len >= SIZE_MAX-1) return NULL; ret = malloc(len + 1); if (ret == NULL) return NULL; strncpy16to8 (ret, s, n); return ret; }