/* * Copyright (C) 2012 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #define _FILE_OFFSET_BITS 64 #define _LARGEFILE64_SOURCE 1 #include #include #include #include #include #include #include #include #include #include #include #include "android-base/stringprintf.h" #include "defs.h" #include "output_file.h" #include "sparse_crc32.h" #include "sparse_file.h" #include "sparse_format.h" #if defined(__APPLE__) && defined(__MACH__) #define lseek64 lseek #define off64_t off_t #endif #define SPARSE_HEADER_MAJOR_VER 1 #define SPARSE_HEADER_LEN (sizeof(sparse_header_t)) #define CHUNK_HEADER_LEN (sizeof(chunk_header_t)) static constexpr int64_t COPY_BUF_SIZE = 1024 * 1024; static char* copybuf; static std::string ErrorString(int err) { if (err == -EOVERFLOW) return "EOF while reading file"; if (err == -EINVAL) return "Invalid sparse file format"; if (err == -ENOMEM) return "Failed allocation while reading file"; return android::base::StringPrintf("Unknown error %d", err); } class SparseFileSource { public: /* Seeks the source ahead by the given offset. */ virtual void Seek(int64_t offset) = 0; /* Return the current offset. */ virtual int64_t GetOffset() = 0; /* Set the current offset. Return 0 if successful. */ virtual int SetOffset(int64_t offset) = 0; /* Adds the given length from the current offset of the source to the file at the given block. * Return 0 if successful. */ virtual int AddToSparseFile(struct sparse_file* s, int64_t len, unsigned int block) = 0; /* Get data of fixed size from the current offset and seek len bytes. Return 0 if successful. */ virtual int ReadValue(void* ptr, int len) = 0; /* Find the crc32 of the next len bytes and seek ahead len bytes. Return 0 if successful. */ virtual int GetCrc32(uint32_t* crc32, int64_t len) = 0; virtual ~SparseFileSource(){}; }; class SparseFileFdSource : public SparseFileSource { private: int fd; public: SparseFileFdSource(int fd) : fd(fd) {} ~SparseFileFdSource() override {} void Seek(int64_t off) override { lseek64(fd, off, SEEK_CUR); } int64_t GetOffset() override { return lseek64(fd, 0, SEEK_CUR); } int SetOffset(int64_t offset) override { return lseek64(fd, offset, SEEK_SET) == offset ? 0 : -errno; } int AddToSparseFile(struct sparse_file* s, int64_t len, unsigned int block) override { return sparse_file_add_fd(s, fd, GetOffset(), len, block); } int ReadValue(void* ptr, int len) override { return read_all(fd, ptr, len); } int GetCrc32(uint32_t* crc32, int64_t len) override { int chunk; int ret; while (len) { chunk = std::min(len, COPY_BUF_SIZE); ret = read_all(fd, copybuf, chunk); if (ret < 0) { return ret; } *crc32 = sparse_crc32(*crc32, copybuf, chunk); len -= chunk; } return 0; } }; class SparseFileBufSource : public SparseFileSource { private: char* buf; int64_t offset; public: SparseFileBufSource(char* buf) : buf(buf), offset(0) {} ~SparseFileBufSource() override {} void Seek(int64_t off) override { buf += off; offset += off; } int64_t GetOffset() override { return offset; } int SetOffset(int64_t off) override { buf += off - offset; offset = off; return 0; } int AddToSparseFile(struct sparse_file* s, int64_t len, unsigned int block) override { return sparse_file_add_data(s, buf, len, block); } int ReadValue(void* ptr, int len) override { memcpy(ptr, buf, len); Seek(len); return 0; } int GetCrc32(uint32_t* crc32, int64_t len) override { *crc32 = sparse_crc32(*crc32, buf, len); Seek(len); return 0; } }; static void verbose_error(bool verbose, int err, const char* fmt, ...) { if (!verbose) return; std::string msg = ErrorString(err); if (fmt) { msg += " at "; va_list argp; va_start(argp, fmt); android::base::StringAppendV(&msg, fmt, argp); va_end(argp); } sparse_print_verbose("%s\n", msg.c_str()); } static int process_raw_chunk(struct sparse_file* s, unsigned int chunk_size, SparseFileSource* source, unsigned int blocks, unsigned int block, uint32_t* crc32) { int ret; int64_t len = blocks * s->block_size; if (chunk_size % s->block_size != 0) { return -EINVAL; } if (chunk_size / s->block_size != blocks) { return -EINVAL; } ret = source->AddToSparseFile(s, len, block); if (ret < 0) { return ret; } if (crc32) { ret = source->GetCrc32(crc32, len); if (ret < 0) { return ret; } } else { source->Seek(len); } return 0; } static int process_fill_chunk(struct sparse_file* s, unsigned int chunk_size, SparseFileSource* source, unsigned int blocks, unsigned int block, uint32_t* crc32) { int ret; int chunk; int64_t len = (int64_t)blocks * s->block_size; uint32_t fill_val; uint32_t* fillbuf; unsigned int i; if (chunk_size != sizeof(fill_val)) { return -EINVAL; } ret = source->ReadValue(&fill_val, sizeof(fill_val)); if (ret < 0) { return ret; } ret = sparse_file_add_fill(s, fill_val, len, block); if (ret < 0) { return ret; } if (crc32) { /* Fill copy_buf with the fill value */ fillbuf = (uint32_t*)copybuf; for (i = 0; i < (COPY_BUF_SIZE / sizeof(fill_val)); i++) { fillbuf[i] = fill_val; } while (len) { chunk = std::min(len, COPY_BUF_SIZE); *crc32 = sparse_crc32(*crc32, copybuf, chunk); len -= chunk; } } return 0; } static int process_skip_chunk(struct sparse_file* s, unsigned int chunk_size, SparseFileSource* source __unused, unsigned int blocks, unsigned int block __unused, uint32_t* crc32) { if (chunk_size != 0) { return -EINVAL; } if (crc32) { int64_t len = (int64_t)blocks * s->block_size; memset(copybuf, 0, COPY_BUF_SIZE); while (len) { int chunk = std::min(len, COPY_BUF_SIZE); *crc32 = sparse_crc32(*crc32, copybuf, chunk); len -= chunk; } } return 0; } static int process_crc32_chunk(SparseFileSource* source, unsigned int chunk_size, uint32_t* crc32) { uint32_t file_crc32; if (chunk_size != sizeof(file_crc32)) { return -EINVAL; } int ret = source->ReadValue(&file_crc32, sizeof(file_crc32)); if (ret < 0) { return ret; } if (crc32 != NULL && file_crc32 != *crc32) { return -EINVAL; } return 0; } static int process_chunk(struct sparse_file* s, SparseFileSource* source, unsigned int chunk_hdr_sz, chunk_header_t* chunk_header, unsigned int cur_block, uint32_t* crc_ptr) { int ret; unsigned int chunk_data_size; int64_t offset = source->GetOffset(); chunk_data_size = chunk_header->total_sz - chunk_hdr_sz; switch (chunk_header->chunk_type) { case CHUNK_TYPE_RAW: ret = process_raw_chunk(s, chunk_data_size, source, chunk_header->chunk_sz, cur_block, crc_ptr); if (ret < 0) { verbose_error(s->verbose, ret, "data block at %" PRId64, offset); return ret; } return chunk_header->chunk_sz; case CHUNK_TYPE_FILL: ret = process_fill_chunk(s, chunk_data_size, source, chunk_header->chunk_sz, cur_block, crc_ptr); if (ret < 0) { verbose_error(s->verbose, ret, "fill block at %" PRId64, offset); return ret; } return chunk_header->chunk_sz; case CHUNK_TYPE_DONT_CARE: ret = process_skip_chunk(s, chunk_data_size, source, chunk_header->chunk_sz, cur_block, crc_ptr); if (chunk_data_size != 0) { if (ret < 0) { verbose_error(s->verbose, ret, "skip block at %" PRId64, offset); return ret; } } return chunk_header->chunk_sz; case CHUNK_TYPE_CRC32: ret = process_crc32_chunk(source, chunk_data_size, crc_ptr); if (ret < 0) { verbose_error(s->verbose, -EINVAL, "crc block at %" PRId64, offset); return ret; } return 0; default: verbose_error(s->verbose, -EINVAL, "unknown block %04X at %" PRId64, chunk_header->chunk_type, offset); } return 0; } static int sparse_file_read_sparse(struct sparse_file* s, SparseFileSource* source, bool crc) { int ret; unsigned int i; sparse_header_t sparse_header; chunk_header_t chunk_header; uint32_t crc32 = 0; uint32_t* crc_ptr = 0; unsigned int cur_block = 0; if (!copybuf) { copybuf = (char*)malloc(COPY_BUF_SIZE); } if (!copybuf) { return -ENOMEM; } if (crc) { crc_ptr = &crc32; } ret = source->ReadValue(&sparse_header, sizeof(sparse_header)); if (ret < 0) { return ret; } if (sparse_header.magic != SPARSE_HEADER_MAGIC) { return -EINVAL; } if (sparse_header.major_version != SPARSE_HEADER_MAJOR_VER) { return -EINVAL; } if (sparse_header.file_hdr_sz < SPARSE_HEADER_LEN) { return -EINVAL; } if (sparse_header.chunk_hdr_sz < sizeof(chunk_header)) { return -EINVAL; } if (sparse_header.file_hdr_sz > SPARSE_HEADER_LEN) { /* Skip the remaining bytes in a header that is longer than * we expected. */ source->Seek(sparse_header.file_hdr_sz - SPARSE_HEADER_LEN); } for (i = 0; i < sparse_header.total_chunks; i++) { ret = source->ReadValue(&chunk_header, sizeof(chunk_header)); if (ret < 0) { return ret; } if (sparse_header.chunk_hdr_sz > CHUNK_HEADER_LEN) { /* Skip the remaining bytes in a header that is longer than * we expected. */ source->Seek(sparse_header.chunk_hdr_sz - CHUNK_HEADER_LEN); } ret = process_chunk(s, source, sparse_header.chunk_hdr_sz, &chunk_header, cur_block, crc_ptr); if (ret < 0) { return ret; } cur_block += ret; } if (sparse_header.total_blks != cur_block) { return -EINVAL; } return 0; } static int sparse_file_read_normal(struct sparse_file* s, int fd) { int ret; uint32_t* buf = (uint32_t*)malloc(s->block_size); unsigned int block = 0; int64_t remain = s->len; int64_t offset = 0; unsigned int to_read; unsigned int i; bool sparse_block; if (!buf) { return -ENOMEM; } while (remain > 0) { to_read = std::min(remain, (int64_t)(s->block_size)); ret = read_all(fd, buf, to_read); if (ret < 0) { error("failed to read sparse file"); free(buf); return ret; } if (to_read == s->block_size) { sparse_block = true; for (i = 1; i < s->block_size / sizeof(uint32_t); i++) { if (buf[0] != buf[i]) { sparse_block = false; break; } } } else { sparse_block = false; } if (sparse_block) { /* TODO: add flag to use skip instead of fill for buf[0] == 0 */ sparse_file_add_fill(s, buf[0], to_read, block); } else { sparse_file_add_fd(s, fd, offset, to_read, block); } remain -= to_read; offset += to_read; block++; } free(buf); return 0; } int sparse_file_read(struct sparse_file* s, int fd, bool sparse, bool crc) { if (crc && !sparse) { return -EINVAL; } if (sparse) { SparseFileFdSource source(fd); return sparse_file_read_sparse(s, &source, crc); } else { return sparse_file_read_normal(s, fd); } } int sparse_file_read_buf(struct sparse_file* s, char* buf, bool crc) { SparseFileBufSource source(buf); return sparse_file_read_sparse(s, &source, crc); } static struct sparse_file* sparse_file_import_source(SparseFileSource* source, bool verbose, bool crc) { int ret; sparse_header_t sparse_header; int64_t len; struct sparse_file* s; ret = source->ReadValue(&sparse_header, sizeof(sparse_header)); if (ret < 0) { verbose_error(verbose, ret, "header"); return NULL; } if (sparse_header.magic != SPARSE_HEADER_MAGIC) { verbose_error(verbose, -EINVAL, "header magic"); return NULL; } if (sparse_header.major_version != SPARSE_HEADER_MAJOR_VER) { verbose_error(verbose, -EINVAL, "header major version"); return NULL; } if (sparse_header.file_hdr_sz < SPARSE_HEADER_LEN) { return NULL; } if (sparse_header.chunk_hdr_sz < sizeof(chunk_header_t)) { return NULL; } len = (int64_t)sparse_header.total_blks * sparse_header.blk_sz; s = sparse_file_new(sparse_header.blk_sz, len); if (!s) { verbose_error(verbose, -EINVAL, NULL); return NULL; } ret = source->SetOffset(0); if (ret < 0) { verbose_error(verbose, ret, "seeking"); sparse_file_destroy(s); return NULL; } s->verbose = verbose; ret = sparse_file_read_sparse(s, source, crc); if (ret < 0) { sparse_file_destroy(s); return NULL; } return s; } struct sparse_file* sparse_file_import(int fd, bool verbose, bool crc) { SparseFileFdSource source(fd); return sparse_file_import_source(&source, verbose, crc); } struct sparse_file* sparse_file_import_buf(char* buf, bool verbose, bool crc) { SparseFileBufSource source(buf); return sparse_file_import_source(&source, verbose, crc); } struct sparse_file* sparse_file_import_auto(int fd, bool crc, bool verbose) { struct sparse_file* s; int64_t len; int ret; s = sparse_file_import(fd, verbose, crc); if (s) { return s; } len = lseek64(fd, 0, SEEK_END); if (len < 0) { return NULL; } lseek64(fd, 0, SEEK_SET); s = sparse_file_new(4096, len); if (!s) { return NULL; } ret = sparse_file_read_normal(s, fd); if (ret < 0) { sparse_file_destroy(s); return NULL; } return s; }