/* * Copyright (C) 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #include #include #include #include #include "MemoryFake.h" namespace unwindstack { class MockDwarfSection : public DwarfSection { public: MockDwarfSection(Memory* memory) : DwarfSection(memory) {} virtual ~MockDwarfSection() = default; MOCK_METHOD3(Init, bool(uint64_t, uint64_t, uint64_t)); MOCK_METHOD5(Eval, bool(const DwarfCie*, Memory*, const dwarf_loc_regs_t&, Regs*, bool*)); MOCK_METHOD3(Log, bool(uint8_t, uint64_t, const DwarfFde*)); MOCK_METHOD1(GetFdes, void(std::vector*)); MOCK_METHOD1(GetFdeFromPc, const DwarfFde*(uint64_t)); MOCK_METHOD3(GetCfaLocationInfo, bool(uint64_t, const DwarfFde*, dwarf_loc_regs_t*)); MOCK_METHOD1(GetCieOffsetFromFde32, uint64_t(uint32_t)); MOCK_METHOD1(GetCieOffsetFromFde64, uint64_t(uint64_t)); MOCK_METHOD1(AdjustPcFromFde, uint64_t(uint64_t)); }; class DwarfSectionTest : public ::testing::Test { protected: void SetUp() override { section_.reset(new MockDwarfSection(&memory_)); } MemoryFake memory_; std::unique_ptr section_; }; TEST_F(DwarfSectionTest, Step_fail_fde) { EXPECT_CALL(*section_, GetFdeFromPc(0x1000)).WillOnce(::testing::Return(nullptr)); bool finished; ASSERT_FALSE(section_->Step(0x1000, nullptr, nullptr, &finished)); } TEST_F(DwarfSectionTest, Step_fail_cie_null) { DwarfFde fde{}; fde.pc_end = 0x2000; fde.cie = nullptr; EXPECT_CALL(*section_, GetFdeFromPc(0x1000)).WillOnce(::testing::Return(&fde)); bool finished; ASSERT_FALSE(section_->Step(0x1000, nullptr, nullptr, &finished)); } TEST_F(DwarfSectionTest, Step_fail_cfa_location) { DwarfCie cie{}; DwarfFde fde{}; fde.pc_end = 0x2000; fde.cie = &cie; EXPECT_CALL(*section_, GetFdeFromPc(0x1000)).WillOnce(::testing::Return(&fde)); EXPECT_CALL(*section_, GetCfaLocationInfo(0x1000, &fde, ::testing::_)) .WillOnce(::testing::Return(false)); bool finished; ASSERT_FALSE(section_->Step(0x1000, nullptr, nullptr, &finished)); } TEST_F(DwarfSectionTest, Step_pass) { DwarfCie cie{}; DwarfFde fde{}; fde.pc_end = 0x2000; fde.cie = &cie; EXPECT_CALL(*section_, GetFdeFromPc(0x1000)).WillOnce(::testing::Return(&fde)); EXPECT_CALL(*section_, GetCfaLocationInfo(0x1000, &fde, ::testing::_)) .WillOnce(::testing::Return(true)); MemoryFake process; EXPECT_CALL(*section_, Eval(&cie, &process, ::testing::_, nullptr, ::testing::_)) .WillOnce(::testing::Return(true)); bool finished; ASSERT_TRUE(section_->Step(0x1000, nullptr, &process, &finished)); } static bool MockGetCfaLocationInfo(::testing::Unused, const DwarfFde* fde, dwarf_loc_regs_t* loc_regs) { loc_regs->pc_start = fde->pc_start; loc_regs->pc_end = fde->pc_end; return true; } TEST_F(DwarfSectionTest, Step_cache) { DwarfCie cie{}; DwarfFde fde{}; fde.pc_start = 0x500; fde.pc_end = 0x2000; fde.cie = &cie; EXPECT_CALL(*section_, GetFdeFromPc(0x1000)).WillOnce(::testing::Return(&fde)); EXPECT_CALL(*section_, GetCfaLocationInfo(0x1000, &fde, ::testing::_)) .WillOnce(::testing::Invoke(MockGetCfaLocationInfo)); MemoryFake process; EXPECT_CALL(*section_, Eval(&cie, &process, ::testing::_, nullptr, ::testing::_)) .WillRepeatedly(::testing::Return(true)); bool finished; ASSERT_TRUE(section_->Step(0x1000, nullptr, &process, &finished)); ASSERT_TRUE(section_->Step(0x1000, nullptr, &process, &finished)); ASSERT_TRUE(section_->Step(0x1500, nullptr, &process, &finished)); } TEST_F(DwarfSectionTest, Step_cache_not_in_pc) { DwarfCie cie{}; DwarfFde fde0{}; fde0.pc_start = 0x1000; fde0.pc_end = 0x2000; fde0.cie = &cie; EXPECT_CALL(*section_, GetFdeFromPc(0x1000)).WillOnce(::testing::Return(&fde0)); EXPECT_CALL(*section_, GetCfaLocationInfo(0x1000, &fde0, ::testing::_)) .WillOnce(::testing::Invoke(MockGetCfaLocationInfo)); MemoryFake process; EXPECT_CALL(*section_, Eval(&cie, &process, ::testing::_, nullptr, ::testing::_)) .WillRepeatedly(::testing::Return(true)); bool finished; ASSERT_TRUE(section_->Step(0x1000, nullptr, &process, &finished)); DwarfFde fde1{}; fde1.pc_start = 0x500; fde1.pc_end = 0x800; fde1.cie = &cie; EXPECT_CALL(*section_, GetFdeFromPc(0x600)).WillOnce(::testing::Return(&fde1)); EXPECT_CALL(*section_, GetCfaLocationInfo(0x600, &fde1, ::testing::_)) .WillOnce(::testing::Invoke(MockGetCfaLocationInfo)); ASSERT_TRUE(section_->Step(0x600, nullptr, &process, &finished)); ASSERT_TRUE(section_->Step(0x700, nullptr, &process, &finished)); } } // namespace unwindstack