/* * Copyright (C) 2008 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ /* * System clock functions. */ #ifdef HAVE_ANDROID_OS #include #include #include #include #endif #include #include #include #include #include #include #include #define LOG_TAG "SystemClock" #include namespace android { /* * native public static long uptimeMillis(); */ int64_t uptimeMillis() { int64_t when = systemTime(SYSTEM_TIME_MONOTONIC); return (int64_t) nanoseconds_to_milliseconds(when); } /* * native public static long elapsedRealtime(); */ int64_t elapsedRealtime() { return nanoseconds_to_milliseconds(elapsedRealtimeNano()); } #define METHOD_CLOCK_GETTIME 0 #define METHOD_IOCTL 1 #define METHOD_SYSTEMTIME 2 /* * To debug/verify the timestamps returned by the kernel, change * DEBUG_TIMESTAMP to 1 and call the timestamp routine from a single thread * in the test program. b/10899829 */ #define DEBUG_TIMESTAMP 0 #if DEBUG_TIMESTAMP && defined(__arm__) static inline void checkTimeStamps(int64_t timestamp, int64_t volatile *prevTimestampPtr, int volatile *prevMethodPtr, int curMethod) { /* * Disable the check for SDK since the prebuilt toolchain doesn't contain * gettid, and int64_t is different on the ARM platform * (ie long vs long long). */ int64_t prevTimestamp = *prevTimestampPtr; int prevMethod = *prevMethodPtr; if (timestamp < prevTimestamp) { static const char *gettime_method_names[] = { "clock_gettime", "ioctl", "systemTime", }; ALOGW("time going backwards: prev %lld(%s) vs now %lld(%s), tid=%d", prevTimestamp, gettime_method_names[prevMethod], timestamp, gettime_method_names[curMethod], gettid()); } // NOTE - not atomic and may generate spurious warnings if the 64-bit // write is interrupted or not observed as a whole. *prevTimestampPtr = timestamp; *prevMethodPtr = curMethod; } #else #define checkTimeStamps(timestamp, prevTimestampPtr, prevMethodPtr, curMethod) #endif /* * native public static long elapsedRealtimeNano(); */ int64_t elapsedRealtimeNano() { #ifdef HAVE_ANDROID_OS struct timespec ts; int result; int64_t timestamp; #if DEBUG_TIMESTAMP static volatile int64_t prevTimestamp; static volatile int prevMethod; #endif static int s_fd = -1; if (s_fd == -1) { int fd = open("/dev/alarm", O_RDONLY); if (android_atomic_cmpxchg(-1, fd, &s_fd)) { close(fd); } } result = ioctl(s_fd, ANDROID_ALARM_GET_TIME(ANDROID_ALARM_ELAPSED_REALTIME), &ts); if (result == 0) { timestamp = seconds_to_nanoseconds(ts.tv_sec) + ts.tv_nsec; checkTimeStamps(timestamp, &prevTimestamp, &prevMethod, METHOD_IOCTL); return timestamp; } // /dev/alarm doesn't exist, fallback to CLOCK_BOOTTIME result = clock_gettime(CLOCK_BOOTTIME, &ts); if (result == 0) { timestamp = seconds_to_nanoseconds(ts.tv_sec) + ts.tv_nsec; checkTimeStamps(timestamp, &prevTimestamp, &prevMethod, METHOD_CLOCK_GETTIME); return timestamp; } // XXX: there was an error, probably because the driver didn't // exist ... this should return // a real error, like an exception! timestamp = systemTime(SYSTEM_TIME_MONOTONIC); checkTimeStamps(timestamp, &prevTimestamp, &prevMethod, METHOD_SYSTEMTIME); return timestamp; #else return systemTime(SYSTEM_TIME_MONOTONIC); #endif } }; // namespace android