/* * Copyright (C) 2007 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef _LIBS_UTILS_ANDROID_THREADS_H #define _LIBS_UTILS_ANDROID_THREADS_H #include #include #if !defined(_WIN32) # include #endif #include // --------------------------------------------------------------------------- // C API #ifdef __cplusplus extern "C" { #endif // Create and run a new thread. extern int androidCreateThread(android_thread_func_t, void *); // Create thread with lots of parameters extern int androidCreateThreadEtc(android_thread_func_t entryFunction, void *userData, const char* threadName, int32_t threadPriority, size_t threadStackSize, android_thread_id_t *threadId); // Get some sort of unique identifier for the current thread. extern android_thread_id_t androidGetThreadId(); // Low-level thread creation -- never creates threads that can // interact with the Java VM. extern int androidCreateRawThreadEtc(android_thread_func_t entryFunction, void *userData, const char* threadName, int32_t threadPriority, size_t threadStackSize, android_thread_id_t *threadId); // set the same of the running thread extern void androidSetThreadName(const char* name); // Used by the Java Runtime to control how threads are created, so that // they can be proper and lovely Java threads. typedef int (*android_create_thread_fn)(android_thread_func_t entryFunction, void *userData, const char* threadName, int32_t threadPriority, size_t threadStackSize, android_thread_id_t *threadId); extern void androidSetCreateThreadFunc(android_create_thread_fn func); // ------------------------------------------------------------------ // Extra functions working with raw pids. #if defined(__ANDROID__) // Change the priority AND scheduling group of a particular thread. The priority // should be one of the ANDROID_PRIORITY constants. Returns INVALID_OPERATION // if the priority set failed, else another value if just the group set failed; // in either case errno is set. Thread ID zero means current thread. extern int androidSetThreadPriority(pid_t tid, int prio); // Get the current priority of a particular thread. Returns one of the // ANDROID_PRIORITY constants or a negative result in case of error. extern int androidGetThreadPriority(pid_t tid); #endif #ifdef __cplusplus } // extern "C" #endif // ---------------------------------------------------------------------------- // C++ API #ifdef __cplusplus namespace android { // ---------------------------------------------------------------------------- // Create and run a new thread. inline bool createThread(thread_func_t f, void *a) { return androidCreateThread(f, a) ? true : false; } // Create thread with lots of parameters inline bool createThreadEtc(thread_func_t entryFunction, void *userData, const char* threadName = "android:unnamed_thread", int32_t threadPriority = PRIORITY_DEFAULT, size_t threadStackSize = 0, thread_id_t *threadId = nullptr) { return androidCreateThreadEtc(entryFunction, userData, threadName, threadPriority, threadStackSize, threadId) ? true : false; } // Get some sort of unique identifier for the current thread. inline thread_id_t getThreadId() { return androidGetThreadId(); } // ---------------------------------------------------------------------------- } // namespace android #endif // __cplusplus // ---------------------------------------------------------------------------- #endif // _LIBS_UTILS_ANDROID_THREADS_H