/* * Copyright (C) 2012-2013 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef _LOGD_LOG_LISTENER_H__ #define _LOGD_LOG_LISTENER_H__ #include #include "LogReader.h" // DEFAULT_OVERFLOWUID is defined in linux/highuid.h, which is not part of // the uapi headers for userspace to use. This value is filled in on the // out-of-band socket credentials if the OS fails to find one available. // One of the causes of this is if SO_PASSCRED is set, all the packets before // that point will have this value. We also use it in a fake credential if // no socket credentials are supplied. #ifndef DEFAULT_OVERFLOWUID #define DEFAULT_OVERFLOWUID 65534 #endif class LogListener : public SocketListener { LogBufferInterface* logbuf; LogReader* reader; public: LogListener(LogBufferInterface* buf, LogReader* reader /* nullable */); protected: virtual bool onDataAvailable(SocketClient* cli); private: static int getLogSocket(); }; #endif