/* system/core/include/logwrap/logwrap.h * * Copyright 2013, The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #ifndef __LIBS_LOGWRAP_H #define __LIBS_LOGWRAP_H #include __BEGIN_DECLS /* * Run a command while logging its stdout and stderr * * WARNING: while this function is running it will clear all SIGCHLD handlers * if you rely on SIGCHLD in the caller there is a chance zombies will be * created if you're not calling waitpid after calling this. This function will * log a warning when it clears SIGCHLD for processes other than the child it * created. * * Arguments: * argc: the number of elements in argv * argv: an array of strings containing the command to be executed and its * arguments as separate strings. argv does not need to be * NULL-terminated * status: the equivalent child status as populated by wait(status). This * value is only valid when logwrap successfully completes. If NULL * the return value of the child will be the function's return value. * ignore_int_quit: set to true if you want to completely ignore SIGINT and * SIGQUIT while logwrap is running. This may force the end-user to * send a signal twice to signal the caller (once for the child, and * once for the caller) * log_target: Specify where to log the output of the child, either LOG_NONE, * LOG_ALOG (for the Android system log) or LOG_KLOG (for the kernel * log). * abbreviated: If true, capture up to the first 100 lines and last 4K of * output from the child. The abbreviated output is not dumped to * the specified log until the child has exited. * * Return value: * 0 when logwrap successfully run the child process and captured its status * -1 when an internal error occurred * -ECHILD if status is NULL and the child didn't exit properly * the return value of the child if it exited properly and status is NULL * */ /* Values for the log_target parameter android_fork_exec_ext() */ #define LOG_NONE 0 #define LOG_ALOG 1 #define LOG_KLOG 2 int android_fork_execvp_ext(int argc, char* argv[], int *status, bool ignore_int_quit, int log_target, bool abbreviated); /* Similar to above, except abbreviated logging is not available, and if logwrap * is true, logging is to the Android system log, and if false, there is no * logging. */ static inline int android_fork_execvp(int argc, char* argv[], int *status, bool ignore_int_quit, bool logwrap) { return android_fork_execvp_ext(argc, argv, status, ignore_int_quit, (logwrap ? LOG_ALOG : LOG_NONE), false); } __END_DECLS #endif /* __LIBS_LOGWRAP_H */