# The entries in this file map a sparse set of log tag numbers to tag names. # This is installed on the device, in /system/etc, and parsed by logcat. # # Tag numbers are decimal integers, from 0 to 2^31. (Let's leave the # negative values alone for now.) # # Tag names are one or more ASCII letters and numbers or underscores, i.e. # "[A-Z][a-z][0-9]_". Do not include spaces or punctuation (the former # impacts log readability, the latter makes regex searches more annoying). # # Tag numbers and names are separated by whitespace. Blank lines and lines # starting with '#' are ignored. # # Optionally, after the tag names can be put a description for the value(s) # of the tag. Description are in the format # (|data type[|data unit]) # Multiple values are separated by commas. # # The data type is a number from the following values: # 1: int # 2: long # 3: string # 4: list # 5: float # # The data unit is a number taken from the following list: # 1: Number of objects # 2: Number of bytes # 3: Number of milliseconds # 4: Number of allocations # 5: Id # 6: Percent # Default value for data of type int/long is 2 (bytes). # # TODO: generate ".java" and ".h" files with integer constants from this file. 2732 storaged_disk_stats (type|3),(start_time|2|3),(end_time|2|3),(read_ios|2|1),(read_merges|2|1),(read_sectors|2|1),(read_ticks|2|3),(write_ios|2|1),(write_merges|2|1),(write_sectors|2|1),(write_ticks|2|3),(o_in_flight|2|1),(io_ticks|2|3),(io_in_queue|2|1) 2733 storaged_emmc_info (mmc_ver|3),(eol|1),(lifetime_a|1),(lifetime_b|1)