1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
|
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <errno.h>
#include <limits.h>
#include <stdarg.h>
#include <zipfile/zipfile.h>
#include <sys/types.h>
#include <sys/stat.h>
#include "sysdeps.h"
#define TRACE_TAG TRACE_ADB
#include "adb_client.h"
static transport_type __adb_transport = kTransportAny;
static const char* __adb_serial = NULL;
static int __adb_server_port = DEFAULT_ADB_PORT;
void adb_set_transport(transport_type type, const char* serial)
{
__adb_transport = type;
__adb_serial = serial;
}
void adb_set_tcp_specifics(int server_port)
{
__adb_server_port = server_port;
}
int adb_get_emulator_console_port(void)
{
const char* serial = __adb_serial;
int port;
if (serial == NULL) {
/* if no specific device was specified, we need to look at */
/* the list of connected devices, and extract an emulator */
/* name from it. two emulators is an error */
char* tmp = adb_query("host:devices");
char* p = tmp;
if(!tmp) {
printf("no emulator connected\n");
return -1;
}
while (*p) {
char* q = strchr(p, '\n');
if (q != NULL)
*q++ = 0;
else
q = p + strlen(p);
if (!memcmp(p, LOCAL_CLIENT_PREFIX, sizeof(LOCAL_CLIENT_PREFIX)-1)) {
if (serial != NULL) { /* more than one emulator listed */
free(tmp);
return -2;
}
serial = p;
}
p = q;
}
free(tmp);
if (serial == NULL)
return -1; /* no emulator found */
}
else {
if (memcmp(serial, LOCAL_CLIENT_PREFIX, sizeof(LOCAL_CLIENT_PREFIX)-1) != 0)
return -1; /* not an emulator */
}
serial += sizeof(LOCAL_CLIENT_PREFIX)-1;
port = strtol(serial, NULL, 10);
return port;
}
static char __adb_error[256] = { 0 };
const char *adb_error(void)
{
return __adb_error;
}
static int switch_socket_transport(int fd)
{
char service[64];
char tmp[5];
int len;
if (__adb_serial)
snprintf(service, sizeof service, "host:transport:%s", __adb_serial);
else {
char* transport_type = "???";
switch (__adb_transport) {
case kTransportUsb:
transport_type = "transport-usb";
break;
case kTransportLocal:
transport_type = "transport-local";
break;
case kTransportAny:
transport_type = "transport-any";
break;
case kTransportHost:
// no switch necessary
return 0;
break;
}
snprintf(service, sizeof service, "host:%s", transport_type);
}
len = strlen(service);
snprintf(tmp, sizeof tmp, "%04x", len);
if(writex(fd, tmp, 4) || writex(fd, service, len)) {
strcpy(__adb_error, "write failure during connection");
adb_close(fd);
return -1;
}
D("Switch transport in progress\n");
if(adb_status(fd)) {
adb_close(fd);
D("Switch transport failed\n");
return -1;
}
D("Switch transport success\n");
return 0;
}
int adb_status(int fd)
{
unsigned char buf[5];
unsigned len;
if(readx(fd, buf, 4)) {
strcpy(__adb_error, "protocol fault (no status)");
return -1;
}
if(!memcmp(buf, "OKAY", 4)) {
return 0;
}
if(memcmp(buf, "FAIL", 4)) {
sprintf(__adb_error,
"protocol fault (status %02x %02x %02x %02x?!)",
buf[0], buf[1], buf[2], buf[3]);
return -1;
}
if(readx(fd, buf, 4)) {
strcpy(__adb_error, "protocol fault (status len)");
return -1;
}
buf[4] = 0;
len = strtoul((char*)buf, 0, 16);
if(len > 255) len = 255;
if(readx(fd, __adb_error, len)) {
strcpy(__adb_error, "protocol fault (status read)");
return -1;
}
__adb_error[len] = 0;
return -1;
}
int _adb_connect(const char *service)
{
char tmp[5];
int len;
int fd;
D("_adb_connect: %s\n", service);
len = strlen(service);
if((len < 1) || (len > 1024)) {
strcpy(__adb_error, "service name too long");
return -1;
}
snprintf(tmp, sizeof tmp, "%04x", len);
fd = socket_loopback_client(__adb_server_port, SOCK_STREAM);
if(fd < 0) {
strcpy(__adb_error, "cannot connect to daemon");
return -2;
}
if (memcmp(service,"host",4) != 0 && switch_socket_transport(fd)) {
return -1;
}
if(writex(fd, tmp, 4) || writex(fd, service, len)) {
strcpy(__adb_error, "write failure during connection");
adb_close(fd);
return -1;
}
if(adb_status(fd)) {
adb_close(fd);
return -1;
}
D("_adb_connect: return fd %d\n", fd);
return fd;
}
int adb_connect(const char *service)
{
// first query the adb server's version
int fd = _adb_connect("host:version");
D("adb_connect: service %s\n", service);
if(fd == -2) {
fprintf(stdout,"* daemon not running. starting it now on port %d *\n",
__adb_server_port);
start_server:
if(launch_server(__adb_server_port)) {
fprintf(stderr,"* failed to start daemon *\n");
return -1;
} else {
fprintf(stdout,"* daemon started successfully *\n");
}
/* give the server some time to start properly and detect devices */
adb_sleep_ms(3000);
// fall through to _adb_connect
} else {
// if server was running, check its version to make sure it is not out of date
char buf[100];
size_t n;
int version = ADB_SERVER_VERSION - 1;
// if we have a file descriptor, then parse version result
if(fd >= 0) {
if(readx(fd, buf, 4)) goto error;
buf[4] = 0;
n = strtoul(buf, 0, 16);
if(n > sizeof(buf)) goto error;
if(readx(fd, buf, n)) goto error;
adb_close(fd);
if (sscanf(buf, "%04x", &version) != 1) goto error;
} else {
// if fd is -1, then check for "unknown host service",
// which would indicate a version of adb that does not support the version command
if (strcmp(__adb_error, "unknown host service") != 0)
return fd;
}
if(version != ADB_SERVER_VERSION) {
printf("adb server is out of date. killing...\n");
fd = _adb_connect("host:kill");
adb_close(fd);
/* XXX can we better detect its death? */
adb_sleep_ms(2000);
goto start_server;
}
}
// if the command is start-server, we are done.
if (!strcmp(service, "host:start-server"))
return 0;
fd = _adb_connect(service);
if(fd == -2) {
fprintf(stderr,"** daemon still not running");
}
D("adb_connect: return fd %d\n", fd);
return fd;
error:
adb_close(fd);
return -1;
}
int adb_command(const char *service)
{
int fd = adb_connect(service);
if(fd < 0) {
return -1;
}
if(adb_status(fd)) {
adb_close(fd);
return -1;
}
return 0;
}
char *adb_query(const char *service)
{
char buf[5];
unsigned n;
char *tmp;
D("adb_query: %s\n", service);
int fd = adb_connect(service);
if(fd < 0) {
fprintf(stderr,"error: %s\n", __adb_error);
return 0;
}
if(readx(fd, buf, 4)) goto oops;
buf[4] = 0;
n = strtoul(buf, 0, 16);
if(n > 1024) goto oops;
tmp = malloc(n + 1);
if(tmp == 0) goto oops;
if(readx(fd, tmp, n) == 0) {
tmp[n] = 0;
adb_close(fd);
return tmp;
}
free(tmp);
oops:
adb_close(fd);
return 0;
}
|