summaryrefslogtreecommitdiffstats
blob: f5d0f02df59bbef160df4c47c19414e5d76bd4ed (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#define TRACE_TAG ADB

#include "sysdeps.h"
#include "adb_client.h"

#include <errno.h>
#include <limits.h>
#include <stdarg.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/stat.h>
#include <sys/types.h>

#include <condition_variable>
#include <mutex>
#include <string>
#include <thread>
#include <vector>

#include <android-base/stringprintf.h>
#include <android-base/strings.h>
#include <android-base/thread_annotations.h>
#include <cutils/sockets.h>

#include "adb_io.h"
#include "adb_utils.h"
#include "socket_spec.h"
#include "sysdeps/chrono.h"

static TransportType __adb_transport = kTransportAny;
static const char* __adb_serial = NULL;

static const char* __adb_server_socket_spec;

void adb_set_transport(TransportType type, const char* serial) {
    __adb_transport = type;
    __adb_serial = serial;
}

void adb_set_socket_spec(const char* socket_spec) {
    if (__adb_server_socket_spec) {
        LOG(FATAL) << "attempted to reinitialize adb_server_socket_spec " << socket_spec << " (was " << __adb_server_socket_spec << ")";
    }
    __adb_server_socket_spec = socket_spec;
}

static int switch_socket_transport(int fd, std::string* error) {
    std::string service;
    if (__adb_serial) {
        service += "host:transport:";
        service += __adb_serial;
    } else {
        const char* transport_type = "???";
        switch (__adb_transport) {
          case kTransportUsb:
            transport_type = "transport-usb";
            break;
          case kTransportLocal:
            transport_type = "transport-local";
            break;
          case kTransportAny:
            transport_type = "transport-any";
            break;
          case kTransportHost:
            // no switch necessary
            return 0;
        }
        service += "host:";
        service += transport_type;
    }

    if (!SendProtocolString(fd, service)) {
        *error = perror_str("write failure during connection");
        adb_close(fd);
        return -1;
    }
    D("Switch transport in progress");

    if (!adb_status(fd, error)) {
        adb_close(fd);
        D("Switch transport failed: %s", error->c_str());
        return -1;
    }
    D("Switch transport success");
    return 0;
}

bool adb_status(int fd, std::string* error) {
    char buf[5];
    if (!ReadFdExactly(fd, buf, 4)) {
        *error = perror_str("protocol fault (couldn't read status)");
        return false;
    }

    if (!memcmp(buf, "OKAY", 4)) {
        return true;
    }

    if (memcmp(buf, "FAIL", 4)) {
        *error = android::base::StringPrintf("protocol fault (status %02x %02x %02x %02x?!)",
                                             buf[0], buf[1], buf[2], buf[3]);
        return false;
    }

    ReadProtocolString(fd, error, error);
    return false;
}

static int _adb_connect(const std::string& service, std::string* error) {
    D("_adb_connect: %s", service.c_str());
    if (service.empty() || service.size() > MAX_PAYLOAD_V1) {
        *error = android::base::StringPrintf("bad service name length (%zd)",
                                             service.size());
        return -1;
    }

    std::string reason;
    int fd = socket_spec_connect(__adb_server_socket_spec, &reason);
    if (fd < 0) {
        *error = android::base::StringPrintf("cannot connect to daemon at %s: %s",
                                             __adb_server_socket_spec, reason.c_str());
        return -2;
    }

    if (memcmp(&service[0], "host", 4) != 0 && switch_socket_transport(fd, error)) {
        return -1;
    }

    if (!SendProtocolString(fd, service)) {
        *error = perror_str("write failure during connection");
        adb_close(fd);
        return -1;
    }

    if (!adb_status(fd, error)) {
        adb_close(fd);
        return -1;
    }

    D("_adb_connect: return fd %d", fd);
    return fd;
}

bool adb_kill_server() {
    D("adb_kill_server");
    std::string reason;
    int fd = socket_spec_connect(__adb_server_socket_spec, &reason);
    if (fd < 0) {
        fprintf(stderr, "cannot connect to daemon at %s: %s\n", __adb_server_socket_spec,
                reason.c_str());
        return true;
    }

    if (!SendProtocolString(fd, "host:kill")) {
        fprintf(stderr, "error: write failure during connection: %s\n", strerror(errno));
        return false;
    }

    ReadOrderlyShutdown(fd);
    return true;
}

int adb_connect(const std::string& service, std::string* error) {
    // first query the adb server's version
    int fd = _adb_connect("host:version", error);

    D("adb_connect: service %s", service.c_str());
    if (fd == -2 && !is_local_socket_spec(__adb_server_socket_spec)) {
        fprintf(stderr, "* cannot start server on remote host\n");
        // error is the original network connection error
        return fd;
    } else if (fd == -2) {
        fprintf(stderr, "* daemon not running; starting now at %s\n", __adb_server_socket_spec);
    start_server:
        if (launch_server(__adb_server_socket_spec)) {
            fprintf(stderr, "* failed to start daemon\n");
            // launch_server() has already printed detailed error info, so just
            // return a generic error string about the overall adb_connect()
            // that the caller requested.
            *error = "cannot connect to daemon";
            return -1;
        } else {
            fprintf(stderr, "* daemon started successfully\n");
        }
        // The server will wait until it detects all of its connected devices before acking.
        // Fall through to _adb_connect.
    } else {
        // If a server is already running, check its version matches.
        int version = ADB_SERVER_VERSION - 1;

        // If we have a file descriptor, then parse version result.
        if (fd >= 0) {
            std::string version_string;
            if (!ReadProtocolString(fd, &version_string, error)) {
                adb_close(fd);
                return -1;
            }

            ReadOrderlyShutdown(fd);
            adb_close(fd);

            if (sscanf(&version_string[0], "%04x", &version) != 1) {
                *error = android::base::StringPrintf("cannot parse version string: %s",
                                                     version_string.c_str());
                return -1;
            }
        } else {
            // If fd is -1 check for "unknown host service" which would
            // indicate a version of adb that does not support the
            // version command, in which case we should fall-through to kill it.
            if (*error != "unknown host service") {
                return fd;
            }
        }

        if (version != ADB_SERVER_VERSION) {
            fprintf(stderr, "adb server version (%d) doesn't match this client (%d); killing...\n",
                    version, ADB_SERVER_VERSION);
            adb_kill_server();
            goto start_server;
        }
    }

    // if the command is start-server, we are done.
    if (service == "host:start-server") {
        return 0;
    }

    fd = _adb_connect(service, error);
    if (fd == -1) {
        D("_adb_connect error: %s", error->c_str());
    } else if(fd == -2) {
        fprintf(stderr, "* daemon still not running\n");
    }
    D("adb_connect: return fd %d", fd);

    return fd;
}


bool adb_command(const std::string& service) {
    std::string error;
    int fd = adb_connect(service, &error);
    if (fd < 0) {
        fprintf(stderr, "error: %s\n", error.c_str());
        return false;
    }

    if (!adb_status(fd, &error)) {
        fprintf(stderr, "error: %s\n", error.c_str());
        adb_close(fd);
        return false;
    }

    ReadOrderlyShutdown(fd);
    adb_close(fd);
    return true;
}

bool adb_query(const std::string& service, std::string* result, std::string* error) {
    D("adb_query: %s", service.c_str());
    int fd = adb_connect(service, error);
    if (fd < 0) {
        return false;
    }

    result->clear();
    if (!ReadProtocolString(fd, result, error)) {
        adb_close(fd);
        return false;
    }

    ReadOrderlyShutdown(fd);
    adb_close(fd);
    return true;
}

std::string format_host_command(const char* command, TransportType type, const char* serial) {
    if (serial) {
        return android::base::StringPrintf("host-serial:%s:%s", serial, command);
    }

    const char* prefix = "host";
    if (type == kTransportUsb) {
        prefix = "host-usb";
    } else if (type == kTransportLocal) {
        prefix = "host-local";
    }
    return android::base::StringPrintf("%s:%s", prefix, command);
}

bool adb_get_feature_set(FeatureSet* feature_set, std::string* error) {
    std::string result;
    if (adb_query(format_host_command("features", __adb_transport, __adb_serial), &result, error)) {
        *feature_set = StringToFeatureSet(result);
        return true;
    }
    feature_set->clear();
    return false;
}