summaryrefslogtreecommitdiffstats
blob: fecf452c1c4e99d4e4de99596a72058eecfa6ed9 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "adb_listeners.h"

#include <stdio.h>
#include <stdlib.h>

#include <algorithm>
#include <list>

#include <android-base/stringprintf.h>
#include <android-base/strings.h>
#include <android-base/thread_annotations.h>
#include <cutils/sockets.h>

#include "socket_spec.h"
#include "sysdeps.h"
#include "sysdeps/memory.h"
#include "transport.h"

// A listener is an entity which binds to a local port and, upon receiving a connection on that
// port, creates an asocket to connect the new local connection to a specific remote service.
//
// TODO: some listeners read from the new connection to determine what exact service to connect to
// on the far side.
class alistener {
  public:
    alistener(const std::string& _local_name, const std::string& _connect_to);
    ~alistener();

    fdevent fde;
    int fd = -1;

    std::string local_name;
    std::string connect_to;
    atransport* transport = nullptr;
    adisconnect disconnect;

  private:
    DISALLOW_COPY_AND_ASSIGN(alistener);
};

alistener::alistener(const std::string& _local_name, const std::string& _connect_to)
    : local_name(_local_name), connect_to(_connect_to) {
}

alistener::~alistener() {
    // Closes the corresponding fd.
    fdevent_remove(&fde);

    if (transport) {
        transport->RemoveDisconnect(&disconnect);
    }
}

// listener_list retains ownership of all created alistener objects. Removing an alistener from
// this list will cause it to be deleted.
static auto& listener_list_mutex = *new std::mutex();
typedef std::list<std::unique_ptr<alistener>> ListenerList;
static ListenerList& listener_list GUARDED_BY(listener_list_mutex) = *new ListenerList();

static void ss_listener_event_func(int _fd, unsigned ev, void *_l) {
    if (ev & FDE_READ) {
        int fd = adb_socket_accept(_fd, nullptr, nullptr);
        if (fd < 0) return;

        int rcv_buf_size = CHUNK_SIZE;
        adb_setsockopt(fd, SOL_SOCKET, SO_RCVBUF, &rcv_buf_size, sizeof(rcv_buf_size));

        asocket* s = create_local_socket(fd);
        if (s) {
            connect_to_smartsocket(s);
            return;
        }

        adb_close(fd);
    }
}

static void listener_event_func(int _fd, unsigned ev, void* _l)
{
    alistener* listener = reinterpret_cast<alistener*>(_l);
    asocket *s;

    if (ev & FDE_READ) {
        int fd = adb_socket_accept(_fd, nullptr, nullptr);
        if (fd < 0) {
            return;
        }

        s = create_local_socket(fd);
        if (s) {
            s->transport = listener->transport;
            connect_to_remote(s, listener->connect_to.c_str());
            return;
        }

        adb_close(fd);
    }
}

// Called as a transport disconnect function. |arg| is the raw alistener*.
static void listener_disconnect(void* arg, atransport*) EXCLUDES(listener_list_mutex) {
    std::lock_guard<std::mutex> lock(listener_list_mutex);
    for (auto iter = listener_list.begin(); iter != listener_list.end(); ++iter) {
        if (iter->get() == arg) {
            (*iter)->transport = nullptr;
            listener_list.erase(iter);
            return;
        }
    }
}

// Write the list of current listeners (network redirections) into a string.
std::string format_listeners() EXCLUDES(listener_list_mutex) {
    std::lock_guard<std::mutex> lock(listener_list_mutex);
    std::string result;
    for (auto& l : listener_list) {
        // Ignore special listeners like those for *smartsocket*
        if (l->connect_to[0] == '*') {
            continue;
        }
        //  <device-serial> " " <local-name> " " <remote-name> "\n"
        // Entries from "adb reverse" have no serial.
        android::base::StringAppendF(&result, "%s %s %s\n",
                                     l->transport->serial ? l->transport->serial : "(reverse)",
                                     l->local_name.c_str(), l->connect_to.c_str());
    }
    return result;
}

InstallStatus remove_listener(const char* local_name, atransport* transport)
    EXCLUDES(listener_list_mutex) {
    std::lock_guard<std::mutex> lock(listener_list_mutex);
    for (auto iter = listener_list.begin(); iter != listener_list.end(); ++iter) {
        if (local_name == (*iter)->local_name) {
            listener_list.erase(iter);
            return INSTALL_STATUS_OK;
        }
    }
    return INSTALL_STATUS_LISTENER_NOT_FOUND;
}

void remove_all_listeners() EXCLUDES(listener_list_mutex) {
    std::lock_guard<std::mutex> lock(listener_list_mutex);
    auto iter = listener_list.begin();
    while (iter != listener_list.end()) {
        // Never remove smart sockets.
        if ((*iter)->connect_to[0] == '*') {
            ++iter;
        } else {
            iter = listener_list.erase(iter);
        }
    }
}

void close_smartsockets() EXCLUDES(listener_list_mutex) {
    std::lock_guard<std::mutex> lock(listener_list_mutex);
    auto pred = [](const std::unique_ptr<alistener>& listener) {
        return listener->local_name == "*smartsocket*";
    };
    listener_list.remove_if(pred);
}

InstallStatus install_listener(const std::string& local_name, const char* connect_to,
                               atransport* transport, int no_rebind, int* resolved_tcp_port,
                               std::string* error) EXCLUDES(listener_list_mutex) {
    std::lock_guard<std::mutex> lock(listener_list_mutex);
    for (auto& l : listener_list) {
        if (local_name == l->local_name) {
            // Can't repurpose a smartsocket.
            if(l->connect_to[0] == '*') {
                *error = "cannot repurpose smartsocket";
                return INSTALL_STATUS_INTERNAL_ERROR;
            }

            // Can't repurpose a listener if 'no_rebind' is true.
            if (no_rebind) {
                *error = "cannot rebind";
                return INSTALL_STATUS_CANNOT_REBIND;
            }

            l->connect_to = connect_to;
            if (l->transport != transport) {
                l->transport->RemoveDisconnect(&l->disconnect);
                l->transport = transport;
                l->transport->AddDisconnect(&l->disconnect);
            }
            return INSTALL_STATUS_OK;
        }
    }

    auto listener = std::make_unique<alistener>(local_name, connect_to);

    int resolved = 0;
    listener->fd = socket_spec_listen(listener->local_name, error, &resolved);
    if (listener->fd < 0) {
        return INSTALL_STATUS_CANNOT_BIND;
    }

    // If the caller requested port 0, update the listener name with the resolved port.
    if (resolved != 0) {
        listener->local_name = android::base::StringPrintf("tcp:%d", resolved);
        if (resolved_tcp_port) {
            *resolved_tcp_port = resolved;
        }
    }

    close_on_exec(listener->fd);
    if (listener->connect_to == "*smartsocket*") {
        fdevent_install(&listener->fde, listener->fd, ss_listener_event_func, listener.get());
    } else {
        fdevent_install(&listener->fde, listener->fd, listener_event_func, listener.get());
    }
    fdevent_set(&listener->fde, FDE_READ);

    listener->transport = transport;

    if (transport) {
        listener->disconnect.opaque = listener.get();
        listener->disconnect.func = listener_disconnect;
        transport->AddDisconnect(&listener->disconnect);
    }

    listener_list.push_back(std::move(listener));
    return INSTALL_STATUS_OK;
}