summaryrefslogtreecommitdiffstats
blob: 3603f097476c3af2407c586ccbb04d2deb6239e8 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
/*
 * Copyright (C) 2016 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#define TRACE_TAG TRANSPORT

#include "transport.h"

#ifdef _WIN32
#include <winsock2.h>
#else
#include <arpa/inet.h>
#endif

#include <thread>

#include <android-base/stringprintf.h>
#include <dns_sd.h>

#include "adb_mdns.h"
#include "adb_trace.h"
#include "fdevent.h"
#include "sysdeps.h"

static DNSServiceRef service_ref;
static fdevent service_ref_fde;

// Use adb_DNSServiceRefSockFD() instead of calling DNSServiceRefSockFD()
// directly so that the socket is put through the appropriate compatibility
// layers to work with the rest of ADB's internal APIs.
static inline int adb_DNSServiceRefSockFD(DNSServiceRef ref) {
    return adb_register_socket(DNSServiceRefSockFD(ref));
}
#define DNSServiceRefSockFD ___xxx_DNSServiceRefSockFD

static void DNSSD_API register_service_ip(DNSServiceRef sdRef,
                                          DNSServiceFlags flags,
                                          uint32_t interfaceIndex,
                                          DNSServiceErrorType errorCode,
                                          const char* hostname,
                                          const sockaddr* address,
                                          uint32_t ttl,
                                          void* context);

static void pump_service_ref(int /*fd*/, unsigned ev, void* data) {
    DNSServiceRef* ref = reinterpret_cast<DNSServiceRef*>(data);

    if (ev & FDE_READ)
        DNSServiceProcessResult(*ref);
}

class AsyncServiceRef {
  public:
    bool Initialized() {
        return initialized_;
    }

    virtual ~AsyncServiceRef() {
        if (! initialized_) {
            return;
        }

        DNSServiceRefDeallocate(sdRef_);
        fdevent_remove(&fde_);
    }

  protected:
    DNSServiceRef sdRef_;

    void Initialize() {
        fdevent_install(&fde_, adb_DNSServiceRefSockFD(sdRef_),
                        pump_service_ref, &sdRef_);
        fdevent_set(&fde_, FDE_READ);
        initialized_ = true;
    }

  private:
    bool initialized_;
    fdevent fde_;
};

class ResolvedService : public AsyncServiceRef {
  public:
    virtual ~ResolvedService() = default;

    ResolvedService(std::string name, uint32_t interfaceIndex,
                    const char* hosttarget, uint16_t port) :
            name_(name),
            port_(port) {

        /* TODO: We should be able to get IPv6 support by adding
         * kDNSServiceProtocol_IPv6 to the flags below. However, when we do
         * this, we get served link-local addresses that are usually useless to
         * connect to. What's more, we seem to /only/ get those and nothing else.
         * If we want IPv6 in the future we'll have to figure out why.
         */
        DNSServiceErrorType ret =
            DNSServiceGetAddrInfo(
                &sdRef_, 0, interfaceIndex,
                kDNSServiceProtocol_IPv4, hosttarget,
                register_service_ip, reinterpret_cast<void*>(this));

        if (ret != kDNSServiceErr_NoError) {
            D("Got %d from DNSServiceGetAddrInfo.", ret);
        } else {
            Initialize();
        }
    }

    void Connect(const sockaddr* address) {
        char ip_addr[INET6_ADDRSTRLEN];
        const void* ip_addr_data;
        const char* addr_format;

        if (address->sa_family == AF_INET) {
            ip_addr_data =
                &reinterpret_cast<const sockaddr_in*>(address)->sin_addr;
            addr_format = "%s:%hu";
        } else if (address->sa_family == AF_INET6) {
            ip_addr_data =
                &reinterpret_cast<const sockaddr_in6*>(address)->sin6_addr;
            addr_format = "[%s]:%hu";
        } else { // Should be impossible
            D("mDNS resolved non-IP address.");
            return;
        }

        // Winsock version requires the const cast Because Microsoft.
        if (!inet_ntop(address->sa_family, const_cast<void*>(ip_addr_data),
                       ip_addr, INET6_ADDRSTRLEN)) {
            D("Could not convert IP address to string.");
            return;
        }

        std::string response;
        connect_device(android::base::StringPrintf(addr_format, ip_addr, port_),
                       &response);
        D("Connect to %s (%s:%hu) : %s", name_.c_str(), ip_addr, port_,
          response.c_str());
    }

  private:
    std::string name_;
    const uint16_t port_;
};

static void DNSSD_API register_service_ip(DNSServiceRef /*sdRef*/,
                                          DNSServiceFlags /*flags*/,
                                          uint32_t /*interfaceIndex*/,
                                          DNSServiceErrorType /*errorCode*/,
                                          const char* /*hostname*/,
                                          const sockaddr* address,
                                          uint32_t /*ttl*/,
                                          void* context) {
    D("Got IP for service.");
    std::unique_ptr<ResolvedService> data(
        reinterpret_cast<ResolvedService*>(context));
    data->Connect(address);
}

static void DNSSD_API register_resolved_mdns_service(DNSServiceRef sdRef,
                                                     DNSServiceFlags flags,
                                                     uint32_t interfaceIndex,
                                                     DNSServiceErrorType errorCode,
                                                     const char* fullname,
                                                     const char* hosttarget,
                                                     uint16_t port,
                                                     uint16_t txtLen,
                                                     const unsigned char* txtRecord,
                                                     void* context);

class DiscoveredService : public AsyncServiceRef {
  public:
    DiscoveredService(uint32_t interfaceIndex, const char* serviceName,
                      const char* regtype, const char* domain)
        : serviceName_(serviceName) {

        DNSServiceErrorType ret =
            DNSServiceResolve(&sdRef_, 0, interfaceIndex, serviceName, regtype,
                              domain, register_resolved_mdns_service,
                              reinterpret_cast<void*>(this));

        if (ret != kDNSServiceErr_NoError) {
            D("Got %d from DNSServiceResolve.", ret);
        } else {
            Initialize();
        }
    }

    const char* ServiceName() {
        return serviceName_.c_str();
    }

  private:
    std::string serviceName_;
};

static void DNSSD_API register_resolved_mdns_service(DNSServiceRef sdRef,
                                                     DNSServiceFlags flags,
                                                     uint32_t interfaceIndex,
                                                     DNSServiceErrorType errorCode,
                                                     const char* fullname,
                                                     const char* hosttarget,
                                                     uint16_t port,
                                                     uint16_t /*txtLen*/,
                                                     const unsigned char* /*txtRecord*/,
                                                     void* context) {
    D("Resolved a service.");
    std::unique_ptr<DiscoveredService> discovered(
        reinterpret_cast<DiscoveredService*>(context));

    if (errorCode != kDNSServiceErr_NoError) {
        D("Got error %d resolving service.", errorCode);
        return;
    }


    auto resolved =
        new ResolvedService(discovered->ServiceName(),
                            interfaceIndex, hosttarget, ntohs(port));

    if (! resolved->Initialized()) {
        delete resolved;
    }

    if (flags) { /* Only ever equals MoreComing or 0 */
        discovered.release();
    }
}

static void DNSSD_API register_mdns_transport(DNSServiceRef sdRef,
                                              DNSServiceFlags flags,
                                              uint32_t interfaceIndex,
                                              DNSServiceErrorType errorCode,
                                              const char* serviceName,
                                              const char* regtype,
                                              const char* domain,
                                              void*  /*context*/) {
    D("Registering a transport.");
    if (errorCode != kDNSServiceErr_NoError) {
        D("Got error %d during mDNS browse.", errorCode);
        DNSServiceRefDeallocate(sdRef);
        fdevent_remove(&service_ref_fde);
        return;
    }

    auto discovered = new DiscoveredService(interfaceIndex, serviceName,
                                            regtype, domain);

    if (! discovered->Initialized()) {
        delete discovered;
    }
}

void init_mdns_transport_discovery_thread(void) {
    DNSServiceErrorType errorCode = DNSServiceBrowse(&service_ref, 0, 0, kADBServiceType, nullptr,
                                                     register_mdns_transport, nullptr);

    if (errorCode != kDNSServiceErr_NoError) {
        D("Got %d initiating mDNS browse.", errorCode);
        return;
    }

    fdevent_run_on_main_thread([]() {
        fdevent_install(&service_ref_fde, adb_DNSServiceRefSockFD(service_ref), pump_service_ref,
                        &service_ref);
        fdevent_set(&service_ref_fde, FDE_READ);
    });
}

void init_mdns_transport_discovery(void) {
    std::thread(init_mdns_transport_discovery_thread).detach();
}