summaryrefslogtreecommitdiffstats
blob: 211d8f345a50eaac2ad77047bd9e996a1019760d (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#if !ADB_HOST

#define TRACE_TAG JDWP

#include "sysdeps.h"

#include <errno.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/socket.h>
#include <sys/un.h>
#include <unistd.h>

#include <list>
#include <memory>
#include <vector>

#include "adb.h"
#include "adb_io.h"
#include "adb_unique_fd.h"
#include "adb_utils.h"

/* here's how these things work.

   when adbd starts, it creates a unix server socket
   named @jdwp-control (@ is a shortcut for "first byte is zero"
   to use the private namespace instead of the file system)

   when a new JDWP daemon thread starts in a new VM process, it creates
   a connection to @jdwp-control to announce its availability.


     JDWP thread                             @jdwp-control
         |                                         |
         |------------------------------->         |
         | hello I'm in process <pid>              |
         |                                         |
         |                                         |

    the connection is kept alive. it will be closed automatically if
    the JDWP process terminates (this allows adbd to detect dead
    processes).

    adbd thus maintains a list of "active" JDWP processes. it can send
    its content to clients through the "device:debug-ports" service,
    or even updates through the "device:track-debug-ports" service.

    when a debugger wants to connect, it simply runs the command
    equivalent to  "adb forward tcp:<hostport> jdwp:<pid>"

    "jdwp:<pid>" is a new forward destination format used to target
    a given JDWP process on the device. when sutch a request arrives,
    adbd does the following:

      - first, it calls socketpair() to create a pair of equivalent
        sockets.

      - it attaches the first socket in the pair to a local socket
        which is itself attached to the transport's remote socket:


      - it sends the file descriptor of the second socket directly
        to the JDWP process with the help of sendmsg()


     JDWP thread                             @jdwp-control
         |                                         |
         |                  <----------------------|
         |           OK, try this file descriptor  |
         |                                         |
         |                                         |

   then, the JDWP thread uses this new socket descriptor as its
   pass-through connection to the debugger (and receives the
   JDWP-Handshake message, answers to it, etc...)

   this gives the following graphics:
                    ____________________________________
                   |                                    |
                   |          ADB Server (host)         |
                   |                                    |
        Debugger <---> LocalSocket <----> RemoteSocket  |
                   |                           ^^       |
                   |___________________________||_______|
                                               ||
                                     Transport ||
           (TCP for emulator - USB for device) ||
                                               ||
                    ___________________________||_______
                   |                           ||       |
                   |          ADBD  (device)   ||       |
                   |                           VV       |
         JDWP <======> LocalSocket <----> RemoteSocket  |
                   |                                    |
                   |____________________________________|

    due to the way adb works, this doesn't need a special socket
    type or fancy handling of socket termination if either the debugger
    or the JDWP process closes the connection.

    THIS IS THE SIMPLEST IMPLEMENTATION I COULD FIND, IF YOU HAPPEN
    TO HAVE A BETTER IDEA, LET ME KNOW - Digit

**********************************************************************/

/** JDWP PID List Support Code
 ** for each JDWP process, we record its pid and its connected socket
 **/

static void jdwp_process_event(int socket, unsigned events, void* _proc);
static void jdwp_process_list_updated(void);

struct JdwpProcess;
static auto& _jdwp_list = *new std::list<std::unique_ptr<JdwpProcess>>();

struct JdwpProcess {
    explicit JdwpProcess(int socket) {
        this->socket = socket;
        this->fde = fdevent_create(socket, jdwp_process_event, this);

        if (!this->fde) {
            fatal("could not create fdevent for new JDWP process");
        }

        /* start by waiting for the PID */
        fdevent_add(this->fde, FDE_READ);
    }

    ~JdwpProcess() {
        if (this->socket >= 0) {
            adb_shutdown(this->socket);
            this->socket = -1;
        }

        if (this->fde) {
            fdevent_destroy(this->fde);
            this->fde = nullptr;
        }

        out_fds.clear();
    }

    void RemoveFromList() {
        if (this->pid >= 0) {
            D("removing pid %d from jdwp process list", this->pid);
        } else {
            D("removing transient JdwpProcess from list");
        }

        auto pred = [this](const auto& proc) { return proc.get() == this; };
        _jdwp_list.remove_if(pred);
    }

    int32_t pid = -1;
    int socket = -1;
    fdevent* fde = nullptr;

    std::vector<unique_fd> out_fds;
};

static size_t jdwp_process_list(char* buffer, size_t bufferlen) {
    std::string temp;

    for (auto& proc : _jdwp_list) {
        /* skip transient connections */
        if (proc->pid < 0) {
            continue;
        }

        std::string next = std::to_string(proc->pid) + "\n";
        if (temp.length() + next.length() > bufferlen) {
            D("truncating JDWP process list (max len = %zu)", bufferlen);
            break;
        }
        temp.append(next);
    }

    memcpy(buffer, temp.data(), temp.length());
    return temp.length();
}

static size_t jdwp_process_list_msg(char* buffer, size_t bufferlen) {
    // Message is length-prefixed with 4 hex digits in ASCII.
    static constexpr size_t header_len = 4;
    if (bufferlen < header_len) {
        fatal("invalid JDWP process list buffer size: %zu", bufferlen);
    }

    char head[header_len + 1];
    size_t len = jdwp_process_list(buffer + header_len, bufferlen - header_len);
    snprintf(head, sizeof head, "%04zx", len);
    memcpy(buffer, head, header_len);
    return len + header_len;
}

static void jdwp_process_event(int socket, unsigned events, void* _proc) {
    JdwpProcess* proc = reinterpret_cast<JdwpProcess*>(_proc);

    if (events & FDE_READ) {
        if (proc->pid < 0) {
            ssize_t rc = TEMP_FAILURE_RETRY(recv(socket, &proc->pid, sizeof(proc->pid), 0));
            if (rc != sizeof(proc->pid)) {
                D("failed to read jdwp pid: rc = %zd, errno = %s", rc, strerror(errno));
                goto CloseProcess;
            }

            /* all is well, keep reading to detect connection closure */
            D("Adding pid %d to jdwp process list", proc->pid);
            jdwp_process_list_updated();
        } else {
            /* the pid was read, if we get there it's probably because the connection
             * was closed (e.g. the JDWP process exited or crashed) */
            char buf[32];

            while (true) {
                int len = TEMP_FAILURE_RETRY(recv(socket, buf, sizeof(buf), 0));

                if (len == 0) {
                    D("terminating JDWP %d connection: EOF", proc->pid);
                    break;
                } else if (len < 0) {
                    if (len < 0 && errno == EAGAIN) {
                        return;
                    }

                    D("terminating JDWP %d connection: EOF", proc->pid);
                    break;
                } else {
                    D("ignoring unexpected JDWP %d control socket activity (%d bytes)", proc->pid,
                      len);
                }
            }

            goto CloseProcess;
        }
    }

    if (events & FDE_WRITE) {
        D("trying to send fd to JDWP process (count = %zu)", proc->out_fds.size());
        if (!proc->out_fds.empty()) {
            int fd = proc->out_fds.back().get();
            struct cmsghdr* cmsg;
            struct msghdr msg;
            struct iovec iov;
            char dummy = '!';
            char buffer[sizeof(struct cmsghdr) + sizeof(int)];

            iov.iov_base = &dummy;
            iov.iov_len = 1;
            msg.msg_name = NULL;
            msg.msg_namelen = 0;
            msg.msg_iov = &iov;
            msg.msg_iovlen = 1;
            msg.msg_flags = 0;
            msg.msg_control = buffer;
            msg.msg_controllen = sizeof(buffer);

            cmsg = CMSG_FIRSTHDR(&msg);
            cmsg->cmsg_len = msg.msg_controllen;
            cmsg->cmsg_level = SOL_SOCKET;
            cmsg->cmsg_type = SCM_RIGHTS;
            ((int*)CMSG_DATA(cmsg))[0] = fd;

            if (!set_file_block_mode(proc->socket, true)) {
                VLOG(JDWP) << "failed to set blocking mode for fd " << proc->socket;
                goto CloseProcess;
            }

            int ret = TEMP_FAILURE_RETRY(sendmsg(proc->socket, &msg, 0));
            if (ret < 0) {
                D("sending new file descriptor to JDWP %d failed: %s", proc->pid, strerror(errno));
                goto CloseProcess;
            }

            adb_close(fd);

            D("sent file descriptor %d to JDWP process %d", fd, proc->pid);

            proc->out_fds.pop_back();

            if (!set_file_block_mode(proc->socket, false)) {
                VLOG(JDWP) << "failed to set non-blocking mode for fd " << proc->socket;
                goto CloseProcess;
            }

            if (proc->out_fds.empty()) {
                fdevent_del(proc->fde, FDE_WRITE);
            }
        }
    }

    return;

CloseProcess:
    proc->RemoveFromList();
    jdwp_process_list_updated();
}

int create_jdwp_connection_fd(int pid) {
    D("looking for pid %d in JDWP process list", pid);

    for (auto& proc : _jdwp_list) {
        if (proc->pid == pid) {
            int fds[2];

            if (adb_socketpair(fds) < 0) {
                D("%s: socket pair creation failed: %s", __FUNCTION__, strerror(errno));
                return -1;
            }
            D("socketpair: (%d,%d)", fds[0], fds[1]);

            proc->out_fds.emplace_back(fds[1]);
            if (proc->out_fds.size() == 1) {
                fdevent_add(proc->fde, FDE_WRITE);
            }

            return fds[0];
        }
    }
    D("search failed !!");
    return -1;
}

/**  VM DEBUG CONTROL SOCKET
 **
 **  we do implement a custom asocket to receive the data
 **/

/* name of the debug control Unix socket */
#define JDWP_CONTROL_NAME "\0jdwp-control"
#define JDWP_CONTROL_NAME_LEN (sizeof(JDWP_CONTROL_NAME) - 1)

struct JdwpControl {
    int listen_socket;
    fdevent* fde;
};

static JdwpControl _jdwp_control;

static void jdwp_control_event(int s, unsigned events, void* user);

static int jdwp_control_init(JdwpControl* control, const char* sockname, int socknamelen) {
    sockaddr_un addr;
    socklen_t addrlen;
    int s;
    int maxpath = sizeof(addr.sun_path);
    int pathlen = socknamelen;

    if (pathlen >= maxpath) {
        D("vm debug control socket name too long (%d extra chars)", pathlen + 1 - maxpath);
        return -1;
    }

    memset(&addr, 0, sizeof(addr));
    addr.sun_family = AF_UNIX;
    memcpy(addr.sun_path, sockname, socknamelen);

    s = socket(AF_UNIX, SOCK_SEQPACKET | SOCK_CLOEXEC, 0);
    if (s < 0) {
        D("could not create vm debug control socket. %d: %s", errno, strerror(errno));
        return -1;
    }

    addrlen = pathlen + sizeof(addr.sun_family);

    if (bind(s, reinterpret_cast<sockaddr*>(&addr), addrlen) < 0) {
        D("could not bind vm debug control socket: %d: %s", errno, strerror(errno));
        adb_close(s);
        return -1;
    }

    if (listen(s, 4) < 0) {
        D("listen failed in jdwp control socket: %d: %s", errno, strerror(errno));
        adb_close(s);
        return -1;
    }

    control->listen_socket = s;

    control->fde = fdevent_create(s, jdwp_control_event, control);
    if (control->fde == NULL) {
        D("could not create fdevent for jdwp control socket");
        adb_close(s);
        return -1;
    }

    /* only wait for incoming connections */
    fdevent_add(control->fde, FDE_READ);

    D("jdwp control socket started (%d)", control->listen_socket);
    return 0;
}

static void jdwp_control_event(int s, unsigned events, void* _control) {
    JdwpControl* control = (JdwpControl*)_control;

    if (events & FDE_READ) {
        int s = adb_socket_accept(control->listen_socket, nullptr, nullptr);
        if (s < 0) {
            if (errno == ECONNABORTED) {
                /* oops, the JDWP process died really quick */
                D("oops, the JDWP process died really quick");
                return;
            } else {
                /* the socket is probably closed ? */
                D("weird accept() failed on jdwp control socket: %s", strerror(errno));
                return;
            }
        }

        auto proc = std::make_unique<JdwpProcess>(s);
        if (!proc) {
            fatal("failed to allocate JdwpProcess");
        }

        _jdwp_list.emplace_back(std::move(proc));
    }
}

/** "jdwp" local service implementation
 ** this simply returns the list of known JDWP process pids
 **/

struct JdwpSocket : public asocket {
    bool pass = false;
};

static void jdwp_socket_close(asocket* s) {
    D("LS(%d): closing jdwp socket", s->id);

    if (s->peer) {
        D("LS(%d) peer->close()ing peer->id=%d peer->fd=%d", s->id, s->peer->id, s->peer->fd);
        s->peer->peer = nullptr;
        s->peer->close(s->peer);
        s->peer = nullptr;
    }

    remove_socket(s);
    delete s;
}

static int jdwp_socket_enqueue(asocket* s, apacket::payload_type) {
    /* you can't write to this asocket */
    D("LS(%d): JDWP socket received data?", s->id);
    s->peer->close(s->peer);
    return -1;
}

static void jdwp_socket_ready(asocket* s) {
    JdwpSocket* jdwp = (JdwpSocket*)s;
    asocket* peer = jdwp->peer;

    /* on the first call, send the list of pids,
     * on the second one, close the connection
     */
    if (!jdwp->pass) {
        apacket::payload_type data;
        data.resize(s->get_max_payload());
        size_t len = jdwp_process_list(&data[0], data.size());
        data.resize(len);
        peer->enqueue(peer, std::move(data));
        jdwp->pass = true;
    } else {
        peer->close(peer);
    }
}

asocket* create_jdwp_service_socket(void) {
    JdwpSocket* s = new JdwpSocket();

    if (!s) {
        fatal("failed to allocate JdwpSocket");
    }

    install_local_socket(s);

    s->ready = jdwp_socket_ready;
    s->enqueue = jdwp_socket_enqueue;
    s->close = jdwp_socket_close;
    s->pass = false;

    return s;
}

/** "track-jdwp" local service implementation
 ** this periodically sends the list of known JDWP process pids
 ** to the client...
 **/

struct JdwpTracker : public asocket {
    bool need_initial;
};

static auto& _jdwp_trackers = *new std::vector<std::unique_ptr<JdwpTracker>>();

static void jdwp_process_list_updated(void) {
    std::string data;
    data.resize(1024);
    data.resize(jdwp_process_list_msg(&data[0], data.size()));

    for (auto& t : _jdwp_trackers) {
        if (t->peer) {
            // The tracker might not have been connected yet.
            apacket::payload_type payload(data.begin(), data.end());
            t->peer->enqueue(t->peer, std::move(payload));
        }
    }
}

static void jdwp_tracker_close(asocket* s) {
    D("LS(%d): destroying jdwp tracker service", s->id);

    if (s->peer) {
        D("LS(%d) peer->close()ing peer->id=%d peer->fd=%d", s->id, s->peer->id, s->peer->fd);
        s->peer->peer = nullptr;
        s->peer->close(s->peer);
        s->peer = nullptr;
    }

    remove_socket(s);

    auto pred = [s](const auto& tracker) { return tracker.get() == s; };
    _jdwp_trackers.erase(std::remove_if(_jdwp_trackers.begin(), _jdwp_trackers.end(), pred),
                         _jdwp_trackers.end());
}

static void jdwp_tracker_ready(asocket* s) {
    JdwpTracker* t = (JdwpTracker*)s;

    if (t->need_initial) {
        apacket::payload_type data;
        data.resize(s->get_max_payload());
        data.resize(jdwp_process_list_msg(&data[0], data.size()));
        t->need_initial = false;
        s->peer->enqueue(s->peer, std::move(data));
    }
}

static int jdwp_tracker_enqueue(asocket* s, apacket::payload_type) {
    /* you can't write to this socket */
    D("LS(%d): JDWP tracker received data?", s->id);
    s->peer->close(s->peer);
    return -1;
}

asocket* create_jdwp_tracker_service_socket(void) {
    auto t = std::make_unique<JdwpTracker>();
    if (!t) {
        fatal("failed to allocate JdwpTracker");
    }

    memset(t.get(), 0, sizeof(asocket));

    install_local_socket(t.get());
    D("LS(%d): created new jdwp tracker service", t->id);

    t->ready = jdwp_tracker_ready;
    t->enqueue = jdwp_tracker_enqueue;
    t->close = jdwp_tracker_close;
    t->need_initial = true;

    asocket* result = t.get();

    _jdwp_trackers.emplace_back(std::move(t));

    return result;
}

int init_jdwp(void) {
    return jdwp_control_init(&_jdwp_control, JDWP_CONTROL_NAME, JDWP_CONTROL_NAME_LEN);
}

#endif /* !ADB_HOST */