1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
|
/*
* Copyright (C) 2015 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#define TRACE_TAG ADB
#include "sysdeps.h"
#include <errno.h>
#include <signal.h>
#include <stdio.h>
#include <stdlib.h>
#include <getopt.h>
#include <sys/prctl.h>
#include <memory>
#include <android-base/logging.h>
#include <android-base/macros.h>
#include <android-base/properties.h>
#include <android-base/stringprintf.h>
#include <libminijail.h>
#include <log/log_properties.h>
#include <scoped_minijail.h>
#include <private/android_filesystem_config.h>
#include "debuggerd/handler.h"
#include "selinux/android.h"
#include "adb.h"
#include "adb_auth.h"
#include "adb_listeners.h"
#include "adb_utils.h"
#include "transport.h"
#include "mdns.h"
static const char* root_seclabel = nullptr;
static inline bool is_device_unlocked() {
return "orange" == android::base::GetProperty("ro.boot.verifiedbootstate", "");
}
static void drop_capabilities_bounding_set_if_needed(struct minijail *j) {
if (ALLOW_ADBD_ROOT || is_device_unlocked()) {
if (__android_log_is_debuggable()) {
return;
}
}
minijail_capbset_drop(j, CAP_TO_MASK(CAP_SETUID) | CAP_TO_MASK(CAP_SETGID));
}
static bool should_drop_privileges() {
// "adb root" not allowed, always drop privileges.
if (!ALLOW_ADBD_ROOT && !is_device_unlocked()) return true;
// The properties that affect `adb root` and `adb unroot` are ro.secure and
// ro.debuggable. In this context the names don't make the expected behavior
// particularly obvious.
//
// ro.debuggable:
// Allowed to become root, but not necessarily the default. Set to 1 on
// eng and userdebug builds.
//
// ro.secure:
// Drop privileges by default. Set to 1 on userdebug and user builds.
bool ro_secure = android::base::GetBoolProperty("ro.secure", true);
bool ro_debuggable = __android_log_is_debuggable();
// Drop privileges if ro.secure is set...
bool drop = ro_secure;
// ... except "adb root" lets you keep privileges in a debuggable build.
std::string prop = android::base::GetProperty("service.adb.root", "");
bool adb_root = (prop == "1");
bool adb_unroot = (prop == "0");
if (ro_debuggable && adb_root) {
drop = false;
}
// ... and "adb unroot" lets you explicitly drop privileges.
if (adb_unroot) {
drop = true;
}
return drop;
}
static void drop_privileges(int server_port) {
ScopedMinijail jail(minijail_new());
// Add extra groups:
// AID_ADB to access the USB driver
// AID_LOG to read system logs (adb logcat)
// AID_INPUT to diagnose input issues (getevent)
// AID_INET to diagnose network issues (ping)
// AID_NET_BT and AID_NET_BT_ADMIN to diagnose bluetooth (hcidump)
// AID_SDCARD_R to allow reading from the SD card
// AID_SDCARD_RW to allow writing to the SD card
// AID_NET_BW_STATS to read out qtaguid statistics
// AID_READPROC for reading /proc entries across UID boundaries
// AID_UHID for using 'hid' command to read/write to /dev/uhid
gid_t groups[] = {AID_ADB, AID_LOG, AID_INPUT, AID_INET,
AID_NET_BT, AID_NET_BT_ADMIN, AID_SDCARD_R, AID_SDCARD_RW,
AID_NET_BW_STATS, AID_READPROC, AID_UHID};
minijail_set_supplementary_gids(jail.get(), arraysize(groups), groups);
// Don't listen on a port (default 5037) if running in secure mode.
// Don't run as root if running in secure mode.
if (should_drop_privileges()) {
drop_capabilities_bounding_set_if_needed(jail.get());
minijail_change_gid(jail.get(), AID_SHELL);
minijail_change_uid(jail.get(), AID_SHELL);
// minijail_enter() will abort if any priv-dropping step fails.
minijail_enter(jail.get());
D("Local port disabled");
} else {
// minijail_enter() will abort if any priv-dropping step fails.
minijail_enter(jail.get());
if (root_seclabel != nullptr) {
if (selinux_android_setcon(root_seclabel) < 0) {
LOG(FATAL) << "Could not set SELinux context";
}
}
std::string error;
std::string local_name =
android::base::StringPrintf("tcp:%d", server_port);
if (install_listener(local_name, "*smartsocket*", nullptr, 0, nullptr, &error)) {
LOG(FATAL) << "Could not install *smartsocket* listener: " << error;
}
}
}
static void setup_port(int port) {
local_init(port);
setup_mdns(port);
}
int adbd_main(int server_port) {
umask(0);
signal(SIGPIPE, SIG_IGN);
init_transport_registration();
// We need to call this even if auth isn't enabled because the file
// descriptor will always be open.
adbd_cloexec_auth_socket();
// Respect ro.adb.secure in userdebug/eng builds (ALLOW_ADBD_NO_AUTH), or when the
// device is unlocked.
if ((ALLOW_ADBD_NO_AUTH || is_device_unlocked()) &&
!android::base::GetBoolProperty("ro.adb.secure", false)) {
auth_required = false;
}
adbd_auth_init();
// Our external storage path may be different than apps, since
// we aren't able to bind mount after dropping root.
const char* adb_external_storage = getenv("ADB_EXTERNAL_STORAGE");
if (adb_external_storage != nullptr) {
setenv("EXTERNAL_STORAGE", adb_external_storage, 1);
} else {
D("Warning: ADB_EXTERNAL_STORAGE is not set. Leaving EXTERNAL_STORAGE"
" unchanged.\n");
}
drop_privileges(server_port);
bool is_usb = false;
if (access(USB_FFS_ADB_EP0, F_OK) == 0) {
// Listen on USB.
usb_init();
is_usb = true;
}
// If one of these properties is set, also listen on that port.
// If one of the properties isn't set and we couldn't listen on usb, listen
// on the default port.
std::string prop_port = android::base::GetProperty("service.adb.tcp.port", "");
if (prop_port.empty()) {
prop_port = android::base::GetProperty("persist.adb.tcp.port", "");
}
int port;
if (sscanf(prop_port.c_str(), "%d", &port) == 1 && port > 0) {
D("using port=%d", port);
// Listen on TCP port specified by service.adb.tcp.port property.
setup_port(port);
} else if (!is_usb) {
// Listen on default port.
setup_port(DEFAULT_ADB_LOCAL_TRANSPORT_PORT);
}
D("adbd_main(): pre init_jdwp()");
init_jdwp();
D("adbd_main(): post init_jdwp()");
D("Event loop starting");
fdevent_loop();
return 0;
}
int main(int argc, char** argv) {
while (true) {
static struct option opts[] = {
{"root_seclabel", required_argument, nullptr, 's'},
{"device_banner", required_argument, nullptr, 'b'},
{"version", no_argument, nullptr, 'v'},
};
int option_index = 0;
int c = getopt_long(argc, argv, "", opts, &option_index);
if (c == -1) {
break;
}
switch (c) {
case 's':
root_seclabel = optarg;
break;
case 'b':
adb_device_banner = optarg;
break;
case 'v':
printf("Android Debug Bridge Daemon version %d.%d.%d (%s)\n", ADB_VERSION_MAJOR,
ADB_VERSION_MINOR, ADB_SERVER_VERSION, ADB_VERSION);
return 0;
default:
// getopt already prints "adbd: invalid option -- %c" for us.
return 1;
}
}
close_stdin();
debuggerd_init(nullptr);
adb_trace_init(argv);
D("Handling main()");
return adbd_main(DEFAULT_ADB_PORT);
}
|