summaryrefslogtreecommitdiffstats
blob: 658858717677aaa71018ddbf165b038b2b251a51 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
/*
 * Copyright (C) 2008 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#define TRACE_TAG ADB

#include "sysdeps.h"

#include <errno.h>
#include <fcntl.h>
#include <mntent.h>
#include <spawn.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/mount.h>
#include <sys/statvfs.h>
#include <sys/vfs.h>
#include <unistd.h>

#include <set>
#include <string>
#include <vector>

#include <android-base/properties.h>
#include <bootloader_message/bootloader_message.h>
#include <cutils/android_reboot.h>
#include <ext4_utils/ext4_utils.h>

#include "adb.h"
#include "adb_io.h"
#include "adb_unique_fd.h"
#include "adb_utils.h"
#include "fs_mgr.h"
#include "set_verity_enable_state_service.h"

// Returns the device used to mount a directory in /proc/mounts.
static std::string find_proc_mount(const char* dir) {
    std::unique_ptr<FILE, int(*)(FILE*)> fp(setmntent("/proc/mounts", "r"), endmntent);
    if (!fp) {
        return "";
    }

    mntent* e;
    while ((e = getmntent(fp.get())) != nullptr) {
        if (strcmp(dir, e->mnt_dir) == 0) {
            return e->mnt_fsname;
        }
    }
    return "";
}

// Returns the device used to mount a directory in the fstab.
static std::string find_fstab_mount(const char* dir) {
    std::unique_ptr<fstab, decltype(&fs_mgr_free_fstab)> fstab(fs_mgr_read_fstab_default(),
                                                               fs_mgr_free_fstab);
    struct fstab_rec* rec = fs_mgr_get_entry_for_mount_point(fstab.get(), dir);
    return rec ? rec->blk_device : "";
}

// The proc entry for / is full of lies, so check fstab instead.
// /proc/mounts lists rootfs and /dev/root, neither of which is what we want.
static std::string find_mount(const char* dir, bool is_root) {
    if (is_root) {
        return find_fstab_mount(dir);
    } else {
       return find_proc_mount(dir);
    }
}

bool make_block_device_writable(const std::string& dev) {
    int fd = unix_open(dev.c_str(), O_RDONLY | O_CLOEXEC);
    if (fd == -1) {
        return false;
    }

    int OFF = 0;
    bool result = (ioctl(fd, BLKROSET, &OFF) != -1);
    unix_close(fd);
    return result;
}

static bool fs_has_shared_blocks(const char* dev) {
    struct statfs fs;
    if (statfs(dev, &fs) == -1 || fs.f_type == EXT4_SUPER_MAGIC) {
        return false;
    }
    unique_fd fd(unix_open(dev, O_RDONLY));
    if (fd < 0) {
        return false;
    }
    struct ext4_super_block sb;
    if (lseek64(fd, 1024, SEEK_SET) < 0 || unix_read(fd, &sb, sizeof(sb)) < 0) {
        return false;
    }
    struct fs_info info;
    if (ext4_parse_sb(&sb, &info) < 0) {
        return false;
    }
    return (info.feat_ro_compat & EXT4_FEATURE_RO_COMPAT_SHARED_BLOCKS) != 0;
}

static bool can_unshare_blocks(int fd, const char* dev) {
    const char* E2FSCK_BIN = "/system/bin/e2fsck";
    if (access(E2FSCK_BIN, X_OK)) {
        WriteFdFmt(fd, "e2fsck is not available, cannot undo deduplication on %s\n", dev);
        return false;
    }

    pid_t child;
    char* env[] = {nullptr};
    const char* argv[] = {E2FSCK_BIN, "-n", "-E", "unshare_blocks", dev, nullptr};
    if (posix_spawn(&child, E2FSCK_BIN, nullptr, nullptr, const_cast<char**>(argv), env)) {
        WriteFdFmt(fd, "failed to e2fsck to check deduplication: %s\n", strerror(errno));
        return false;
    }
    int status = 0;
    int ret = TEMP_FAILURE_RETRY(waitpid(child, &status, 0));
    if (ret < 0) {
        WriteFdFmt(fd, "failed to get e2fsck status: %s\n", strerror(errno));
        return false;
    }
    if (!WIFEXITED(status)) {
        WriteFdFmt(fd, "e2fsck exited abnormally with status %d\n", status);
        return false;
    }
    int rc = WEXITSTATUS(status);
    if (rc != 0) {
        WriteFdFmt(fd,
                   "%s is deduplicated, and an e2fsck check failed. It might not "
                   "have enough free-space to be remounted as writable.\n",
                   dev);
        return false;
    }
    return true;
}

static unsigned long get_mount_flags(int fd, const char* dir) {
    struct statvfs st_vfs;
    if (statvfs(dir, &st_vfs) == -1) {
        // Even though we could not get the original mount flags, assume that
        // the mount was originally read-only.
        WriteFdFmt(fd, "statvfs of the %s mount failed: %s.\n", dir, strerror(errno));
        return MS_RDONLY;
    }
    return st_vfs.f_flag;
}

static bool remount_partition(int fd, const char* dir) {
    if (!directory_exists(dir)) {
        return true;
    }
    bool is_root = strcmp(dir, "/") == 0;
    std::string dev = find_mount(dir, is_root);
    // Even if the device for the root is not found, we still try to remount it
    // as rw. This typically only happens when running Android in a container:
    // the root will almost always be in a loop device, which is dynamic, so
    // it's not convenient to put in the fstab.
    if (dev.empty() && !is_root) {
        return true;
    }
    if (!dev.empty() && !make_block_device_writable(dev)) {
        WriteFdFmt(fd, "remount of %s failed; couldn't make block device %s writable: %s\n",
                   dir, dev.c_str(), strerror(errno));
        return false;
    }

    unsigned long remount_flags = get_mount_flags(fd, dir);
    remount_flags &= ~MS_RDONLY;
    remount_flags |= MS_REMOUNT;

    if (mount(dev.c_str(), dir, "none", remount_flags | MS_BIND, nullptr) == -1) {
        // This is useful for cases where the superblock is already marked as
        // read-write, but the mount itself is read-only, such as containers
        // where the remount with just MS_REMOUNT is forbidden by the kernel.
        WriteFdFmt(fd, "remount of the %s mount failed: %s.\n", dir, strerror(errno));
        return false;
    }
    if (mount(dev.c_str(), dir, "none", MS_REMOUNT, nullptr) == -1) {
        WriteFdFmt(fd, "remount of the %s superblock failed: %s\n", dir, strerror(errno));
        return false;
    }
    return true;
}

static void reboot_for_remount(int fd, bool need_fsck) {
    std::string reboot_cmd = "reboot";
    if (need_fsck) {
        const std::vector<std::string> options = {"--fsck_unshare_blocks"};
        std::string err;
        if (!write_bootloader_message(options, &err)) {
            WriteFdFmt(fd, "Failed to set bootloader message: %s\n", err.c_str());
            return;
        }

        WriteFdExactly(fd,
                       "The device will now reboot to recovery and attempt "
                       "un-deduplication.\n");
        reboot_cmd = "reboot,recovery";
    }

    sync();
    android::base::SetProperty(ANDROID_RB_PROPERTY, reboot_cmd.c_str());
}

void remount_service(unique_fd fd, const std::string& cmd) {
    bool user_requested_reboot = cmd == "-R";

    if (getuid() != 0) {
        WriteFdExactly(fd.get(), "Not running as root. Try \"adb root\" first.\n");
        return;
    }

    bool system_verified = !(android::base::GetProperty("partition.system.verified", "").empty());
    bool vendor_verified = !(android::base::GetProperty("partition.vendor.verified", "").empty());

    std::vector<std::string> partitions = {"/odm", "/oem", "/product", "/vendor"};
    if (android::base::GetBoolProperty("ro.build.system_root_image", false)) {
        partitions.push_back("/");
    } else {
        partitions.push_back("/system");
    }

    // Find partitions that are deduplicated, and can be un-deduplicated.
    std::set<std::string> dedup;
    for (const auto& partition : partitions) {
        std::string dev = find_mount(partition.c_str(), partition == "/");
        if (dev.empty() || !fs_has_shared_blocks(dev.c_str())) {
            continue;
        }
        if (can_unshare_blocks(fd.get(), dev.c_str())) {
            dedup.emplace(partition);
        }
    }

    bool verity_enabled = (system_verified || vendor_verified);

    // Reboot now if the user requested it (and an operation needs a reboot).
    if (user_requested_reboot) {
        if (!dedup.empty() || verity_enabled) {
            if (verity_enabled) {
                set_verity_enabled_state_service(unique_fd(dup(fd.get())), false);
            }
            reboot_for_remount(fd.get(), !dedup.empty());
            return;
        }
        WriteFdExactly(fd.get(), "No reboot needed, skipping -R.\n");
    }

    // If we need to disable-verity, but we also need to perform a recovery
    // fsck for deduplicated partitions, hold off on warning about verity. We
    // can handle both verity and the recovery fsck in the same reboot cycle.
    if (verity_enabled && dedup.empty()) {
        // Allow remount but warn of likely bad effects
        bool both = system_verified && vendor_verified;
        WriteFdFmt(fd.get(), "dm_verity is enabled on the %s%s%s partition%s.\n",
                   system_verified ? "system" : "", both ? " and " : "",
                   vendor_verified ? "vendor" : "", both ? "s" : "");
        WriteFdExactly(fd.get(),
                       "Use \"adb disable-verity\" to disable verity.\n"
                       "If you do not, remount may succeed, however, you will still "
                       "not be able to write to these volumes.\n");
        WriteFdExactly(fd.get(),
                       "Alternately, use \"adb remount -R\" to disable verity "
                       "and automatically reboot.\n");
    }

    bool success = true;
    for (const auto& partition : partitions) {
        // Don't try to remount partitions that need an fsck in recovery.
        if (dedup.count(partition)) {
            continue;
        }
        success &= remount_partition(fd.get(), partition.c_str());
    }

    if (!dedup.empty()) {
        WriteFdExactly(fd.get(),
                       "The following partitions are deduplicated and cannot "
                       "yet be remounted:\n");
        for (const std::string& name : dedup) {
            WriteFdFmt(fd.get(), "  %s\n", name.c_str());
        }

        WriteFdExactly(fd.get(),
                       "To reboot and un-deduplicate the listed partitions, "
                       "please retry with adb remount -R.\n");
        if (system_verified || vendor_verified) {
            WriteFdExactly(fd.get(), "Note: verity will be automatically disabled after reboot.\n");
        }
        return;
    }

    if (!success) {
        WriteFdExactly(fd.get(), "remount failed\n");
    } else {
        WriteFdExactly(fd.get(), "remount succeeded\n");
    }
}