summaryrefslogtreecommitdiffstats
blob: f9e262c51bf3ff87c4f45517dfd312827e60b494 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
/* http://frotznet.googlecode.com/svn/trunk/utils/fdevent.c
**
** Copyright 2006, Brian Swetland <swetland@frotz.net>
**
** Licensed under the Apache License, Version 2.0 (the "License");
** you may not use this file except in compliance with the License.
** You may obtain a copy of the License at
**
**     http://www.apache.org/licenses/LICENSE-2.0
**
** Unless required by applicable law or agreed to in writing, software
** distributed under the License is distributed on an "AS IS" BASIS,
** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
** See the License for the specific language governing permissions and
** limitations under the License.
*/

#define TRACE_TAG FDEVENT

#include "sysdeps.h"
#include "fdevent.h"

#include <fcntl.h>
#include <stdint.h>
#include <stdlib.h>
#include <string.h>
#include <unistd.h>

#include <atomic>
#include <deque>
#include <functional>
#include <list>
#include <mutex>
#include <unordered_map>
#include <vector>

#include <android-base/logging.h>
#include <android-base/stringprintf.h>
#include <android-base/thread_annotations.h>
#include <android-base/threads.h>

#include "adb_io.h"
#include "adb_trace.h"
#include "adb_unique_fd.h"
#include "adb_utils.h"

#define FDE_EVENTMASK  0x00ff
#define FDE_STATEMASK  0xff00

#define FDE_ACTIVE     0x0100
#define FDE_PENDING    0x0200
#define FDE_CREATED    0x0400

struct PollNode {
  fdevent* fde;
  adb_pollfd pollfd;

  explicit PollNode(fdevent* fde) : fde(fde) {
      memset(&pollfd, 0, sizeof(pollfd));
      pollfd.fd = fde->fd;

#if defined(__linux__)
      // Always enable POLLRDHUP, so the host server can take action when some clients disconnect.
      // Then we can avoid leaving many sockets in CLOSE_WAIT state. See http://b/23314034.
      pollfd.events = POLLRDHUP;
#endif
  }
};

// All operations to fdevent should happen only in the main thread.
// That's why we don't need a lock for fdevent.
static auto& g_poll_node_map = *new std::unordered_map<int, PollNode>();
static auto& g_pending_list = *new std::list<fdevent*>();
static std::atomic<bool> terminate_loop(false);
static bool main_thread_valid;
static uint64_t main_thread_id;

static bool run_needs_flush = false;
static auto& run_queue_notify_fd = *new unique_fd();
static auto& run_queue_mutex = *new std::mutex();
static auto& run_queue GUARDED_BY(run_queue_mutex) = *new std::deque<std::function<void()>>();

void check_main_thread() {
    if (main_thread_valid) {
        CHECK_EQ(main_thread_id, android::base::GetThreadId());
    }
}

void set_main_thread() {
    main_thread_valid = true;
    main_thread_id = android::base::GetThreadId();
}

static std::string dump_fde(const fdevent* fde) {
    std::string state;
    if (fde->state & FDE_ACTIVE) {
        state += "A";
    }
    if (fde->state & FDE_PENDING) {
        state += "P";
    }
    if (fde->state & FDE_CREATED) {
        state += "C";
    }
    if (fde->state & FDE_READ) {
        state += "R";
    }
    if (fde->state & FDE_WRITE) {
        state += "W";
    }
    if (fde->state & FDE_ERROR) {
        state += "E";
    }
    return android::base::StringPrintf("(fdevent %d %s)", fde->fd, state.c_str());
}

void fdevent_install(fdevent* fde, int fd, fd_func func, void* arg) {
    check_main_thread();
    CHECK_GE(fd, 0);
    memset(fde, 0, sizeof(fdevent));
}

fdevent* fdevent_create(int fd, fd_func func, void* arg) {
    check_main_thread();
    CHECK_GE(fd, 0);

    fdevent* fde = new fdevent();
    fde->state = FDE_ACTIVE;
    fde->fd = fd;
    fde->func = func;
    fde->arg = arg;
    if (!set_file_block_mode(fd, false)) {
        // Here is not proper to handle the error. If it fails here, some error is
        // likely to be detected by poll(), then we can let the callback function
        // to handle it.
        LOG(ERROR) << "failed to set non-blocking mode for fd " << fd;
    }
    auto pair = g_poll_node_map.emplace(fde->fd, PollNode(fde));
    CHECK(pair.second) << "install existing fd " << fd;

    fde->state |= FDE_CREATED;
    return fde;
}

void fdevent_destroy(fdevent* fde) {
    check_main_thread();
    if (fde == 0) return;
    if (!(fde->state & FDE_CREATED)) {
        LOG(FATAL) << "destroying fde not created by fdevent_create(): " << dump_fde(fde);
    }

    if (fde->state & FDE_ACTIVE) {
        g_poll_node_map.erase(fde->fd);
        if (fde->state & FDE_PENDING) {
            g_pending_list.remove(fde);
        }
        adb_close(fde->fd);
        fde->fd = -1;
        fde->state = 0;
        fde->events = 0;
    }

    delete fde;
}

static void fdevent_update(fdevent* fde, unsigned events) {
    auto it = g_poll_node_map.find(fde->fd);
    CHECK(it != g_poll_node_map.end());
    PollNode& node = it->second;
    if (events & FDE_READ) {
        node.pollfd.events |= POLLIN;
    } else {
        node.pollfd.events &= ~POLLIN;
    }

    if (events & FDE_WRITE) {
        node.pollfd.events |= POLLOUT;
    } else {
        node.pollfd.events &= ~POLLOUT;
    }
    fde->state = (fde->state & FDE_STATEMASK) | events;
}

void fdevent_set(fdevent* fde, unsigned events) {
    check_main_thread();
    events &= FDE_EVENTMASK;
    if ((fde->state & FDE_EVENTMASK) == events) {
        return;
    }
    CHECK(fde->state & FDE_ACTIVE);
    fdevent_update(fde, events);
    D("fdevent_set: %s, events = %u", dump_fde(fde).c_str(), events);

    if (fde->state & FDE_PENDING) {
        // If we are pending, make sure we don't signal an event that is no longer wanted.
        fde->events &= events;
        if (fde->events == 0) {
            g_pending_list.remove(fde);
            fde->state &= ~FDE_PENDING;
        }
    }
}

void fdevent_add(fdevent* fde, unsigned events) {
    check_main_thread();
    fdevent_set(fde, (fde->state & FDE_EVENTMASK) | events);
}

void fdevent_del(fdevent* fde, unsigned events) {
    check_main_thread();
    fdevent_set(fde, (fde->state & FDE_EVENTMASK) & ~events);
}

static std::string dump_pollfds(const std::vector<adb_pollfd>& pollfds) {
    std::string result;
    for (const auto& pollfd : pollfds) {
        std::string op;
        if (pollfd.events & POLLIN) {
            op += "R";
        }
        if (pollfd.events & POLLOUT) {
            op += "W";
        }
        android::base::StringAppendF(&result, " %d(%s)", pollfd.fd, op.c_str());
    }
    return result;
}

static void fdevent_process() {
    std::vector<adb_pollfd> pollfds;
    for (const auto& pair : g_poll_node_map) {
        pollfds.push_back(pair.second.pollfd);
    }
    CHECK_GT(pollfds.size(), 0u);
    D("poll(), pollfds = %s", dump_pollfds(pollfds).c_str());
    int ret = adb_poll(&pollfds[0], pollfds.size(), -1);
    if (ret == -1) {
        PLOG(ERROR) << "poll(), ret = " << ret;
        return;
    }
    for (const auto& pollfd : pollfds) {
        if (pollfd.revents != 0) {
            D("for fd %d, revents = %x", pollfd.fd, pollfd.revents);
        }
        unsigned events = 0;
        if (pollfd.revents & POLLIN) {
            events |= FDE_READ;
        }
        if (pollfd.revents & POLLOUT) {
            events |= FDE_WRITE;
        }
        if (pollfd.revents & (POLLERR | POLLHUP | POLLNVAL)) {
            // We fake a read, as the rest of the code assumes that errors will
            // be detected at that point.
            events |= FDE_READ | FDE_ERROR;
        }
#if defined(__linux__)
        if (pollfd.revents & POLLRDHUP) {
            events |= FDE_READ | FDE_ERROR;
        }
#endif
        if (events != 0) {
            auto it = g_poll_node_map.find(pollfd.fd);
            CHECK(it != g_poll_node_map.end());
            fdevent* fde = it->second.fde;
            CHECK_EQ(fde->fd, pollfd.fd);
            fde->events |= events;
            D("%s got events %x", dump_fde(fde).c_str(), events);
            fde->state |= FDE_PENDING;
            g_pending_list.push_back(fde);
        }
    }
}

static void fdevent_call_fdfunc(fdevent* fde) {
    unsigned events = fde->events;
    fde->events = 0;
    CHECK(fde->state & FDE_PENDING);
    fde->state &= (~FDE_PENDING);
    D("fdevent_call_fdfunc %s", dump_fde(fde).c_str());
    fde->func(fde->fd, events, fde->arg);
}

static void fdevent_run_flush() EXCLUDES(run_queue_mutex) {
    // We need to be careful around reentrancy here, since a function we call can queue up another
    // function.
    while (true) {
        std::function<void()> fn;
        {
            std::lock_guard<std::mutex> lock(run_queue_mutex);
            if (run_queue.empty()) {
                break;
            }
            fn = run_queue.front();
            run_queue.pop_front();
        }
        fn();
    }
}

static void fdevent_run_func(int fd, unsigned ev, void* /* userdata */) {
    CHECK_GE(fd, 0);
    CHECK(ev & FDE_READ);

    char buf[1024];

    // Empty the fd.
    if (adb_read(fd, buf, sizeof(buf)) == -1) {
        PLOG(FATAL) << "failed to empty run queue notify fd";
    }

    // Mark that we need to flush, and then run it at the end of fdevent_loop.
    run_needs_flush = true;
}

static void fdevent_run_setup() {
    {
        std::lock_guard<std::mutex> lock(run_queue_mutex);
        CHECK(run_queue_notify_fd.get() == -1);
        int s[2];
        if (adb_socketpair(s) != 0) {
            PLOG(FATAL) << "failed to create run queue notify socketpair";
        }

        if (!set_file_block_mode(s[0], false) || !set_file_block_mode(s[1], false)) {
            PLOG(FATAL) << "failed to make run queue notify socket nonblocking";
        }

        run_queue_notify_fd.reset(s[0]);
        fdevent* fde = fdevent_create(s[1], fdevent_run_func, nullptr);
        CHECK(fde != nullptr);
        fdevent_add(fde, FDE_READ);
    }

    fdevent_run_flush();
}

void fdevent_run_on_main_thread(std::function<void()> fn) {
    std::lock_guard<std::mutex> lock(run_queue_mutex);
    run_queue.push_back(std::move(fn));

    // run_queue_notify_fd could still be -1 if we're called before fdevent has finished setting up.
    // In that case, rely on the setup code to flush the queue without a notification being needed.
    if (run_queue_notify_fd != -1) {
        int rc = adb_write(run_queue_notify_fd.get(), "", 1);

        // It's possible that we get EAGAIN here, if lots of notifications came in while handling.
        if (rc == 0) {
            PLOG(FATAL) << "run queue notify fd was closed?";
        } else if (rc == -1 && errno != EAGAIN) {
            PLOG(FATAL) << "failed to write to run queue notify fd";
        }
    }
}

void fdevent_loop() {
    set_main_thread();
    fdevent_run_setup();

    while (true) {
        if (terminate_loop) {
            return;
        }

        D("--- --- waiting for events");

        fdevent_process();

        while (!g_pending_list.empty()) {
            fdevent* fde = g_pending_list.front();
            g_pending_list.pop_front();
            fdevent_call_fdfunc(fde);
        }

        if (run_needs_flush) {
            fdevent_run_flush();
            run_needs_flush = false;
        }
    }
}

void fdevent_terminate_loop() {
    terminate_loop = true;
}

size_t fdevent_installed_count() {
    return g_poll_node_map.size();
}

void fdevent_reset() {
    g_poll_node_map.clear();
    g_pending_list.clear();

    std::lock_guard<std::mutex> lock(run_queue_mutex);
    run_queue_notify_fd.reset();
    run_queue.clear();

    main_thread_valid = false;
    terminate_loop = false;
}