1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
|
/*
* Copyright (C) 2007 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
/* this file contains system-dependent definitions used by ADB
* they're related to threads, sockets and file descriptors
*/
#ifndef _ADB_SYSDEPS_H
#define _ADB_SYSDEPS_H
#ifdef __CYGWIN__
# undef _WIN32
#endif
#include <errno.h>
#include <string>
#include <vector>
// Include this before open/close/unlink are defined as macros below.
#include <android-base/errors.h>
#include <android-base/macros.h>
#include <android-base/unique_fd.h>
#include <android-base/utf8.h>
#include "sysdeps/errno.h"
#include "sysdeps/network.h"
#include "sysdeps/stat.h"
// Some printf-like functions are implemented in terms of
// android::base::StringAppendV, so they should use the same attribute for
// compile-time format string checking. On Windows, if the mingw version of
// vsnprintf is used in StringAppendV, use `gnu_printf' which allows z in %zd
// and PRIu64 (and related) to be recognized by the compile-time checking.
#define ADB_FORMAT_ARCHETYPE __printf__
#ifdef __USE_MINGW_ANSI_STDIO
#if __USE_MINGW_ANSI_STDIO
#undef ADB_FORMAT_ARCHETYPE
#define ADB_FORMAT_ARCHETYPE gnu_printf
#endif
#endif
#ifdef _WIN32
// Clang-only nullability specifiers
#define _Nonnull
#define _Nullable
#include <ctype.h>
#include <direct.h>
#include <dirent.h>
#include <errno.h>
#include <fcntl.h>
#include <io.h>
#include <process.h>
#include <sys/stat.h>
#include <utime.h>
#include <winsock2.h>
#include <windows.h>
#include <ws2tcpip.h>
#include <memory> // unique_ptr
#include <string>
#include "fdevent.h"
#define OS_PATH_SEPARATORS "\\/"
#define OS_PATH_SEPARATOR '\\'
#define OS_PATH_SEPARATOR_STR "\\"
#define ENV_PATH_SEPARATOR_STR ";"
static __inline__ bool adb_is_separator(char c) {
return c == '\\' || c == '/';
}
static __inline__ int adb_thread_setname(const std::string& name) {
// TODO: See https://msdn.microsoft.com/en-us/library/xcb2z8hs.aspx for how to set
// the thread name in Windows. Unfortunately, it only works during debugging, but
// our build process doesn't generate PDB files needed for debugging.
return 0;
}
static __inline__ unsigned long adb_thread_id()
{
return GetCurrentThreadId();
}
static __inline__ void close_on_exec(int fd)
{
/* nothing really */
}
extern int adb_unlink(const char* path);
#undef unlink
#define unlink ___xxx_unlink
extern int adb_mkdir(const std::string& path, int mode);
#undef mkdir
#define mkdir ___xxx_mkdir
// See the comments for the !defined(_WIN32) versions of adb_*().
extern int adb_open(const char* path, int options);
extern int adb_creat(const char* path, int mode);
extern int adb_read(int fd, void* buf, int len);
extern int adb_write(int fd, const void* buf, int len);
extern int adb_lseek(int fd, int pos, int where);
extern int adb_shutdown(int fd);
extern int adb_close(int fd);
extern int adb_register_socket(SOCKET s);
// See the comments for the !defined(_WIN32) version of unix_close().
static __inline__ int unix_close(int fd)
{
return close(fd);
}
#undef close
#define close ____xxx_close
// Like unix_read(), but may return EINTR.
extern int unix_read_interruptible(int fd, void* buf, size_t len);
// See the comments for the !defined(_WIN32) version of unix_read().
static __inline__ int unix_read(int fd, void* buf, size_t len) {
return TEMP_FAILURE_RETRY(unix_read_interruptible(fd, buf, len));
}
#undef read
#define read ___xxx_read
// See the comments for the !defined(_WIN32) version of unix_write().
static __inline__ int unix_write(int fd, const void* buf, size_t len)
{
return write(fd, buf, len);
}
#undef write
#define write ___xxx_write
// See the comments for the !defined(_WIN32) version of adb_open_mode().
static __inline__ int adb_open_mode(const char* path, int options, int mode)
{
return adb_open(path, options);
}
// See the comments for the !defined(_WIN32) version of unix_open().
extern int unix_open(const char* path, int options, ...);
#define open ___xxx_unix_open
// Checks if |fd| corresponds to a console.
// Standard Windows isatty() returns 1 for both console FDs and character
// devices like NUL. unix_isatty() performs some extra checking to only match
// console FDs.
// |fd| must be a real file descriptor, meaning STDxx_FILENO or unix_open() FDs
// will work but adb_open() FDs will not. Additionally the OS handle associated
// with |fd| must have GENERIC_READ access (which console FDs have by default).
// Returns 1 if |fd| is a console FD, 0 otherwise. The value of errno after
// calling this function is unreliable and should not be used.
int unix_isatty(int fd);
#define isatty ___xxx_isatty
int network_inaddr_any_server(int port, int type, std::string* error);
inline int network_local_client(const char* name, int namespace_id, int type, std::string* error) {
abort();
}
inline int network_local_server(const char* name, int namespace_id, int type, std::string* error) {
abort();
}
int network_connect(const std::string& host, int port, int type, int timeout,
std::string* error);
extern int adb_socket_accept(int serverfd, struct sockaddr* addr, socklen_t *addrlen);
#undef accept
#define accept ___xxx_accept
// Returns the local port number of a bound socket, or -1 on failure.
int adb_socket_get_local_port(int fd);
extern int adb_setsockopt(int fd, int level, int optname, const void* optval, socklen_t optlen);
#undef setsockopt
#define setsockopt ___xxx_setsockopt
extern int adb_socketpair( int sv[2] );
struct adb_pollfd {
int fd;
short events;
short revents;
};
extern int adb_poll(adb_pollfd* fds, size_t nfds, int timeout);
#define poll ___xxx_poll
static __inline__ int adb_is_absolute_host_path(const char* path) {
return isalpha(path[0]) && path[1] == ':' && path[2] == '\\';
}
// UTF-8 versions of POSIX APIs.
extern DIR* adb_opendir(const char* dirname);
extern struct dirent* adb_readdir(DIR* dir);
extern int adb_closedir(DIR* dir);
extern int adb_utime(const char *, struct utimbuf *);
extern int adb_chmod(const char *, int);
extern int adb_vfprintf(FILE *stream, const char *format, va_list ap)
__attribute__((__format__(ADB_FORMAT_ARCHETYPE, 2, 0)));
extern int adb_vprintf(const char *format, va_list ap)
__attribute__((__format__(ADB_FORMAT_ARCHETYPE, 1, 0)));
extern int adb_fprintf(FILE *stream, const char *format, ...)
__attribute__((__format__(ADB_FORMAT_ARCHETYPE, 2, 3)));
extern int adb_printf(const char *format, ...)
__attribute__((__format__(ADB_FORMAT_ARCHETYPE, 1, 2)));
extern int adb_fputs(const char* buf, FILE* stream);
extern int adb_fputc(int ch, FILE* stream);
extern int adb_putchar(int ch);
extern int adb_puts(const char* buf);
extern size_t adb_fwrite(const void* ptr, size_t size, size_t nmemb,
FILE* stream);
extern FILE* adb_fopen(const char* f, const char* m);
extern char* adb_getenv(const char* name);
extern char* adb_getcwd(char* buf, int size);
// Remap calls to POSIX APIs to our UTF-8 versions.
#define opendir adb_opendir
#define readdir adb_readdir
#define closedir adb_closedir
#define rewinddir rewinddir_utf8_not_yet_implemented
#define telldir telldir_utf8_not_yet_implemented
// Some compiler's C++ headers have members named seekdir, so we can't do the
// macro technique and instead cause a link error if seekdir is called.
inline void seekdir(DIR*, long) {
extern int seekdir_utf8_not_yet_implemented;
seekdir_utf8_not_yet_implemented = 1;
}
#define utime adb_utime
#define chmod adb_chmod
#define vfprintf adb_vfprintf
#define vprintf adb_vprintf
#define fprintf adb_fprintf
#define printf adb_printf
#define fputs adb_fputs
#define fputc adb_fputc
// putc may be a macro, so if so, undefine it, so that we can redefine it.
#undef putc
#define putc(c, s) adb_fputc(c, s)
#define putchar adb_putchar
#define puts adb_puts
#define fwrite adb_fwrite
#define fopen adb_fopen
#define freopen freopen_utf8_not_yet_implemented
#define getenv adb_getenv
#define putenv putenv_utf8_not_yet_implemented
#define setenv setenv_utf8_not_yet_implemented
#define unsetenv unsetenv_utf8_not_yet_implemented
#define getcwd adb_getcwd
// Helper class to convert UTF-16 argv from wmain() to UTF-8 args that can be
// passed to main().
class NarrowArgs {
public:
NarrowArgs(int argc, wchar_t** argv);
~NarrowArgs();
inline char** data() {
return narrow_args;
}
private:
char** narrow_args;
};
// Windows HANDLE values only use 32-bits of the type, even on 64-bit machines,
// so they can fit in an int. To convert back, we just need to sign-extend.
// https://msdn.microsoft.com/en-us/library/windows/desktop/aa384203%28v=vs.85%29.aspx
// Note that this does not make a HANDLE value work with APIs like open(), nor
// does this make a value from open() passable to APIs taking a HANDLE. This
// just lets you take a HANDLE, pass it around as an int, and then use it again
// as a HANDLE.
inline int cast_handle_to_int(const HANDLE h) {
// truncate
return static_cast<int>(reinterpret_cast<INT_PTR>(h));
}
inline HANDLE cast_int_to_handle(const int fd) {
// sign-extend
return reinterpret_cast<HANDLE>(static_cast<INT_PTR>(fd));
}
// Deleter for unique_handle. Adapted from many sources, including:
// http://stackoverflow.com/questions/14841396/stdunique-ptr-deleters-and-the-win32-api
// https://visualstudiomagazine.com/articles/2013/09/01/get-a-handle-on-the-windows-api.aspx
class handle_deleter {
public:
typedef HANDLE pointer;
void operator()(HANDLE h);
};
// Like std::unique_ptr, but for Windows HANDLE objects that should be
// CloseHandle()'d. Operator bool() only checks if the handle != nullptr,
// but does not check if the handle != INVALID_HANDLE_VALUE.
typedef std::unique_ptr<HANDLE, handle_deleter> unique_handle;
namespace internal {
size_t ParseCompleteUTF8(const char* first, const char* last, std::vector<char>* remaining_bytes);
}
#else /* !_WIN32 a.k.a. Unix */
#include <cutils/sockets.h>
#include <cutils/threads.h>
#include <fcntl.h>
#include <poll.h>
#include <signal.h>
#include <sys/stat.h>
#include <sys/wait.h>
#include <pthread.h>
#include <unistd.h>
#include <fcntl.h>
#include <stdarg.h>
#include <netdb.h>
#include <netinet/in.h>
#include <netinet/tcp.h>
#include <string.h>
#include <unistd.h>
#include <string>
#define OS_PATH_SEPARATORS "/"
#define OS_PATH_SEPARATOR '/'
#define OS_PATH_SEPARATOR_STR "/"
#define ENV_PATH_SEPARATOR_STR ":"
static __inline__ bool adb_is_separator(char c) {
return c == '/';
}
static __inline__ void close_on_exec(int fd)
{
fcntl( fd, F_SETFD, FD_CLOEXEC );
}
// Open a file and return a file descriptor that may be used with unix_read(),
// unix_write(), unix_close(), but not adb_read(), adb_write(), adb_close().
//
// On Unix, this is based on open(), so the file descriptor is a real OS file
// descriptor, but the Windows implementation (in sysdeps_win32.cpp) returns a
// file descriptor that can only be used with C Runtime APIs (which are wrapped
// by unix_read(), unix_write(), unix_close()). Also, the C Runtime has
// configurable CR/LF translation which defaults to text mode, but is settable
// with _setmode().
static __inline__ int unix_open(const char* path, int options,...)
{
if ((options & O_CREAT) == 0)
{
return TEMP_FAILURE_RETRY( open(path, options) );
}
else
{
int mode;
va_list args;
va_start( args, options );
mode = va_arg( args, int );
va_end( args );
return TEMP_FAILURE_RETRY( open( path, options, mode ) );
}
}
// Similar to the two-argument adb_open(), but takes a mode parameter for file
// creation. See adb_open() for more info.
static __inline__ int adb_open_mode( const char* pathname, int options, int mode )
{
return TEMP_FAILURE_RETRY( open( pathname, options, mode ) );
}
// Open a file and return a file descriptor that may be used with adb_read(),
// adb_write(), adb_close(), but not unix_read(), unix_write(), unix_close().
//
// On Unix, this is based on open(), but the Windows implementation (in
// sysdeps_win32.cpp) uses Windows native file I/O and bypasses the C Runtime
// and its CR/LF translation. The returned file descriptor should be used with
// adb_read(), adb_write(), adb_close(), etc.
static __inline__ int adb_open( const char* pathname, int options )
{
int fd = TEMP_FAILURE_RETRY( open( pathname, options ) );
if (fd < 0)
return -1;
close_on_exec( fd );
return fd;
}
#undef open
#define open ___xxx_open
static __inline__ int adb_shutdown(int fd)
{
return shutdown(fd, SHUT_RDWR);
}
static __inline__ int adb_shutdown(int fd, int direction)
{
return shutdown(fd, direction);
}
#undef shutdown
#define shutdown ____xxx_shutdown
// Closes a file descriptor that came from adb_open() or adb_open_mode(), but
// not designed to take a file descriptor from unix_open(). See the comments
// for adb_open() for more info.
__inline__ int adb_close(int fd) {
return close(fd);
}
#undef close
#define close ____xxx_close
// On Windows, ADB has an indirection layer for file descriptors. If we get a
// Win32 SOCKET object from an external library, we have to map it in to that
// indirection layer, which this does.
__inline__ int adb_register_socket(int s) {
return s;
}
static __inline__ int adb_read(int fd, void* buf, size_t len)
{
return TEMP_FAILURE_RETRY( read( fd, buf, len ) );
}
// Like unix_read(), but does not handle EINTR.
static __inline__ int unix_read_interruptible(int fd, void* buf, size_t len) {
return read(fd, buf, len);
}
#undef read
#define read ___xxx_read
static __inline__ int adb_write(int fd, const void* buf, size_t len)
{
return TEMP_FAILURE_RETRY( write( fd, buf, len ) );
}
#undef write
#define write ___xxx_write
static __inline__ int adb_lseek(int fd, int pos, int where)
{
return lseek(fd, pos, where);
}
#undef lseek
#define lseek ___xxx_lseek
static __inline__ int adb_unlink(const char* path)
{
return unlink(path);
}
#undef unlink
#define unlink ___xxx_unlink
static __inline__ int adb_creat(const char* path, int mode)
{
int fd = TEMP_FAILURE_RETRY( creat( path, mode ) );
if ( fd < 0 )
return -1;
close_on_exec(fd);
return fd;
}
#undef creat
#define creat ___xxx_creat
static __inline__ int unix_isatty(int fd) {
return isatty(fd);
}
#define isatty ___xxx_isatty
// Helper for network_* functions.
inline int _fd_set_error_str(int fd, std::string* error) {
if (fd == -1) {
*error = strerror(errno);
}
return fd;
}
inline int network_inaddr_any_server(int port, int type, std::string* error) {
return _fd_set_error_str(socket_inaddr_any_server(port, type), error);
}
inline int network_local_client(const char* name, int namespace_id, int type, std::string* error) {
return _fd_set_error_str(socket_local_client(name, namespace_id, type), error);
}
inline int network_local_server(const char* name, int namespace_id, int type, std::string* error) {
return _fd_set_error_str(socket_local_server(name, namespace_id, type), error);
}
inline int network_connect(const std::string& host, int port, int type,
int timeout, std::string* error) {
int getaddrinfo_error = 0;
int fd = socket_network_client_timeout(host.c_str(), port, type, timeout,
&getaddrinfo_error);
if (fd != -1) {
return fd;
}
if (getaddrinfo_error != 0) {
*error = gai_strerror(getaddrinfo_error);
} else {
*error = strerror(errno);
}
return -1;
}
static __inline__ int adb_socket_accept(int serverfd, struct sockaddr* addr, socklen_t *addrlen)
{
int fd;
fd = TEMP_FAILURE_RETRY( accept( serverfd, addr, addrlen ) );
if (fd >= 0)
close_on_exec(fd);
return fd;
}
#undef accept
#define accept ___xxx_accept
inline int adb_socket_get_local_port(int fd) {
return socket_get_local_port(fd);
}
// Operate on a file descriptor returned from unix_open() or a well-known file
// descriptor such as STDIN_FILENO, STDOUT_FILENO, STDERR_FILENO.
//
// On Unix, unix_read(), unix_write(), unix_close() map to adb_read(),
// adb_write(), adb_close() (which all map to Unix system calls), but the
// Windows implementations (in the ifdef above and in sysdeps_win32.cpp) call
// into the C Runtime and its configurable CR/LF translation (which is settable
// via _setmode()).
#define unix_read adb_read
#define unix_write adb_write
#define unix_close adb_close
static __inline__ int adb_thread_setname(const std::string& name) {
#ifdef __APPLE__
return pthread_setname_np(name.c_str());
#else
// Both bionic and glibc's pthread_setname_np fails rather than truncating long strings.
// glibc doesn't have strlcpy, so we have to fake it.
char buf[16]; // MAX_TASK_COMM_LEN, but that's not exported by the kernel headers.
strncpy(buf, name.c_str(), sizeof(buf) - 1);
buf[sizeof(buf) - 1] = '\0';
return pthread_setname_np(pthread_self(), buf);
#endif
}
static __inline__ int adb_setsockopt( int fd, int level, int optname, const void* optval, socklen_t optlen )
{
return setsockopt( fd, level, optname, optval, optlen );
}
#undef setsockopt
#define setsockopt ___xxx_setsockopt
static __inline__ int unix_socketpair( int d, int type, int protocol, int sv[2] )
{
return socketpair( d, type, protocol, sv );
}
static __inline__ int adb_socketpair( int sv[2] )
{
int rc;
rc = unix_socketpair( AF_UNIX, SOCK_STREAM, 0, sv );
if (rc < 0)
return -1;
close_on_exec( sv[0] );
close_on_exec( sv[1] );
return 0;
}
#undef socketpair
#define socketpair ___xxx_socketpair
typedef struct pollfd adb_pollfd;
static __inline__ int adb_poll(adb_pollfd* fds, size_t nfds, int timeout) {
return TEMP_FAILURE_RETRY(poll(fds, nfds, timeout));
}
#define poll ___xxx_poll
static __inline__ int adb_mkdir(const std::string& path, int mode)
{
return mkdir(path.c_str(), mode);
}
#undef mkdir
#define mkdir ___xxx_mkdir
static __inline__ int adb_is_absolute_host_path(const char* path) {
return path[0] == '/';
}
static __inline__ unsigned long adb_thread_id()
{
return (unsigned long)gettid();
}
#endif /* !_WIN32 */
static inline void disable_tcp_nagle(int fd) {
int off = 1;
adb_setsockopt(fd, IPPROTO_TCP, TCP_NODELAY, &off, sizeof(off));
}
// Sets TCP socket |fd| to send a keepalive TCP message every |interval_sec| seconds. Set
// |interval_sec| to 0 to disable keepalives. If keepalives are enabled, the connection will be
// configured to drop after 10 missed keepalives. Returns true on success.
bool set_tcp_keepalive(int fd, int interval_sec);
#if defined(_WIN32)
// Win32 defines ERROR, which we don't need, but which conflicts with google3 logging.
#undef ERROR
#endif
#endif /* _ADB_SYSDEPS_H */
|