1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
|
/*
* Copyright (C) 2011 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef __TRANSPORT_H
#define __TRANSPORT_H
#include <sys/types.h>
#include <atomic>
#include <chrono>
#include <condition_variable>
#include <deque>
#include <functional>
#include <list>
#include <memory>
#include <mutex>
#include <string>
#include <thread>
#include <unordered_set>
#include <android-base/macros.h>
#include <android-base/thread_annotations.h>
#include <openssl/rsa.h>
#include "adb.h"
#include "adb_unique_fd.h"
typedef std::unordered_set<std::string> FeatureSet;
const FeatureSet& supported_features();
// Encodes and decodes FeatureSet objects into human-readable strings.
std::string FeatureSetToString(const FeatureSet& features);
FeatureSet StringToFeatureSet(const std::string& features_string);
// Returns true if both local features and |feature_set| support |feature|.
bool CanUseFeature(const FeatureSet& feature_set, const std::string& feature);
// Do not use any of [:;=,] in feature strings, they have special meaning
// in the connection banner.
extern const char* const kFeatureShell2;
// The 'cmd' command is available
extern const char* const kFeatureCmd;
extern const char* const kFeatureStat2;
// The server is running with libusb enabled.
extern const char* const kFeatureLibusb;
// The server supports `push --sync`.
extern const char* const kFeaturePushSync;
TransportId NextTransportId();
// Abstraction for a non-blocking packet transport.
struct Connection {
Connection() = default;
virtual ~Connection() = default;
void SetTransportName(std::string transport_name) {
transport_name_ = std::move(transport_name);
}
using ReadCallback = std::function<bool(Connection*, std::unique_ptr<apacket>)>;
void SetReadCallback(ReadCallback callback) {
CHECK(!read_callback_);
read_callback_ = callback;
}
// Called after the Connection has terminated, either by an error or because Stop was called.
using ErrorCallback = std::function<void(Connection*, const std::string&)>;
void SetErrorCallback(ErrorCallback callback) {
CHECK(!error_callback_);
error_callback_ = callback;
}
virtual bool Write(std::unique_ptr<apacket> packet) = 0;
virtual void Start() = 0;
virtual void Stop() = 0;
std::string transport_name_;
ReadCallback read_callback_;
ErrorCallback error_callback_;
static std::unique_ptr<Connection> FromFd(unique_fd fd);
};
// Abstraction for a blocking packet transport.
struct BlockingConnection {
BlockingConnection() = default;
BlockingConnection(const BlockingConnection& copy) = delete;
BlockingConnection(BlockingConnection&& move) = delete;
// Destroy a BlockingConnection. Formerly known as 'Close' in atransport.
virtual ~BlockingConnection() = default;
// Read/Write a packet. These functions are concurrently called from a transport's reader/writer
// threads.
virtual bool Read(apacket* packet) = 0;
virtual bool Write(apacket* packet) = 0;
// Terminate a connection.
// This method must be thread-safe, and must cause concurrent Reads/Writes to terminate.
// Formerly known as 'Kick' in atransport.
virtual void Close() = 0;
};
struct BlockingConnectionAdapter : public Connection {
explicit BlockingConnectionAdapter(std::unique_ptr<BlockingConnection> connection);
virtual ~BlockingConnectionAdapter();
virtual bool Write(std::unique_ptr<apacket> packet) override final;
virtual void Start() override final;
virtual void Stop() override final;
bool started_ GUARDED_BY(mutex_) = false;
bool stopped_ GUARDED_BY(mutex_) = false;
std::unique_ptr<BlockingConnection> underlying_;
std::thread read_thread_ GUARDED_BY(mutex_);
std::thread write_thread_ GUARDED_BY(mutex_);
std::deque<std::unique_ptr<apacket>> write_queue_ GUARDED_BY(mutex_);
std::mutex mutex_;
std::condition_variable cv_;
std::once_flag error_flag_;
};
struct FdConnection : public BlockingConnection {
explicit FdConnection(unique_fd fd) : fd_(std::move(fd)) {}
bool Read(apacket* packet) override final;
bool Write(apacket* packet) override final;
void Close() override;
private:
unique_fd fd_;
};
struct UsbConnection : public BlockingConnection {
explicit UsbConnection(usb_handle* handle) : handle_(handle) {}
~UsbConnection();
bool Read(apacket* packet) override final;
bool Write(apacket* packet) override final;
void Close() override final;
usb_handle* handle_;
};
// Waits for a transport's connection to be not pending. This is a separate
// object so that the transport can be destroyed and another thread can be
// notified of it in a race-free way.
class ConnectionWaitable {
public:
ConnectionWaitable() = default;
~ConnectionWaitable() = default;
// Waits until the first CNXN packet has been received by the owning
// atransport, or the specified timeout has elapsed. Can be called from any
// thread.
//
// Returns true if the CNXN packet was received in a timely fashion, false
// otherwise.
bool WaitForConnection(std::chrono::milliseconds timeout);
// Can be called from any thread when the connection stops being pending.
// Only the first invocation will be acknowledged, the rest will be no-ops.
void SetConnectionEstablished(bool success);
private:
bool connection_established_ GUARDED_BY(mutex_) = false;
bool connection_established_ready_ GUARDED_BY(mutex_) = false;
std::mutex mutex_;
std::condition_variable cv_;
DISALLOW_COPY_AND_ASSIGN(ConnectionWaitable);
};
class atransport {
public:
// TODO(danalbert): We expose waaaaaaay too much stuff because this was
// historically just a struct, but making the whole thing a more idiomatic
// class in one go is a very large change. Given how bad our testing is,
// it's better to do this piece by piece.
using ReconnectCallback = std::function<bool(atransport*)>;
atransport(ReconnectCallback reconnect, ConnectionState state)
: id(NextTransportId()),
kicked_(false),
connection_state_(state),
connection_waitable_(std::make_shared<ConnectionWaitable>()),
connection_(nullptr),
reconnect_(std::move(reconnect)) {
// Initialize protocol to min version for compatibility with older versions.
// Version will be updated post-connect.
protocol_version = A_VERSION_MIN;
max_payload = MAX_PAYLOAD;
}
atransport(ConnectionState state = kCsOffline)
: atransport([](atransport*) { return false; }, state) {}
virtual ~atransport();
int Write(apacket* p);
void Kick();
bool kicked() const { return kicked_; }
// ConnectionState can be read by all threads, but can only be written in the main thread.
ConnectionState GetConnectionState() const;
void SetConnectionState(ConnectionState state);
void SetConnection(std::unique_ptr<Connection> connection);
std::shared_ptr<Connection> connection() {
std::lock_guard<std::mutex> lock(mutex_);
return connection_;
}
const TransportId id;
size_t ref_count = 0;
bool online = false;
TransportType type = kTransportAny;
// Used to identify transports for clients.
std::string serial;
std::string product;
std::string model;
std::string device;
std::string devpath;
bool IsTcpDevice() const { return type == kTransportLocal; }
#if ADB_HOST
std::shared_ptr<RSA> NextKey();
#endif
char token[TOKEN_SIZE] = {};
size_t failed_auth_attempts = 0;
std::string serial_name() const { return !serial.empty() ? serial : "<unknown>"; }
std::string connection_state_name() const;
void update_version(int version, size_t payload);
int get_protocol_version() const;
size_t get_max_payload() const;
const FeatureSet& features() const {
return features_;
}
bool has_feature(const std::string& feature) const;
// Loads the transport's feature set from the given string.
void SetFeatures(const std::string& features_string);
void AddDisconnect(adisconnect* disconnect);
void RemoveDisconnect(adisconnect* disconnect);
void RunDisconnects();
// Returns true if |target| matches this transport. A matching |target| can be any of:
// * <serial>
// * <devpath>
// * product:<product>
// * model:<model>
// * device:<device>
//
// If this is a local transport, serial will also match [tcp:|udp:]<hostname>[:port] targets.
// For example, serial "100.100.100.100:5555" would match any of:
// * 100.100.100.100
// * tcp:100.100.100.100
// * udp:100.100.100.100:5555
// This is to make it easier to use the same network target for both fastboot and adb.
bool MatchesTarget(const std::string& target) const;
// Notifies that the atransport is no longer waiting for the connection
// being established.
void SetConnectionEstablished(bool success);
// Gets a shared reference to the ConnectionWaitable.
std::shared_ptr<ConnectionWaitable> connection_waitable() { return connection_waitable_; }
// Attempts to reconnect with the underlying Connection. Returns true if the
// reconnection attempt succeeded.
bool Reconnect();
private:
std::atomic<bool> kicked_;
// A set of features transmitted in the banner with the initial connection.
// This is stored in the banner as 'features=feature0,feature1,etc'.
FeatureSet features_;
int protocol_version;
size_t max_payload;
// A list of adisconnect callbacks called when the transport is kicked.
std::list<adisconnect*> disconnects_;
std::atomic<ConnectionState> connection_state_;
#if ADB_HOST
std::deque<std::shared_ptr<RSA>> keys_;
#endif
// A sharable object that can be used to wait for the atransport's
// connection to be established.
std::shared_ptr<ConnectionWaitable> connection_waitable_;
// The underlying connection object.
std::shared_ptr<Connection> connection_ GUARDED_BY(mutex_);
// A callback that will be invoked when the atransport needs to reconnect.
ReconnectCallback reconnect_;
std::mutex mutex_;
DISALLOW_COPY_AND_ASSIGN(atransport);
};
/*
* Obtain a transport from the available transports.
* If serial is non-null then only the device with that serial will be chosen.
* If transport_id is non-zero then only the device with that transport ID will be chosen.
* If multiple devices/emulators would match, *is_ambiguous (if non-null)
* is set to true and nullptr returned.
* If no suitable transport is found, error is set and nullptr returned.
*/
atransport* acquire_one_transport(TransportType type, const char* serial, TransportId transport_id,
bool* is_ambiguous, std::string* error_out,
bool accept_any_state = false);
void kick_transport(atransport* t);
void update_transports(void);
// Iterates across all of the current and pending transports.
// Stops iteration and returns false if fn returns false, otherwise returns true.
bool iterate_transports(std::function<bool(const atransport*)> fn);
void init_reconnect_handler(void);
void init_transport_registration(void);
void init_mdns_transport_discovery(void);
std::string list_transports(bool long_listing);
atransport* find_transport(const char* serial);
void kick_all_tcp_devices();
void kick_all_transports();
void register_usb_transport(usb_handle* h, const char* serial,
const char* devpath, unsigned writeable);
/* Connect to a network address and register it as a device */
void connect_device(const std::string& address, std::string* response);
/* cause new transports to be init'd and added to the list */
int register_socket_transport(unique_fd s, std::string serial, int port, int local,
atransport::ReconnectCallback reconnect);
// This should only be used for transports with connection_state == kCsNoPerm.
void unregister_usb_transport(usb_handle* usb);
bool check_header(apacket* p, atransport* t);
void close_usb_devices();
void close_usb_devices(std::function<bool(const atransport*)> predicate);
void send_packet(apacket* p, atransport* t);
asocket* create_device_tracker(bool long_output);
#endif /* __TRANSPORT_H */
|