summaryrefslogtreecommitdiffstats
blob: 2f697a1cc139846179b29b005d39b5b8a1ec2fba (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "android-base/file.h"

#include <errno.h>
#include <fcntl.h>
#include <libgen.h>
#include <sys/stat.h>
#include <sys/types.h>
#include <unistd.h>

#include <memory>
#include <mutex>
#include <string>
#include <vector>

#include "android-base/logging.h"
#include "android-base/macros.h"  // For TEMP_FAILURE_RETRY on Darwin.
#include "android-base/unique_fd.h"
#include "android-base/utf8.h"

#if defined(__APPLE__)
#include <mach-o/dyld.h>
#endif
#if defined(_WIN32)
#include <windows.h>
#define O_CLOEXEC O_NOINHERIT
#define O_NOFOLLOW 0
#endif

namespace android {
namespace base {

// Versions of standard library APIs that support UTF-8 strings.
using namespace android::base::utf8;

bool ReadFdToString(int fd, std::string* content) {
  content->clear();

  // Although original we had small files in mind, this code gets used for
  // very large files too, where the std::string growth heuristics might not
  // be suitable. https://code.google.com/p/android/issues/detail?id=258500.
  struct stat sb;
  if (fstat(fd, &sb) != -1 && sb.st_size > 0) {
    content->reserve(sb.st_size);
  }

  char buf[BUFSIZ];
  ssize_t n;
  while ((n = TEMP_FAILURE_RETRY(read(fd, &buf[0], sizeof(buf)))) > 0) {
    content->append(buf, n);
  }
  return (n == 0) ? true : false;
}

bool ReadFileToString(const std::string& path, std::string* content, bool follow_symlinks) {
  content->clear();

  int flags = O_RDONLY | O_CLOEXEC | O_BINARY | (follow_symlinks ? 0 : O_NOFOLLOW);
  android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(path.c_str(), flags)));
  if (fd == -1) {
    return false;
  }
  return ReadFdToString(fd, content);
}

bool WriteStringToFd(const std::string& content, int fd) {
  const char* p = content.data();
  size_t left = content.size();
  while (left > 0) {
    ssize_t n = TEMP_FAILURE_RETRY(write(fd, p, left));
    if (n == -1) {
      return false;
    }
    p += n;
    left -= n;
  }
  return true;
}

static bool CleanUpAfterFailedWrite(const std::string& path) {
  // Something went wrong. Let's not leave a corrupt file lying around.
  int saved_errno = errno;
  unlink(path.c_str());
  errno = saved_errno;
  return false;
}

#if !defined(_WIN32)
bool WriteStringToFile(const std::string& content, const std::string& path,
                       mode_t mode, uid_t owner, gid_t group,
                       bool follow_symlinks) {
  int flags = O_WRONLY | O_CREAT | O_TRUNC | O_CLOEXEC | O_BINARY |
              (follow_symlinks ? 0 : O_NOFOLLOW);
  android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(path.c_str(), flags, mode)));
  if (fd == -1) {
    PLOG(ERROR) << "android::WriteStringToFile open failed";
    return false;
  }

  // We do an explicit fchmod here because we assume that the caller really
  // meant what they said and doesn't want the umask-influenced mode.
  if (fchmod(fd, mode) == -1) {
    PLOG(ERROR) << "android::WriteStringToFile fchmod failed";
    return CleanUpAfterFailedWrite(path);
  }
  if (fchown(fd, owner, group) == -1) {
    PLOG(ERROR) << "android::WriteStringToFile fchown failed";
    return CleanUpAfterFailedWrite(path);
  }
  if (!WriteStringToFd(content, fd)) {
    PLOG(ERROR) << "android::WriteStringToFile write failed";
    return CleanUpAfterFailedWrite(path);
  }
  return true;
}
#endif

bool WriteStringToFile(const std::string& content, const std::string& path,
                       bool follow_symlinks) {
  int flags = O_WRONLY | O_CREAT | O_TRUNC | O_CLOEXEC | O_BINARY |
              (follow_symlinks ? 0 : O_NOFOLLOW);
  android::base::unique_fd fd(TEMP_FAILURE_RETRY(open(path.c_str(), flags, 0666)));
  if (fd == -1) {
    return false;
  }
  return WriteStringToFd(content, fd) || CleanUpAfterFailedWrite(path);
}

bool ReadFully(int fd, void* data, size_t byte_count) {
  uint8_t* p = reinterpret_cast<uint8_t*>(data);
  size_t remaining = byte_count;
  while (remaining > 0) {
    ssize_t n = TEMP_FAILURE_RETRY(read(fd, p, remaining));
    if (n <= 0) return false;
    p += n;
    remaining -= n;
  }
  return true;
}

#if defined(_WIN32)
// Windows implementation of pread. Note that this DOES move the file descriptors read position,
// but it does so atomically.
static ssize_t pread(int fd, void* data, size_t byte_count, off64_t offset) {
  DWORD bytes_read;
  OVERLAPPED overlapped;
  memset(&overlapped, 0, sizeof(OVERLAPPED));
  overlapped.Offset = static_cast<DWORD>(offset);
  overlapped.OffsetHigh = static_cast<DWORD>(offset >> 32);
  if (!ReadFile(reinterpret_cast<HANDLE>(_get_osfhandle(fd)), data, static_cast<DWORD>(byte_count),
                &bytes_read, &overlapped)) {
    // In case someone tries to read errno (since this is masquerading as a POSIX call)
    errno = EIO;
    return -1;
  }
  return static_cast<ssize_t>(bytes_read);
}
#endif

bool ReadFullyAtOffset(int fd, void* data, size_t byte_count, off64_t offset) {
  uint8_t* p = reinterpret_cast<uint8_t*>(data);
  while (byte_count > 0) {
    ssize_t n = TEMP_FAILURE_RETRY(pread(fd, p, byte_count, offset));
    if (n <= 0) return false;
    p += n;
    byte_count -= n;
    offset += n;
  }
  return true;
}

bool WriteFully(int fd, const void* data, size_t byte_count) {
  const uint8_t* p = reinterpret_cast<const uint8_t*>(data);
  size_t remaining = byte_count;
  while (remaining > 0) {
    ssize_t n = TEMP_FAILURE_RETRY(write(fd, p, remaining));
    if (n == -1) return false;
    p += n;
    remaining -= n;
  }
  return true;
}

bool RemoveFileIfExists(const std::string& path, std::string* err) {
  struct stat st;
#if defined(_WIN32)
  //TODO: Windows version can't handle symbol link correctly.
  int result = stat(path.c_str(), &st);
  bool file_type_removable = (result == 0 && S_ISREG(st.st_mode));
#else
  int result = lstat(path.c_str(), &st);
  bool file_type_removable = (result == 0 && (S_ISREG(st.st_mode) || S_ISLNK(st.st_mode)));
#endif
  if (result == 0) {
    if (!file_type_removable) {
      if (err != nullptr) {
        *err = "is not a regular or symbol link file";
      }
      return false;
    }
    if (unlink(path.c_str()) == -1) {
      if (err != nullptr) {
        *err = strerror(errno);
      }
      return false;
    }
  }
  return true;
}

#if !defined(_WIN32)
bool Readlink(const std::string& path, std::string* result) {
  result->clear();

  // Most Linux file systems (ext2 and ext4, say) limit symbolic links to
  // 4095 bytes. Since we'll copy out into the string anyway, it doesn't
  // waste memory to just start there. We add 1 so that we can recognize
  // whether it actually fit (rather than being truncated to 4095).
  std::vector<char> buf(4095 + 1);
  while (true) {
    ssize_t size = readlink(path.c_str(), &buf[0], buf.size());
    // Unrecoverable error?
    if (size == -1) return false;
    // It fit! (If size == buf.size(), it may have been truncated.)
    if (static_cast<size_t>(size) < buf.size()) {
      result->assign(&buf[0], size);
      return true;
    }
    // Double our buffer and try again.
    buf.resize(buf.size() * 2);
  }
}
#endif

#if !defined(_WIN32)
bool Realpath(const std::string& path, std::string* result) {
  result->clear();

  char* realpath_buf = realpath(path.c_str(), nullptr);
  if (realpath_buf == nullptr) {
    return false;
  }
  result->assign(realpath_buf);
  free(realpath_buf);
  return true;
}
#endif

std::string GetExecutablePath() {
#if defined(__linux__)
  std::string path;
  android::base::Readlink("/proc/self/exe", &path);
  return path;
#elif defined(__APPLE__)
  char path[PATH_MAX + 1];
  uint32_t path_len = sizeof(path);
  int rc = _NSGetExecutablePath(path, &path_len);
  if (rc < 0) {
    std::unique_ptr<char> path_buf(new char[path_len]);
    _NSGetExecutablePath(path_buf.get(), &path_len);
    return path_buf.get();
  }
  return path;
#elif defined(_WIN32)
  char path[PATH_MAX + 1];
  DWORD result = GetModuleFileName(NULL, path, sizeof(path) - 1);
  if (result == 0 || result == sizeof(path) - 1) return "";
  path[PATH_MAX - 1] = 0;
  return path;
#else
#error unknown OS
#endif
}

std::string GetExecutableDirectory() {
  return Dirname(GetExecutablePath());
}

std::string Basename(const std::string& path) {
  // Copy path because basename may modify the string passed in.
  std::string result(path);

#if !defined(__BIONIC__)
  // Use lock because basename() may write to a process global and return a
  // pointer to that. Note that this locking strategy only works if all other
  // callers to basename in the process also grab this same lock, but its
  // better than nothing.  Bionic's basename returns a thread-local buffer.
  static std::mutex& basename_lock = *new std::mutex();
  std::lock_guard<std::mutex> lock(basename_lock);
#endif

  // Note that if std::string uses copy-on-write strings, &str[0] will cause
  // the copy to be made, so there is no chance of us accidentally writing to
  // the storage for 'path'.
  char* name = basename(&result[0]);

  // In case basename returned a pointer to a process global, copy that string
  // before leaving the lock.
  result.assign(name);

  return result;
}

std::string Dirname(const std::string& path) {
  // Copy path because dirname may modify the string passed in.
  std::string result(path);

#if !defined(__BIONIC__)
  // Use lock because dirname() may write to a process global and return a
  // pointer to that. Note that this locking strategy only works if all other
  // callers to dirname in the process also grab this same lock, but its
  // better than nothing.  Bionic's dirname returns a thread-local buffer.
  static std::mutex& dirname_lock = *new std::mutex();
  std::lock_guard<std::mutex> lock(dirname_lock);
#endif

  // Note that if std::string uses copy-on-write strings, &str[0] will cause
  // the copy to be made, so there is no chance of us accidentally writing to
  // the storage for 'path'.
  char* parent = dirname(&result[0]);

  // In case dirname returned a pointer to a process global, copy that string
  // before leaving the lock.
  result.assign(parent);

  return result;
}

}  // namespace base
}  // namespace android