1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
|
/*
* Copyright (C) 2015 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#pragma once
//
// Google-style C++ logging.
//
// This header provides a C++ stream interface to logging.
//
// To log:
//
// LOG(INFO) << "Some text; " << some_value;
//
// Replace `INFO` with any severity from `enum LogSeverity`.
//
// To log the result of a failed function and include the string
// representation of `errno` at the end:
//
// PLOG(ERROR) << "Write failed";
//
// The output will be something like `Write failed: I/O error`.
// Remember this as 'P' as in perror(3).
//
// To output your own types, simply implement operator<< as normal.
//
// By default, output goes to logcat on Android and stderr on the host.
// A process can use `SetLogger` to decide where all logging goes.
// Implementations are provided for logcat, stderr, and dmesg.
//
// By default, the process' name is used as the log tag.
// Code can choose a specific log tag by defining LOG_TAG
// before including this header.
// This header also provides assertions:
//
// CHECK(must_be_true);
// CHECK_EQ(a, b) << z_is_interesting_too;
// NOTE: For Windows, you must include logging.h after windows.h to allow the
// following code to suppress the evil ERROR macro:
#ifdef _WIN32
// windows.h includes wingdi.h which defines an evil macro ERROR.
#ifdef ERROR
#undef ERROR
#endif
#endif
#include <functional>
#include <memory>
#include <ostream>
#include "android-base/macros.h"
// Note: DO NOT USE DIRECTLY. Use LOG_TAG instead.
#ifdef _LOG_TAG_INTERNAL
#error "_LOG_TAG_INTERNAL must not be defined"
#endif
#ifdef LOG_TAG
#define _LOG_TAG_INTERNAL LOG_TAG
#else
#define _LOG_TAG_INTERNAL nullptr
#endif
namespace android {
namespace base {
enum LogSeverity {
VERBOSE,
DEBUG,
INFO,
WARNING,
ERROR,
FATAL_WITHOUT_ABORT,
FATAL,
};
enum LogId {
DEFAULT,
MAIN,
SYSTEM,
};
using LogFunction = std::function<void(LogId, LogSeverity, const char*, const char*,
unsigned int, const char*)>;
using AbortFunction = std::function<void(const char*)>;
// Loggers for use with InitLogging/SetLogger.
// Log to the kernel log (dmesg).
void KernelLogger(LogId, LogSeverity, const char*, const char*, unsigned int, const char*);
// Log to stderr in the full logcat format (with pid/tid/time/tag details).
void StderrLogger(LogId, LogSeverity, const char*, const char*, unsigned int, const char*);
// Log just the message to stdout/stderr (without pid/tid/time/tag details).
// The choice of stdout versus stderr is based on the severity.
// Errors are also prefixed by the program name (as with err(3)/error(3)).
// Useful for replacing printf(3)/perror(3)/err(3)/error(3) in command-line tools.
void StdioLogger(LogId, LogSeverity, const char*, const char*, unsigned int, const char*);
void DefaultAborter(const char* abort_message);
std::string GetDefaultTag();
void SetDefaultTag(const std::string& tag);
#ifdef __ANDROID__
// We expose this even though it is the default because a user that wants to
// override the default log buffer will have to construct this themselves.
class LogdLogger {
public:
explicit LogdLogger(LogId default_log_id = android::base::MAIN);
void operator()(LogId, LogSeverity, const char* tag, const char* file,
unsigned int line, const char* message);
private:
LogId default_log_id_;
};
#endif
// Configure logging based on ANDROID_LOG_TAGS environment variable.
// We need to parse a string that looks like
//
// *:v jdwp:d dalvikvm:d dalvikvm-gc:i dalvikvmi:i
//
// The tag (or '*' for the global level) comes first, followed by a colon and a
// letter indicating the minimum priority level we're expected to log. This can
// be used to reveal or conceal logs with specific tags.
#ifdef __ANDROID__
#define INIT_LOGGING_DEFAULT_LOGGER LogdLogger()
#else
#define INIT_LOGGING_DEFAULT_LOGGER StderrLogger
#endif
void InitLogging(char* argv[],
LogFunction&& logger = INIT_LOGGING_DEFAULT_LOGGER,
AbortFunction&& aborter = DefaultAborter);
#undef INIT_LOGGING_DEFAULT_LOGGER
// Replace the current logger.
void SetLogger(LogFunction&& logger);
// Replace the current aborter.
void SetAborter(AbortFunction&& aborter);
class ErrnoRestorer {
public:
ErrnoRestorer()
: saved_errno_(errno) {
}
~ErrnoRestorer() {
errno = saved_errno_;
}
// Allow this object to be used as part of && operation.
operator bool() const {
return true;
}
private:
const int saved_errno_;
DISALLOW_COPY_AND_ASSIGN(ErrnoRestorer);
};
// A helper macro that produces an expression that accepts both a qualified name and an
// unqualified name for a LogSeverity, and returns a LogSeverity value.
// Note: DO NOT USE DIRECTLY. This is an implementation detail.
#define SEVERITY_LAMBDA(severity) ([&]() { \
using ::android::base::VERBOSE; \
using ::android::base::DEBUG; \
using ::android::base::INFO; \
using ::android::base::WARNING; \
using ::android::base::ERROR; \
using ::android::base::FATAL_WITHOUT_ABORT; \
using ::android::base::FATAL; \
return (severity); }())
#ifdef __clang_analyzer__
// Clang's static analyzer does not see the conditional statement inside
// LogMessage's destructor that will abort on FATAL severity.
#define ABORT_AFTER_LOG_FATAL for (;; abort())
struct LogAbortAfterFullExpr {
~LogAbortAfterFullExpr() __attribute__((noreturn)) { abort(); }
explicit operator bool() const { return false; }
};
// Provides an expression that evaluates to the truthiness of `x`, automatically
// aborting if `c` is true.
#define ABORT_AFTER_LOG_EXPR_IF(c, x) (((c) && ::android::base::LogAbortAfterFullExpr()) || (x))
// Note to the static analyzer that we always execute FATAL logs in practice.
#define MUST_LOG_MESSAGE(severity) (SEVERITY_LAMBDA(severity) == ::android::base::FATAL)
#else
#define ABORT_AFTER_LOG_FATAL
#define ABORT_AFTER_LOG_EXPR_IF(c, x) (x)
#define MUST_LOG_MESSAGE(severity) false
#endif
#define ABORT_AFTER_LOG_FATAL_EXPR(x) ABORT_AFTER_LOG_EXPR_IF(true, x)
// Defines whether the given severity will be logged or silently swallowed.
#define WOULD_LOG(severity) \
(UNLIKELY((SEVERITY_LAMBDA(severity)) >= ::android::base::GetMinimumLogSeverity()) || \
MUST_LOG_MESSAGE(severity))
// Get an ostream that can be used for logging at the given severity and to the default
// destination.
//
// Notes:
// 1) This will not check whether the severity is high enough. One should use WOULD_LOG to filter
// usage manually.
// 2) This does not save and restore errno.
#define LOG_STREAM(severity) LOG_STREAM_TO(DEFAULT, severity)
// Get an ostream that can be used for logging at the given severity and to the
// given destination. The same notes as for LOG_STREAM apply.
#define LOG_STREAM_TO(dest, severity) \
::android::base::LogMessage(__FILE__, __LINE__, ::android::base::dest, \
SEVERITY_LAMBDA(severity), _LOG_TAG_INTERNAL, -1) \
.stream()
// Logs a message to logcat on Android otherwise to stderr. If the severity is
// FATAL it also causes an abort. For example:
//
// LOG(FATAL) << "We didn't expect to reach here";
#define LOG(severity) LOG_TO(DEFAULT, severity)
// Checks if we want to log something, and sets up appropriate RAII objects if
// so.
// Note: DO NOT USE DIRECTLY. This is an implementation detail.
#define LOGGING_PREAMBLE(severity) \
(WOULD_LOG(severity) && \
ABORT_AFTER_LOG_EXPR_IF((SEVERITY_LAMBDA(severity)) == ::android::base::FATAL, true) && \
::android::base::ErrnoRestorer())
// Logs a message to logcat with the specified log ID on Android otherwise to
// stderr. If the severity is FATAL it also causes an abort.
// Use an expression here so we can support the << operator following the macro,
// like "LOG(DEBUG) << xxx;".
#define LOG_TO(dest, severity) LOGGING_PREAMBLE(severity) && LOG_STREAM_TO(dest, severity)
// A variant of LOG that also logs the current errno value. To be used when
// library calls fail.
#define PLOG(severity) PLOG_TO(DEFAULT, severity)
// Behaves like PLOG, but logs to the specified log ID.
#define PLOG_TO(dest, severity) \
LOGGING_PREAMBLE(severity) && \
::android::base::LogMessage(__FILE__, __LINE__, ::android::base::dest, \
SEVERITY_LAMBDA(severity), _LOG_TAG_INTERNAL, errno) \
.stream()
// Marker that code is yet to be implemented.
#define UNIMPLEMENTED(level) \
LOG(level) << __PRETTY_FUNCTION__ << " unimplemented "
// Check whether condition x holds and LOG(FATAL) if not. The value of the
// expression x is only evaluated once. Extra logging can be appended using <<
// after. For example:
//
// CHECK(false == true) results in a log message of
// "Check failed: false == true".
#define CHECK(x) \
LIKELY((x)) || ABORT_AFTER_LOG_FATAL_EXPR(false) || \
::android::base::LogMessage(__FILE__, __LINE__, ::android::base::DEFAULT, \
::android::base::FATAL, _LOG_TAG_INTERNAL, -1) \
.stream() \
<< "Check failed: " #x << " "
// clang-format off
// Helper for CHECK_xx(x,y) macros.
#define CHECK_OP(LHS, RHS, OP) \
for (auto _values = ::android::base::MakeEagerEvaluator(LHS, RHS); \
UNLIKELY(!(_values.lhs OP _values.rhs)); \
/* empty */) \
ABORT_AFTER_LOG_FATAL \
::android::base::LogMessage(__FILE__, __LINE__, ::android::base::DEFAULT, \
::android::base::FATAL, _LOG_TAG_INTERNAL, -1) \
.stream() \
<< "Check failed: " << #LHS << " " << #OP << " " << #RHS << " (" #LHS "=" << _values.lhs \
<< ", " #RHS "=" << _values.rhs << ") "
// clang-format on
// Check whether a condition holds between x and y, LOG(FATAL) if not. The value
// of the expressions x and y is evaluated once. Extra logging can be appended
// using << after. For example:
//
// CHECK_NE(0 == 1, false) results in
// "Check failed: false != false (0==1=false, false=false) ".
#define CHECK_EQ(x, y) CHECK_OP(x, y, == )
#define CHECK_NE(x, y) CHECK_OP(x, y, != )
#define CHECK_LE(x, y) CHECK_OP(x, y, <= )
#define CHECK_LT(x, y) CHECK_OP(x, y, < )
#define CHECK_GE(x, y) CHECK_OP(x, y, >= )
#define CHECK_GT(x, y) CHECK_OP(x, y, > )
// clang-format off
// Helper for CHECK_STRxx(s1,s2) macros.
#define CHECK_STROP(s1, s2, sense) \
while (UNLIKELY((strcmp(s1, s2) == 0) != (sense))) \
ABORT_AFTER_LOG_FATAL \
::android::base::LogMessage(__FILE__, __LINE__, ::android::base::DEFAULT, \
::android::base::FATAL, _LOG_TAG_INTERNAL, -1) \
.stream() \
<< "Check failed: " << "\"" << (s1) << "\"" \
<< ((sense) ? " == " : " != ") << "\"" << (s2) << "\""
// clang-format on
// Check for string (const char*) equality between s1 and s2, LOG(FATAL) if not.
#define CHECK_STREQ(s1, s2) CHECK_STROP(s1, s2, true)
#define CHECK_STRNE(s1, s2) CHECK_STROP(s1, s2, false)
// Perform the pthread function call(args), LOG(FATAL) on error.
#define CHECK_PTHREAD_CALL(call, args, what) \
do { \
int rc = call args; \
if (rc != 0) { \
errno = rc; \
ABORT_AFTER_LOG_FATAL \
PLOG(FATAL) << #call << " failed for " << (what); \
} \
} while (false)
// CHECK that can be used in a constexpr function. For example:
//
// constexpr int half(int n) {
// return
// DCHECK_CONSTEXPR(n >= 0, , 0)
// CHECK_CONSTEXPR((n & 1) == 0),
// << "Extra debugging output: n = " << n, 0)
// n / 2;
// }
#define CHECK_CONSTEXPR(x, out, dummy) \
(UNLIKELY(!(x))) \
? (LOG(FATAL) << "Check failed: " << #x out, dummy) \
:
// DCHECKs are debug variants of CHECKs only enabled in debug builds. Generally
// CHECK should be used unless profiling identifies a CHECK as being in
// performance critical code.
#if defined(NDEBUG) && !defined(__clang_analyzer__)
static constexpr bool kEnableDChecks = false;
#else
static constexpr bool kEnableDChecks = true;
#endif
#define DCHECK(x) \
if (::android::base::kEnableDChecks) CHECK(x)
#define DCHECK_EQ(x, y) \
if (::android::base::kEnableDChecks) CHECK_EQ(x, y)
#define DCHECK_NE(x, y) \
if (::android::base::kEnableDChecks) CHECK_NE(x, y)
#define DCHECK_LE(x, y) \
if (::android::base::kEnableDChecks) CHECK_LE(x, y)
#define DCHECK_LT(x, y) \
if (::android::base::kEnableDChecks) CHECK_LT(x, y)
#define DCHECK_GE(x, y) \
if (::android::base::kEnableDChecks) CHECK_GE(x, y)
#define DCHECK_GT(x, y) \
if (::android::base::kEnableDChecks) CHECK_GT(x, y)
#define DCHECK_STREQ(s1, s2) \
if (::android::base::kEnableDChecks) CHECK_STREQ(s1, s2)
#define DCHECK_STRNE(s1, s2) \
if (::android::base::kEnableDChecks) CHECK_STRNE(s1, s2)
#if defined(NDEBUG) && !defined(__clang_analyzer__)
#define DCHECK_CONSTEXPR(x, out, dummy)
#else
#define DCHECK_CONSTEXPR(x, out, dummy) CHECK_CONSTEXPR(x, out, dummy)
#endif
// Temporary class created to evaluate the LHS and RHS, used with
// MakeEagerEvaluator to infer the types of LHS and RHS.
template <typename LHS, typename RHS>
struct EagerEvaluator {
constexpr EagerEvaluator(LHS l, RHS r) : lhs(l), rhs(r) {
}
LHS lhs;
RHS rhs;
};
// Helper function for CHECK_xx.
template <typename LHS, typename RHS>
constexpr EagerEvaluator<LHS, RHS> MakeEagerEvaluator(LHS lhs, RHS rhs) {
return EagerEvaluator<LHS, RHS>(lhs, rhs);
}
// Explicitly instantiate EagerEvalue for pointers so that char*s aren't treated
// as strings. To compare strings use CHECK_STREQ and CHECK_STRNE. We rely on
// signed/unsigned warnings to protect you against combinations not explicitly
// listed below.
#define EAGER_PTR_EVALUATOR(T1, T2) \
template <> \
struct EagerEvaluator<T1, T2> { \
EagerEvaluator(T1 l, T2 r) \
: lhs(reinterpret_cast<const void*>(l)), \
rhs(reinterpret_cast<const void*>(r)) { \
} \
const void* lhs; \
const void* rhs; \
}
EAGER_PTR_EVALUATOR(const char*, const char*);
EAGER_PTR_EVALUATOR(const char*, char*);
EAGER_PTR_EVALUATOR(char*, const char*);
EAGER_PTR_EVALUATOR(char*, char*);
EAGER_PTR_EVALUATOR(const unsigned char*, const unsigned char*);
EAGER_PTR_EVALUATOR(const unsigned char*, unsigned char*);
EAGER_PTR_EVALUATOR(unsigned char*, const unsigned char*);
EAGER_PTR_EVALUATOR(unsigned char*, unsigned char*);
EAGER_PTR_EVALUATOR(const signed char*, const signed char*);
EAGER_PTR_EVALUATOR(const signed char*, signed char*);
EAGER_PTR_EVALUATOR(signed char*, const signed char*);
EAGER_PTR_EVALUATOR(signed char*, signed char*);
// Data for the log message, not stored in LogMessage to avoid increasing the
// stack size.
class LogMessageData;
// A LogMessage is a temporarily scoped object used by LOG and the unlikely part
// of a CHECK. The destructor will abort if the severity is FATAL.
class LogMessage {
public:
LogMessage(const char* file, unsigned int line, LogId id, LogSeverity severity, const char* tag,
int error);
~LogMessage();
// Returns the stream associated with the message, the LogMessage performs
// output when it goes out of scope.
std::ostream& stream();
// The routine that performs the actual logging.
static void LogLine(const char* file, unsigned int line, LogId id, LogSeverity severity,
const char* tag, const char* msg);
private:
const std::unique_ptr<LogMessageData> data_;
// TODO(b/35361699): remove these symbols once all prebuilds stop using it.
LogMessage(const char* file, unsigned int line, LogId id, LogSeverity severity, int error);
static void LogLine(const char* file, unsigned int line, LogId id, LogSeverity severity,
const char* msg);
DISALLOW_COPY_AND_ASSIGN(LogMessage);
};
// Get the minimum severity level for logging.
LogSeverity GetMinimumLogSeverity();
// Set the minimum severity level for logging, returning the old severity.
LogSeverity SetMinimumLogSeverity(LogSeverity new_severity);
// Allows to temporarily change the minimum severity level for logging.
class ScopedLogSeverity {
public:
explicit ScopedLogSeverity(LogSeverity level);
~ScopedLogSeverity();
private:
LogSeverity old_;
};
} // namespace base
} // namespace android
namespace std {
// Emit a warning of ostream<< with std::string*. The intention was most likely to print *string.
//
// Note: for this to work, we need to have this in a namespace.
// Note: lots of ifdef magic to make this work with Clang (platform) vs GCC (windows tools)
// Note: using diagnose_if(true) under Clang and nothing under GCC/mingw as there is no common
// attribute support.
// Note: using a pragma because "-Wgcc-compat" (included in "-Weverything") complains about
// diagnose_if.
// Note: to print the pointer, use "<< static_cast<const void*>(string_pointer)" instead.
// Note: a not-recommended alternative is to let Clang ignore the warning by adding
// -Wno-user-defined-warnings to CPPFLAGS.
#ifdef __clang__
#pragma clang diagnostic push
#pragma clang diagnostic ignored "-Wgcc-compat"
#define OSTREAM_STRING_POINTER_USAGE_WARNING \
__attribute__((diagnose_if(true, "Unexpected logging of string pointer", "warning")))
#else
#define OSTREAM_STRING_POINTER_USAGE_WARNING /* empty */
#endif
inline std::ostream& operator<<(std::ostream& stream, const std::string* string_pointer)
OSTREAM_STRING_POINTER_USAGE_WARNING {
return stream << static_cast<const void*>(string_pointer);
}
#ifdef __clang__
#pragma clang diagnostic pop
#endif
#undef OSTREAM_STRING_POINTER_USAGE_WARNING
} // namespace std
|