1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
|
/*
* Copyright (C) 2015 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef ANDROID_BASE_MACROS_H
#define ANDROID_BASE_MACROS_H
#include <stddef.h> // for size_t
#include <unistd.h> // for TEMP_FAILURE_RETRY
#include <utility>
// bionic and glibc both have TEMP_FAILURE_RETRY, but eg Mac OS' libc doesn't.
#ifndef TEMP_FAILURE_RETRY
#define TEMP_FAILURE_RETRY(exp) \
({ \
decltype(exp) _rc; \
do { \
_rc = (exp); \
} while (_rc == -1 && errno == EINTR); \
_rc; \
})
#endif
// A macro to disallow the copy constructor and operator= functions
// This must be placed in the private: declarations for a class.
//
// For disallowing only assign or copy, delete the relevant operator or
// constructor, for example:
// void operator=(const TypeName&) = delete;
// Note, that most uses of DISALLOW_ASSIGN and DISALLOW_COPY are broken
// semantically, one should either use disallow both or neither. Try to
// avoid these in new code.
#define DISALLOW_COPY_AND_ASSIGN(TypeName) \
TypeName(const TypeName&) = delete; \
void operator=(const TypeName&) = delete
// A macro to disallow all the implicit constructors, namely the
// default constructor, copy constructor and operator= functions.
//
// This should be used in the private: declarations for a class
// that wants to prevent anyone from instantiating it. This is
// especially useful for classes containing only static methods.
#define DISALLOW_IMPLICIT_CONSTRUCTORS(TypeName) \
TypeName() = delete; \
DISALLOW_COPY_AND_ASSIGN(TypeName)
// The arraysize(arr) macro returns the # of elements in an array arr.
// The expression is a compile-time constant, and therefore can be
// used in defining new arrays, for example. If you use arraysize on
// a pointer by mistake, you will get a compile-time error.
//
// One caveat is that arraysize() doesn't accept any array of an
// anonymous type or a type defined inside a function. In these rare
// cases, you have to use the unsafe ARRAYSIZE_UNSAFE() macro below. This is
// due to a limitation in C++'s template system. The limitation might
// eventually be removed, but it hasn't happened yet.
// This template function declaration is used in defining arraysize.
// Note that the function doesn't need an implementation, as we only
// use its type.
template <typename T, size_t N>
char(&ArraySizeHelper(T(&array)[N]))[N]; // NOLINT(readability/casting)
#define arraysize(array) (sizeof(ArraySizeHelper(array)))
// ARRAYSIZE_UNSAFE performs essentially the same calculation as arraysize,
// but can be used on anonymous types or types defined inside
// functions. It's less safe than arraysize as it accepts some
// (although not all) pointers. Therefore, you should use arraysize
// whenever possible.
//
// The expression ARRAYSIZE_UNSAFE(a) is a compile-time constant of type
// size_t.
//
// ARRAYSIZE_UNSAFE catches a few type errors. If you see a compiler error
//
// "warning: division by zero in ..."
//
// when using ARRAYSIZE_UNSAFE, you are (wrongfully) giving it a pointer.
// You should only use ARRAYSIZE_UNSAFE on statically allocated arrays.
//
// The following comments are on the implementation details, and can
// be ignored by the users.
//
// ARRAYSIZE_UNSAFE(arr) works by inspecting sizeof(arr) (the # of bytes in
// the array) and sizeof(*(arr)) (the # of bytes in one array
// element). If the former is divisible by the latter, perhaps arr is
// indeed an array, in which case the division result is the # of
// elements in the array. Otherwise, arr cannot possibly be an array,
// and we generate a compiler error to prevent the code from
// compiling.
//
// Since the size of bool is implementation-defined, we need to cast
// !(sizeof(a) & sizeof(*(a))) to size_t in order to ensure the final
// result has type size_t.
//
// This macro is not perfect as it wrongfully accepts certain
// pointers, namely where the pointer size is divisible by the pointee
// size. Since all our code has to go through a 32-bit compiler,
// where a pointer is 4 bytes, this means all pointers to a type whose
// size is 3 or greater than 4 will be (righteously) rejected.
#define ARRAYSIZE_UNSAFE(a) \
((sizeof(a) / sizeof(*(a))) / \
static_cast<size_t>(!(sizeof(a) % sizeof(*(a)))))
#define SIZEOF_MEMBER(t, f) sizeof(std::declval<t>().f)
// Changing this definition will cause you a lot of pain. A majority of
// vendor code defines LIKELY and UNLIKELY this way, and includes
// this header through an indirect path.
#define LIKELY( exp ) (__builtin_expect( (exp) != 0, true ))
#define UNLIKELY( exp ) (__builtin_expect( (exp) != 0, false ))
#define WARN_UNUSED __attribute__((warn_unused_result))
// A deprecated function to call to create a false use of the parameter, for
// example:
// int foo(int x) { UNUSED(x); return 10; }
// to avoid compiler warnings. Going forward we prefer ATTRIBUTE_UNUSED.
template <typename... T>
void UNUSED(const T&...) {
}
// An attribute to place on a parameter to a function, for example:
// int foo(int x ATTRIBUTE_UNUSED) { return 10; }
// to avoid compiler warnings.
#define ATTRIBUTE_UNUSED __attribute__((__unused__))
// The FALLTHROUGH_INTENDED macro can be used to annotate implicit fall-through
// between switch labels:
// switch (x) {
// case 40:
// case 41:
// if (truth_is_out_there) {
// ++x;
// FALLTHROUGH_INTENDED; // Use instead of/along with annotations in
// // comments.
// } else {
// return x;
// }
// case 42:
// ...
//
// As shown in the example above, the FALLTHROUGH_INTENDED macro should be
// followed by a semicolon. It is designed to mimic control-flow statements
// like 'break;', so it can be placed in most places where 'break;' can, but
// only if there are no statements on the execution path between it and the
// next switch label.
//
// When compiled with clang, the FALLTHROUGH_INTENDED macro is expanded to
// [[clang::fallthrough]] attribute, which is analysed when performing switch
// labels fall-through diagnostic ('-Wimplicit-fallthrough'). See clang
// documentation on language extensions for details:
// http://clang.llvm.org/docs/LanguageExtensions.html#clang__fallthrough
//
// When used with unsupported compilers, the FALLTHROUGH_INTENDED macro has no
// effect on diagnostics.
//
// In either case this macro has no effect on runtime behavior and performance
// of code.
#if defined(__clang__) && defined(__has_warning)
#if __has_feature(cxx_attributes) && __has_warning("-Wimplicit-fallthrough")
#define FALLTHROUGH_INTENDED [[clang::fallthrough]] // NOLINT
#endif
#endif
#ifndef FALLTHROUGH_INTENDED
#define FALLTHROUGH_INTENDED \
do { \
} while (0)
#endif
// Current ABI string
#if defined(__arm__)
#define ABI_STRING "arm"
#elif defined(__aarch64__)
#define ABI_STRING "arm64"
#elif defined(__i386__)
#define ABI_STRING "x86"
#elif defined(__x86_64__)
#define ABI_STRING "x86_64"
#elif defined(__mips__) && !defined(__LP64__)
#define ABI_STRING "mips"
#elif defined(__mips__) && defined(__LP64__)
#define ABI_STRING "mips64"
#endif
#endif // ANDROID_BASE_MACROS_H
|