summaryrefslogtreecommitdiffstats
blob: c6936f137fb2ea7c0a224a40ab913a42152491ed (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#pragma once

#include <fcntl.h>

#if !defined(_WIN32)
#include <sys/socket.h>
#endif

#include <sys/types.h>
#include <unistd.h>

// DO NOT INCLUDE OTHER LIBBASE HEADERS!
// This file gets used in libbinder, and libbinder is used everywhere.
// Including other headers from libbase frequently results in inclusion of
// android-base/macros.h, which causes macro collisions.

// Container for a file descriptor that automatically closes the descriptor as
// it goes out of scope.
//
//      unique_fd ufd(open("/some/path", "r"));
//      if (ufd.get() == -1) return error;
//
//      // Do something useful, possibly including 'return'.
//
//      return 0; // Descriptor is closed for you.
//
// unique_fd is also known as ScopedFd/ScopedFD/scoped_fd; mentioned here to help
// you find this class if you're searching for one of those names.

#if defined(__BIONIC__)
#include <android/fdsan.h>
#endif

namespace android {
namespace base {

struct DefaultCloser {
#if defined(__BIONIC__)
  static void Tag(int fd, void* old_addr, void* new_addr) {
    if (android_fdsan_exchange_owner_tag) {
      uint64_t old_tag = android_fdsan_create_owner_tag(ANDROID_FDSAN_OWNER_TYPE_UNIQUE_FD,
                                                        reinterpret_cast<uint64_t>(old_addr));
      uint64_t new_tag = android_fdsan_create_owner_tag(ANDROID_FDSAN_OWNER_TYPE_UNIQUE_FD,
                                                        reinterpret_cast<uint64_t>(new_addr));
      android_fdsan_exchange_owner_tag(fd, old_tag, new_tag);
    }
  }
  static void Close(int fd, void* addr) {
    if (android_fdsan_close_with_tag) {
      uint64_t tag = android_fdsan_create_owner_tag(ANDROID_FDSAN_OWNER_TYPE_UNIQUE_FD,
                                                    reinterpret_cast<uint64_t>(addr));
      android_fdsan_close_with_tag(fd, tag);
    } else {
      close(fd);
    }
  }
#else
  static void Close(int fd) {
    // Even if close(2) fails with EINTR, the fd will have been closed.
    // Using TEMP_FAILURE_RETRY will either lead to EBADF or closing someone
    // else's fd.
    // http://lkml.indiana.edu/hypermail/linux/kernel/0509.1/0877.html
    ::close(fd);
  }
#endif
};

template <typename Closer>
class unique_fd_impl final {
 public:
  unique_fd_impl() {}

  explicit unique_fd_impl(int fd) { reset(fd); }
  ~unique_fd_impl() { reset(); }

  unique_fd_impl(unique_fd_impl&& other) { reset(other.release()); }
  unique_fd_impl& operator=(unique_fd_impl&& s) {
    int fd = s.fd_;
    s.fd_ = -1;
    reset(fd, &s);
    return *this;
  }

  void reset(int new_value = -1) { reset(new_value, nullptr); }

  int get() const { return fd_; }
  operator int() const { return get(); }

  int release() __attribute__((warn_unused_result)) {
    tag(fd_, this, nullptr);
    int ret = fd_;
    fd_ = -1;
    return ret;
  }

 private:
  void reset(int new_value, void* previous_tag) {
    if (fd_ != -1) {
      close(fd_, this);
    }

    fd_ = new_value;
    if (new_value != -1) {
      tag(new_value, previous_tag, this);
    }
  }

  int fd_ = -1;

  // Template magic to use Closer::Tag if available, and do nothing if not.
  // If Closer::Tag exists, this implementation is preferred, because int is a better match.
  // If not, this implementation is SFINAEd away, and the no-op below is the only one that exists.
  template <typename T = Closer>
  static auto tag(int fd, void* old_tag, void* new_tag)
      -> decltype(T::Tag(fd, old_tag, new_tag), void()) {
    T::Tag(fd, old_tag, new_tag);
  }

  template <typename T = Closer>
  static void tag(long, void*, void*) {
    // No-op.
  }

  // Same as above, to select between Closer::Close(int) and Closer::Close(int, void*).
  template <typename T = Closer>
  static auto close(int fd, void* tag_value) -> decltype(T::Close(fd, tag_value), void()) {
    T::Close(fd, tag_value);
  }

  template <typename T = Closer>
  static auto close(int fd, void*) -> decltype(T::Close(fd), void()) {
    T::Close(fd);
  }

  unique_fd_impl(const unique_fd_impl&);
  void operator=(const unique_fd_impl&);
};

using unique_fd = unique_fd_impl<DefaultCloser>;

#if !defined(_WIN32)

// Inline functions, so that they can be used header-only.
template <typename Closer>
inline bool Pipe(unique_fd_impl<Closer>* read, unique_fd_impl<Closer>* write) {
  int pipefd[2];

#if defined(__linux__)
  if (pipe2(pipefd, O_CLOEXEC) != 0) {
    return false;
  }
#else  // defined(__APPLE__)
  if (pipe(pipefd) != 0) {
    return false;
  }

  if (fcntl(pipefd[0], F_SETFD, FD_CLOEXEC) != 0 || fcntl(pipefd[1], F_SETFD, FD_CLOEXEC) != 0) {
    close(pipefd[0]);
    close(pipefd[1]);
    return false;
  }
#endif

  read->reset(pipefd[0]);
  write->reset(pipefd[1]);
  return true;
}

template <typename Closer>
inline bool Socketpair(int domain, int type, int protocol, unique_fd_impl<Closer>* left,
                       unique_fd_impl<Closer>* right) {
  int sockfd[2];
  if (socketpair(domain, type, protocol, sockfd) != 0) {
    return false;
  }
  left->reset(sockfd[0]);
  right->reset(sockfd[1]);
  return true;
}

template <typename Closer>
inline bool Socketpair(int type, unique_fd_impl<Closer>* left, unique_fd_impl<Closer>* right) {
  return Socketpair(AF_UNIX, type, 0, left, right);
}

#endif  // !defined(_WIN32)

}  // namespace base
}  // namespace android

template <typename T>
int close(const android::base::unique_fd_impl<T>&)
    __attribute__((__unavailable__("close called on unique_fd")));