summaryrefslogtreecommitdiffstats
blob: 5984fb06c635fe652ea5b6879656dd84332f55f0 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
/*
 * Copyright (C) 2015 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include <windows.h>

#include "android-base/utf8.h"

#include <fcntl.h>
#include <stdio.h>

#include <algorithm>
#include <string>

#include "android-base/logging.h"

namespace android {
namespace base {

// Helper to set errno based on GetLastError() after WideCharToMultiByte()/MultiByteToWideChar().
static void SetErrnoFromLastError() {
  switch (GetLastError()) {
    case ERROR_NO_UNICODE_TRANSLATION:
      errno = EILSEQ;
      break;
    default:
      errno = EINVAL;
      break;
  }
}

bool WideToUTF8(const wchar_t* utf16, const size_t size, std::string* utf8) {
  utf8->clear();

  if (size == 0) {
    return true;
  }

  // TODO: Consider using std::wstring_convert once libcxx is supported on
  // Windows.

  // Only Vista or later has this flag that causes WideCharToMultiByte() to
  // return an error on invalid characters.
  const DWORD flags =
#if (WINVER >= 0x0600)
    WC_ERR_INVALID_CHARS;
#else
    0;
#endif

  const int chars_required = WideCharToMultiByte(CP_UTF8, flags, utf16, size,
                                                 NULL, 0, NULL, NULL);
  if (chars_required <= 0) {
    SetErrnoFromLastError();
    return false;
  }

  // This could potentially throw a std::bad_alloc exception.
  utf8->resize(chars_required);

  const int result = WideCharToMultiByte(CP_UTF8, flags, utf16, size,
                                         &(*utf8)[0], chars_required, NULL,
                                         NULL);
  if (result != chars_required) {
    SetErrnoFromLastError();
    CHECK_LE(result, chars_required) << "WideCharToMultiByte wrote " << result
        << " chars to buffer of " << chars_required << " chars";
    utf8->clear();
    return false;
  }

  return true;
}

bool WideToUTF8(const wchar_t* utf16, std::string* utf8) {
  // Compute string length of NULL-terminated string with wcslen().
  return WideToUTF8(utf16, wcslen(utf16), utf8);
}

bool WideToUTF8(const std::wstring& utf16, std::string* utf8) {
  // Use the stored length of the string which allows embedded NULL characters
  // to be converted.
  return WideToUTF8(utf16.c_str(), utf16.length(), utf8);
}

// Internal helper function that takes MultiByteToWideChar() flags.
static bool UTF8ToWideWithFlags(const char* utf8, const size_t size, std::wstring* utf16,
                                const DWORD flags) {
  utf16->clear();

  if (size == 0) {
    return true;
  }

  // TODO: Consider using std::wstring_convert once libcxx is supported on
  // Windows.
  const int chars_required = MultiByteToWideChar(CP_UTF8, flags, utf8, size,
                                                 NULL, 0);
  if (chars_required <= 0) {
    SetErrnoFromLastError();
    return false;
  }

  // This could potentially throw a std::bad_alloc exception.
  utf16->resize(chars_required);

  const int result = MultiByteToWideChar(CP_UTF8, flags, utf8, size,
                                         &(*utf16)[0], chars_required);
  if (result != chars_required) {
    SetErrnoFromLastError();
    CHECK_LE(result, chars_required) << "MultiByteToWideChar wrote " << result
        << " chars to buffer of " << chars_required << " chars";
    utf16->clear();
    return false;
  }

  return true;
}

bool UTF8ToWide(const char* utf8, const size_t size, std::wstring* utf16) {
  // If strictly interpreting as UTF-8 succeeds, return success.
  if (UTF8ToWideWithFlags(utf8, size, utf16, MB_ERR_INVALID_CHARS)) {
    return true;
  }

  const int saved_errno = errno;

  // Fallback to non-strict interpretation, allowing invalid characters and
  // converting as best as possible, and return false to signify a problem.
  (void)UTF8ToWideWithFlags(utf8, size, utf16, 0);
  errno = saved_errno;
  return false;
}

bool UTF8ToWide(const char* utf8, std::wstring* utf16) {
  // Compute string length of NULL-terminated string with strlen().
  return UTF8ToWide(utf8, strlen(utf8), utf16);
}

bool UTF8ToWide(const std::string& utf8, std::wstring* utf16) {
  // Use the stored length of the string which allows embedded NULL characters
  // to be converted.
  return UTF8ToWide(utf8.c_str(), utf8.length(), utf16);
}

static bool isDriveLetter(wchar_t c) {
  return (c >= L'a' && c <= L'z') || (c >= L'A' && c <= L'Z');
}

bool UTF8PathToWindowsLongPath(const char* utf8, std::wstring* utf16) {
  if (!UTF8ToWide(utf8, utf16)) {
    return false;
  }
  // Note: Although most Win32 File I/O API are limited to MAX_PATH (260
  //       characters), the CreateDirectory API is limited to 248 characters.
  if (utf16->length() >= 248) {
    // If path is of the form "x:\" or "x:/"
    if (isDriveLetter((*utf16)[0]) && (*utf16)[1] == L':' &&
        ((*utf16)[2] == L'\\' || (*utf16)[2] == L'/')) {
      // Append long path prefix, and make sure there are no unix-style
      // separators to ensure a fully compliant Win32 long path string.
      utf16->insert(0, LR"(\\?\)");
      std::replace(utf16->begin(), utf16->end(), L'/', L'\\');
    }
  }
  return true;
}

// Versions of standard library APIs that support UTF-8 strings.
namespace utf8 {

FILE* fopen(const char* name, const char* mode) {
  std::wstring name_utf16;
  if (!UTF8PathToWindowsLongPath(name, &name_utf16)) {
    return nullptr;
  }

  std::wstring mode_utf16;
  if (!UTF8ToWide(mode, &mode_utf16)) {
    return nullptr;
  }

  return _wfopen(name_utf16.c_str(), mode_utf16.c_str());
}

int mkdir(const char* name, mode_t mode) {
  std::wstring name_utf16;
  if (!UTF8PathToWindowsLongPath(name, &name_utf16)) {
    return -1;
  }

  return _wmkdir(name_utf16.c_str());
}

int open(const char* name, int flags, ...) {
  std::wstring name_utf16;
  if (!UTF8PathToWindowsLongPath(name, &name_utf16)) {
    return -1;
  }

  int mode = 0;
  if ((flags & O_CREAT) != 0) {
    va_list args;
    va_start(args, flags);
    mode = va_arg(args, int);
    va_end(args);
  }

  return _wopen(name_utf16.c_str(), flags, mode);
}

int unlink(const char* name) {
  std::wstring name_utf16;
  if (!UTF8PathToWindowsLongPath(name, &name_utf16)) {
    return -1;
  }

  return _wunlink(name_utf16.c_str());
}

}  // namespace utf8
}  // namespace base
}  // namespace android