summaryrefslogtreecommitdiffstats
blob: fcb25c3507f17b7f8122798943f82abc37556325 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
/*
* Copyright (C) 2015 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
*      http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/

#include "android-base/utf8.h"

#include <gtest/gtest.h>

#include <fcntl.h>
#include <stdlib.h>

#include "android-base/macros.h"
#include "android-base/test_utils.h"
#include "android-base/unique_fd.h"

namespace android {
namespace base {

TEST(UTFStringConversionsTest, ConvertInvalidUTF8) {
  std::wstring wide;

  errno = 0;

  // Standalone \xa2 is an invalid UTF-8 sequence, so this should return an
  // error. Concatenate two C/C++ literal string constants to prevent the
  // compiler from giving an error about "\xa2af" containing a "hex escape
  // sequence out of range".
  EXPECT_FALSE(android::base::UTF8ToWide("before\xa2" "after", &wide));

  EXPECT_EQ(EILSEQ, errno);

  // Even if an invalid character is encountered, UTF8ToWide() should still do
  // its best to convert the rest of the string. sysdeps_win32.cpp:
  // _console_write_utf8() depends on this behavior.
  //
  // Thus, we verify that the valid characters are converted, but we ignore the
  // specific replacement character that UTF8ToWide() may replace the invalid
  // UTF-8 characters with because we want to allow that to change if the
  // implementation changes.
  EXPECT_EQ(0U, wide.find(L"before"));
  const wchar_t after_wide[] = L"after";
  EXPECT_EQ(wide.length() - (arraysize(after_wide) - 1), wide.find(after_wide));
}

// Below is adapted from https://chromium.googlesource.com/chromium/src/+/master/base/strings/utf_string_conversions_unittest.cc

// Copyright (c) 2010 The Chromium Authors. All rights reserved.
// Use of this source code is governed by a BSD-style license that can be
// found in the LICENSE file.

// The tests below from utf_string_conversions_unittest.cc check for this
// preprocessor symbol, so define it, as it is appropriate for Windows.
#define WCHAR_T_IS_UTF16
static_assert(sizeof(wchar_t) == 2, "wchar_t is not 2 bytes");

// The tests below from utf_string_conversions_unittest.cc call versions of
// UTF8ToWide() and WideToUTF8() that don't return success/failure, so these are
// stub implementations with that signature. These are just for testing and
// should not be moved to base because they assert/expect no errors which is
// probably not a good idea (or at least it is something that should be left
// up to the caller, not a base library).

static std::wstring UTF8ToWide(const std::string& utf8) {
  std::wstring utf16;
  EXPECT_TRUE(UTF8ToWide(utf8, &utf16));
  return utf16;
}

static std::string WideToUTF8(const std::wstring& utf16) {
  std::string utf8;
  EXPECT_TRUE(WideToUTF8(utf16, &utf8));
  return utf8;
}

namespace {

const wchar_t* const kConvertRoundtripCases[] = {
  L"Google Video",
  // "网页 图片 资讯更多 »"
  L"\x7f51\x9875\x0020\x56fe\x7247\x0020\x8d44\x8baf\x66f4\x591a\x0020\x00bb",
  //  "Παγκόσμιος Ιστός"
  L"\x03a0\x03b1\x03b3\x03ba\x03cc\x03c3\x03bc\x03b9"
  L"\x03bf\x03c2\x0020\x0399\x03c3\x03c4\x03cc\x03c2",
  // "Поиск страниц на русском"
  L"\x041f\x043e\x0438\x0441\x043a\x0020\x0441\x0442"
  L"\x0440\x0430\x043d\x0438\x0446\x0020\x043d\x0430"
  L"\x0020\x0440\x0443\x0441\x0441\x043a\x043e\x043c",
  // "전체서비스"
  L"\xc804\xccb4\xc11c\xbe44\xc2a4",

  // Test characters that take more than 16 bits. This will depend on whether
  // wchar_t is 16 or 32 bits.
#if defined(WCHAR_T_IS_UTF16)
  L"\xd800\xdf00",
  // ?????  (Mathematical Alphanumeric Symbols (U+011d40 - U+011d44 : A,B,C,D,E)
  L"\xd807\xdd40\xd807\xdd41\xd807\xdd42\xd807\xdd43\xd807\xdd44",
#elif defined(WCHAR_T_IS_UTF32)
  L"\x10300",
  // ?????  (Mathematical Alphanumeric Symbols (U+011d40 - U+011d44 : A,B,C,D,E)
  L"\x11d40\x11d41\x11d42\x11d43\x11d44",
#endif
};

}  // namespace

TEST(UTFStringConversionsTest, ConvertUTF8AndWide) {
  // we round-trip all the wide strings through UTF-8 to make sure everything
  // agrees on the conversion. This uses the stream operators to test them
  // simultaneously.
  for (size_t i = 0; i < arraysize(kConvertRoundtripCases); ++i) {
    std::ostringstream utf8;
    utf8 << WideToUTF8(kConvertRoundtripCases[i]);
    std::wostringstream wide;
    wide << UTF8ToWide(utf8.str());

    EXPECT_EQ(kConvertRoundtripCases[i], wide.str());
  }
}

TEST(UTFStringConversionsTest, ConvertUTF8AndWideEmptyString) {
  // An empty std::wstring should be converted to an empty std::string,
  // and vice versa.
  std::wstring wempty;
  std::string empty;
  EXPECT_EQ(empty, WideToUTF8(wempty));
  EXPECT_EQ(wempty, UTF8ToWide(empty));
}

TEST(UTFStringConversionsTest, ConvertUTF8ToWide) {
  struct UTF8ToWideCase {
    const char* utf8;
    const wchar_t* wide;
    bool success;
  } convert_cases[] = {
    // Regular UTF-8 input.
    {"\xe4\xbd\xa0\xe5\xa5\xbd", L"\x4f60\x597d", true},
    // Non-character is passed through.
    {"\xef\xbf\xbfHello", L"\xffffHello", true},
    // Truncated UTF-8 sequence.
    {"\xe4\xa0\xe5\xa5\xbd", L"\xfffd\x597d", false},
    // Truncated off the end.
    {"\xe5\xa5\xbd\xe4\xa0", L"\x597d\xfffd", false},
    // Non-shortest-form UTF-8.
    {"\xf0\x84\xbd\xa0\xe5\xa5\xbd", L"\xfffd\x597d", false},
    // This UTF-8 character decodes to a UTF-16 surrogate, which is illegal.
    // Note that for whatever reason, this test fails on Windows XP.
    {"\xed\xb0\x80", L"\xfffd", false},
    // Non-BMP characters. The second is a non-character regarded as valid.
    // The result will either be in UTF-16 or UTF-32.
#if defined(WCHAR_T_IS_UTF16)
    {"A\xF0\x90\x8C\x80z", L"A\xd800\xdf00z", true},
    {"A\xF4\x8F\xBF\xBEz", L"A\xdbff\xdffez", true},
#elif defined(WCHAR_T_IS_UTF32)
    {"A\xF0\x90\x8C\x80z", L"A\x10300z", true},
    {"A\xF4\x8F\xBF\xBEz", L"A\x10fffez", true},
#endif
  };

  for (size_t i = 0; i < arraysize(convert_cases); i++) {
    std::wstring converted;
    errno = 0;
    const bool success = UTF8ToWide(convert_cases[i].utf8,
                                    strlen(convert_cases[i].utf8),
                                    &converted);
    EXPECT_EQ(convert_cases[i].success, success);
    // The original test always compared expected and converted, but don't do
    // that because our implementation of UTF8ToWide() does not guarantee to
    // produce the same output in error situations.
    if (success) {
      std::wstring expected(convert_cases[i].wide);
      EXPECT_EQ(expected, converted);
    } else {
      EXPECT_EQ(EILSEQ, errno);
    }
  }

  // Manually test an embedded NULL.
  std::wstring converted;
  EXPECT_TRUE(UTF8ToWide("\00Z\t", 3, &converted));
  ASSERT_EQ(3U, converted.length());
  EXPECT_EQ(static_cast<wchar_t>(0), converted[0]);
  EXPECT_EQ('Z', converted[1]);
  EXPECT_EQ('\t', converted[2]);

  // Make sure that conversion replaces, not appends.
  EXPECT_TRUE(UTF8ToWide("B", 1, &converted));
  ASSERT_EQ(1U, converted.length());
  EXPECT_EQ('B', converted[0]);
}

#if defined(WCHAR_T_IS_UTF16)
// This test is only valid when wchar_t == UTF-16.
TEST(UTFStringConversionsTest, ConvertUTF16ToUTF8) {
  struct WideToUTF8Case {
    const wchar_t* utf16;
    const char* utf8;
    bool success;
  } convert_cases[] = {
    // Regular UTF-16 input.
    {L"\x4f60\x597d", "\xe4\xbd\xa0\xe5\xa5\xbd", true},
    // Test a non-BMP character.
    {L"\xd800\xdf00", "\xF0\x90\x8C\x80", true},
    // Non-characters are passed through.
    {L"\xffffHello", "\xEF\xBF\xBFHello", true},
    {L"\xdbff\xdffeHello", "\xF4\x8F\xBF\xBEHello", true},
    // The first character is a truncated UTF-16 character.
    // Note that for whatever reason, this test fails on Windows XP.
    {L"\xd800\x597d", "\xef\xbf\xbd\xe5\xa5\xbd",
#if (WINVER >= 0x0600)
    // Only Vista and later has a new API/flag that correctly returns false.
    false
#else
    true
#endif
    },
    // Truncated at the end.
    // Note that for whatever reason, this test fails on Windows XP.
    {L"\x597d\xd800", "\xe5\xa5\xbd\xef\xbf\xbd",
#if (WINVER >= 0x0600)
    // Only Vista and later has a new API/flag that correctly returns false.
    false
#else
    true
#endif
    },
  };

  for (size_t i = 0; i < arraysize(convert_cases); i++) {
    std::string converted;
    errno = 0;
    const bool success = WideToUTF8(convert_cases[i].utf16,
                                    wcslen(convert_cases[i].utf16),
                                    &converted);
    EXPECT_EQ(convert_cases[i].success, success);
    // The original test always compared expected and converted, but don't do
    // that because our implementation of WideToUTF8() does not guarantee to
    // produce the same output in error situations.
    if (success) {
      std::string expected(convert_cases[i].utf8);
      EXPECT_EQ(expected, converted);
    } else {
      EXPECT_EQ(EILSEQ, errno);
    }
  }
}

#elif defined(WCHAR_T_IS_UTF32)
// This test is only valid when wchar_t == UTF-32.
TEST(UTFStringConversionsTest, ConvertUTF32ToUTF8) {
  struct WideToUTF8Case {
    const wchar_t* utf32;
    const char* utf8;
    bool success;
  } convert_cases[] = {
    // Regular 16-bit input.
    {L"\x4f60\x597d", "\xe4\xbd\xa0\xe5\xa5\xbd", true},
    // Test a non-BMP character.
    {L"A\x10300z", "A\xF0\x90\x8C\x80z", true},
    // Non-characters are passed through.
    {L"\xffffHello", "\xEF\xBF\xBFHello", true},
    {L"\x10fffeHello", "\xF4\x8F\xBF\xBEHello", true},
    // Invalid Unicode code points.
    {L"\xfffffffHello", "\xEF\xBF\xBDHello", false},
    // The first character is a truncated UTF-16 character.
    {L"\xd800\x597d", "\xef\xbf\xbd\xe5\xa5\xbd", false},
    {L"\xdc01Hello", "\xef\xbf\xbdHello", false},
  };

  for (size_t i = 0; i < arraysize(convert_cases); i++) {
    std::string converted;
    EXPECT_EQ(convert_cases[i].success,
              WideToUTF8(convert_cases[i].utf32,
                         wcslen(convert_cases[i].utf32),
                         &converted));
    std::string expected(convert_cases[i].utf8);
    EXPECT_EQ(expected, converted);
  }
}
#endif  // defined(WCHAR_T_IS_UTF32)

// The test below uses these types and functions, so just do enough to get the
// test running.
typedef wchar_t char16;
typedef std::wstring string16;

template<typename T>
static void* WriteInto(T* t, size_t size) {
  // std::(w)string::resize() already includes space for a NULL terminator.
  t->resize(size - 1);
  return &(*t)[0];
}

// A stub implementation that calls a helper from above, just to get the test
// below working. This is just for testing and should not be moved to base
// because this ignores errors which is probably not a good idea, plus it takes
// a string16 type which we don't really have.
static std::string UTF16ToUTF8(const string16& utf16) {
  return WideToUTF8(utf16);
}

TEST(UTFStringConversionsTest, ConvertMultiString) {
  static char16 multi16[] = {
    'f', 'o', 'o', '\0',
    'b', 'a', 'r', '\0',
    'b', 'a', 'z', '\0',
    '\0'
  };
  static char multi[] = {
    'f', 'o', 'o', '\0',
    'b', 'a', 'r', '\0',
    'b', 'a', 'z', '\0',
    '\0'
  };
  string16 multistring16;
  memcpy(WriteInto(&multistring16, arraysize(multi16)), multi16,
                   sizeof(multi16));
  EXPECT_EQ(arraysize(multi16) - 1, multistring16.length());
  std::string expected;
  memcpy(WriteInto(&expected, arraysize(multi)), multi, sizeof(multi));
  EXPECT_EQ(arraysize(multi) - 1, expected.length());
  const std::string& converted = UTF16ToUTF8(multistring16);
  EXPECT_EQ(arraysize(multi) - 1, converted.length());
  EXPECT_EQ(expected, converted);
}

// The tests below from sys_string_conversions_unittest.cc call SysWideToUTF8()
// and SysUTF8ToWide(), so these are stub implementations that call the helpers
// above. These are just for testing and should not be moved to base because
// they ignore errors which is probably not a good idea.

static std::string SysWideToUTF8(const std::wstring& utf16) {
  return WideToUTF8(utf16);
}

static std::wstring SysUTF8ToWide(const std::string& utf8) {
  return UTF8ToWide(utf8);
}

// Below is adapted from https://chromium.googlesource.com/chromium/src/+/master/base/strings/sys_string_conversions_unittest.cc

// Copyright (c) 2011 The Chromium Authors. All rights reserved.
// Use of this source code is governed by a BSD-style license that can be
// found in the LICENSE file.

#ifdef WCHAR_T_IS_UTF32
static const std::wstring kSysWideOldItalicLetterA = L"\x10300";
#else
static const std::wstring kSysWideOldItalicLetterA = L"\xd800\xdf00";
#endif

TEST(SysStrings, SysWideToUTF8) {
  EXPECT_EQ("Hello, world", SysWideToUTF8(L"Hello, world"));
  EXPECT_EQ("\xe4\xbd\xa0\xe5\xa5\xbd", SysWideToUTF8(L"\x4f60\x597d"));

  // >16 bits
  EXPECT_EQ("\xF0\x90\x8C\x80", SysWideToUTF8(kSysWideOldItalicLetterA));

  // Error case. When Windows finds a UTF-16 character going off the end of
  // a string, it just converts that literal value to UTF-8, even though this
  // is invalid.
  //
  // This is what XP does, but Vista has different behavior, so we don't bother
  // verifying it:
  // EXPECT_EQ("\xE4\xBD\xA0\xED\xA0\x80zyxw",
  //           SysWideToUTF8(L"\x4f60\xd800zyxw"));

  // Test embedded NULLs.
  std::wstring wide_null(L"a");
  wide_null.push_back(0);
  wide_null.push_back('b');

  std::string expected_null("a");
  expected_null.push_back(0);
  expected_null.push_back('b');

  EXPECT_EQ(expected_null, SysWideToUTF8(wide_null));
}

TEST(SysStrings, SysUTF8ToWide) {
  EXPECT_EQ(L"Hello, world", SysUTF8ToWide("Hello, world"));
  EXPECT_EQ(L"\x4f60\x597d", SysUTF8ToWide("\xe4\xbd\xa0\xe5\xa5\xbd"));
  // >16 bits
  EXPECT_EQ(kSysWideOldItalicLetterA, SysUTF8ToWide("\xF0\x90\x8C\x80"));

  // Error case. When Windows finds an invalid UTF-8 character, it just skips
  // it. This seems weird because it's inconsistent with the reverse conversion.
  //
  // This is what XP does, but Vista has different behavior, so we don't bother
  // verifying it:
  // EXPECT_EQ(L"\x4f60zyxw", SysUTF8ToWide("\xe4\xbd\xa0\xe5\xa5zyxw"));

  // Test embedded NULLs.
  std::string utf8_null("a");
  utf8_null.push_back(0);
  utf8_null.push_back('b');

  std::wstring expected_null(L"a");
  expected_null.push_back(0);
  expected_null.push_back('b');

  EXPECT_EQ(expected_null, SysUTF8ToWide(utf8_null));
}

TEST(UTF8PathToWindowsLongPathTest, DontAddPrefixIfShorterThanMaxPath) {
  std::string utf8 = "c:\\mypath\\myfile.txt";

  std::wstring wide;
  EXPECT_TRUE(UTF8PathToWindowsLongPath(utf8.c_str(), &wide));

  EXPECT_EQ(std::string::npos, wide.find(LR"(\\?\)"));
}

TEST(UTF8PathToWindowsLongPathTest, AddPrefixIfLongerThanMaxPath) {
  std::string utf8 = "c:\\mypath";
  while (utf8.length() < 300 /* MAX_PATH is 260 */) {
    utf8 += "\\mypathsegment";
  }

  std::wstring wide;
  EXPECT_TRUE(UTF8PathToWindowsLongPath(utf8.c_str(), &wide));

  EXPECT_EQ(0U, wide.find(LR"(\\?\)"));
  EXPECT_EQ(std::string::npos, wide.find(L"/"));
}

TEST(UTF8PathToWindowsLongPathTest, AddPrefixAndFixSeparatorsIfLongerThanMaxPath) {
  std::string utf8 = "c:/mypath";
  while (utf8.length() < 300 /* MAX_PATH is 260 */) {
    utf8 += "/mypathsegment";
  }

  std::wstring wide;
  EXPECT_TRUE(UTF8PathToWindowsLongPath(utf8.c_str(), &wide));

  EXPECT_EQ(0U, wide.find(LR"(\\?\)"));
  EXPECT_EQ(std::string::npos, wide.find(L"/"));
}

namespace utf8 {

TEST(Utf8FilesTest, CanCreateOpenAndDeleteFileWithLongPath) {
  TemporaryDir td;

  // Create long directory path
  std::string utf8 = td.path;
  while (utf8.length() < 300 /* MAX_PATH is 260 */) {
    utf8 += "\\mypathsegment";
    EXPECT_EQ(0, mkdir(utf8.c_str(), 0));
  }

  // Create file
  utf8 += "\\test-file.bin";
  int flags = O_WRONLY | O_CREAT | O_TRUNC | O_BINARY;
  int mode = 0666;
  android::base::unique_fd fd(open(utf8.c_str(), flags, mode));
  EXPECT_NE(-1, fd.get());

  // Close file
  fd.reset();
  EXPECT_EQ(-1, fd.get());

  // Open file with fopen
  FILE* file = fopen(utf8.c_str(), "rb");
  EXPECT_NE(nullptr, file);

  if (file) {
    fclose(file);
  }

  // Delete file
  EXPECT_EQ(0, unlink(utf8.c_str()));
}

}  // namespace utf8
}  // namespace base
}  // namespace android