1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
|
/*
* Copyright 2006, The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#define LOG_TAG "crasher"
#include <assert.h>
#include <dirent.h>
#include <errno.h>
#include <fcntl.h>
#include <pthread.h>
#include <signal.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sys/mman.h>
#include <sys/prctl.h>
#include <unistd.h>
// We test both kinds of logging.
#include <android-base/logging.h>
#include <log/log.h>
#include "seccomp_policy.h"
#if defined(STATIC_CRASHER)
#include "debuggerd/handler.h"
#endif
#if defined(__arm__)
// See https://www.kernel.org/doc/Documentation/arm/kernel_user_helpers.txt for details.
#define __kuser_helper_version (*(int32_t*) 0xffff0ffc)
typedef void * (__kuser_get_tls_t)(void);
#define __kuser_get_tls (*(__kuser_get_tls_t*) 0xffff0fe0)
typedef int (__kuser_cmpxchg_t)(int oldval, int newval, volatile int *ptr);
#define __kuser_cmpxchg (*(__kuser_cmpxchg_t*) 0xffff0fc0)
typedef void (__kuser_dmb_t)(void);
#define __kuser_dmb (*(__kuser_dmb_t*) 0xffff0fa0)
typedef int (__kuser_cmpxchg64_t)(const int64_t*, const int64_t*, volatile int64_t*);
#define __kuser_cmpxchg64 (*(__kuser_cmpxchg64_t*) 0xffff0f60)
#endif
#define noinline __attribute__((__noinline__))
// Avoid name mangling so that stacks are more readable.
extern "C" {
void crash1(void);
void crashnostack(void);
int do_action(const char* arg);
noinline void maybe_abort() {
if (time(0) != 42) {
abort();
}
}
char* smash_stack_dummy_buf;
noinline void smash_stack_dummy_function(volatile int* plen) {
smash_stack_dummy_buf[*plen] = 0;
}
// This must be marked with "__attribute__ ((noinline))", to ensure the
// compiler generates the proper stack guards around this function.
// Assign local array address to global variable to force stack guards.
// Use another noinline function to corrupt the stack.
noinline int smash_stack(volatile int* plen) {
printf("%s: deliberately corrupting stack...\n", getprogname());
char buf[128];
smash_stack_dummy_buf = buf;
// This should corrupt stack guards and make process abort.
smash_stack_dummy_function(plen);
return 0;
}
#pragma clang diagnostic push
#pragma clang diagnostic ignored "-Winfinite-recursion"
void* global = 0; // So GCC doesn't optimize the tail recursion out of overflow_stack.
noinline void overflow_stack(void* p) {
void* buf[1];
buf[0] = p;
global = buf;
overflow_stack(&buf);
}
#pragma clang diagnostic pop
noinline void* thread_callback(void* raw_arg) {
const char* arg = reinterpret_cast<const char*>(raw_arg);
return reinterpret_cast<void*>(static_cast<uintptr_t>(do_action(arg)));
}
noinline int do_action_on_thread(const char* arg) {
pthread_t t;
pthread_create(&t, nullptr, thread_callback, const_cast<char*>(arg));
void* result = nullptr;
pthread_join(t, &result);
return reinterpret_cast<uintptr_t>(result);
}
noinline int crash3(int a) {
*reinterpret_cast<int*>(0xdead) = a;
return a*4;
}
noinline int crash2(int a) {
a = crash3(a) + 2;
return a*3;
}
noinline int crash(int a) {
a = crash2(a) + 1;
return a*2;
}
noinline void abuse_heap() {
char buf[16];
free(buf); // GCC is smart enough to warn about this, but we're doing it deliberately.
}
noinline void sigsegv_non_null() {
int* a = (int *)(&do_action);
*a = 42;
}
noinline void fprintf_null() {
fprintf(nullptr, "oops");
}
noinline void readdir_null() {
readdir(nullptr);
}
noinline int strlen_null() {
char* sneaky_null = nullptr;
return strlen(sneaky_null);
}
static int usage() {
fprintf(stderr, "usage: %s KIND\n", getprogname());
fprintf(stderr, "\n");
fprintf(stderr, "where KIND is:\n");
fprintf(stderr, " smash-stack overwrite a -fstack-protector guard\n");
fprintf(stderr, " stack-overflow recurse until the stack overflows\n");
fprintf(stderr, " nostack crash with a NULL stack pointer\n");
fprintf(stderr, "\n");
fprintf(stderr, " heap-corruption cause a libc abort by corrupting the heap\n");
fprintf(stderr, " heap-usage cause a libc abort by abusing a heap function\n");
fprintf(stderr, "\n");
fprintf(stderr, " abort call abort()\n");
fprintf(stderr, " assert call assert() without a function\n");
fprintf(stderr, " assert2 call assert() with a function\n");
fprintf(stderr, " exit call exit(1)\n");
fprintf(stderr, "\n");
fprintf(stderr, " fortify fail a _FORTIFY_SOURCE check\n");
fprintf(stderr, " seccomp fail a seccomp check\n");
#if defined(__arm__)
fprintf(stderr, " kuser_helper_version call kuser_helper_version\n");
fprintf(stderr, " kuser_get_tls call kuser_get_tls\n");
fprintf(stderr, " kuser_cmpxchg call kuser_cmpxchg\n");
fprintf(stderr, " kuser_memory_barrier call kuser_memory_barrier\n");
fprintf(stderr, " kuser_cmpxchg64 call kuser_cmpxchg64\n");
#endif
fprintf(stderr, "\n");
fprintf(stderr, " LOG_ALWAYS_FATAL call liblog LOG_ALWAYS_FATAL\n");
fprintf(stderr, " LOG_ALWAYS_FATAL_IF call liblog LOG_ALWAYS_FATAL_IF\n");
fprintf(stderr, " LOG-FATAL call libbase LOG(FATAL)\n");
fprintf(stderr, "\n");
fprintf(stderr, " SIGFPE cause a SIGFPE\n");
fprintf(stderr, " SIGSEGV cause a SIGSEGV at address 0x0 (synonym: crash)\n");
fprintf(stderr, " SIGSEGV-non-null cause a SIGSEGV at a non-zero address\n");
fprintf(stderr, " SIGSEGV-unmapped mmap/munmap a region of memory and then attempt to access it\n");
fprintf(stderr, " SIGTRAP cause a SIGTRAP\n");
fprintf(stderr, "\n");
fprintf(stderr, " fprintf-NULL pass a null pointer to fprintf\n");
fprintf(stderr, " readdir-NULL pass a null pointer to readdir\n");
fprintf(stderr, " strlen-NULL pass a null pointer to strlen\n");
fprintf(stderr, " pthread_join-NULL pass a null pointer to pthread_join\n");
fprintf(stderr, "\n");
fprintf(stderr, " no_new_privs set PR_SET_NO_NEW_PRIVS and then abort\n");
fprintf(stderr, "\n");
fprintf(stderr, "prefix any of the above with 'thread-' to run on a new thread\n");
fprintf(stderr, "prefix any of the above with 'exhaustfd-' to exhaust\n");
fprintf(stderr, "all available file descriptors before crashing.\n");
fprintf(stderr, "prefix any of the above with 'wait-' to wait until input is received on stdin\n");
return EXIT_FAILURE;
}
noinline int do_action(const char* arg) {
// Prefixes.
if (!strncmp(arg, "wait-", strlen("wait-"))) {
char buf[1];
TEMP_FAILURE_RETRY(read(STDIN_FILENO, buf, sizeof(buf)));
return do_action(arg + strlen("wait-"));
} else if (!strncmp(arg, "exhaustfd-", strlen("exhaustfd-"))) {
errno = 0;
while (errno != EMFILE) {
open("/dev/null", O_RDONLY);
}
return do_action(arg + strlen("exhaustfd-"));
} else if (!strncmp(arg, "thread-", strlen("thread-"))) {
return do_action_on_thread(arg + strlen("thread-"));
}
// Actions.
if (!strcasecmp(arg, "SIGSEGV-non-null")) {
sigsegv_non_null();
} else if (!strcasecmp(arg, "smash-stack")) {
volatile int len = 128;
return smash_stack(&len);
} else if (!strcasecmp(arg, "stack-overflow")) {
overflow_stack(nullptr);
} else if (!strcasecmp(arg, "nostack")) {
crashnostack();
} else if (!strcasecmp(arg, "exit")) {
exit(1);
} else if (!strcasecmp(arg, "crash") || !strcmp(arg, "SIGSEGV")) {
return crash(42);
} else if (!strcasecmp(arg, "abort")) {
maybe_abort();
} else if (!strcasecmp(arg, "assert")) {
__assert("some_file.c", 123, "false");
} else if (!strcasecmp(arg, "assert2")) {
__assert2("some_file.c", 123, "some_function", "false");
} else if (!strcasecmp(arg, "fortify")) {
char buf[10];
__read_chk(-1, buf, 32, 10);
while (true) pause();
} else if (!strcasecmp(arg, "LOG(FATAL)")) {
LOG(FATAL) << "hello " << 123;
} else if (!strcasecmp(arg, "LOG_ALWAYS_FATAL")) {
LOG_ALWAYS_FATAL("hello %s", "world");
} else if (!strcasecmp(arg, "LOG_ALWAYS_FATAL_IF")) {
LOG_ALWAYS_FATAL_IF(true, "hello %s", "world");
} else if (!strcasecmp(arg, "SIGFPE")) {
raise(SIGFPE);
return EXIT_SUCCESS;
} else if (!strcasecmp(arg, "SIGTRAP")) {
raise(SIGTRAP);
return EXIT_SUCCESS;
} else if (!strcasecmp(arg, "fprintf-NULL")) {
fprintf_null();
} else if (!strcasecmp(arg, "readdir-NULL")) {
readdir_null();
} else if (!strcasecmp(arg, "strlen-NULL")) {
return strlen_null();
} else if (!strcasecmp(arg, "pthread_join-NULL")) {
return pthread_join(0, nullptr);
} else if (!strcasecmp(arg, "heap-usage")) {
abuse_heap();
} else if (!strcasecmp(arg, "SIGSEGV-unmapped")) {
char* map = reinterpret_cast<char*>(mmap(nullptr, sizeof(int), PROT_READ | PROT_WRITE,
MAP_SHARED | MAP_ANONYMOUS, -1, 0));
munmap(map, sizeof(int));
map[0] = '8';
} else if (!strcasecmp(arg, "seccomp")) {
set_seccomp_filter();
syscall(99999);
#if defined(__arm__)
} else if (!strcasecmp(arg, "kuser_helper_version")) {
return __kuser_helper_version;
} else if (!strcasecmp(arg, "kuser_get_tls")) {
return !__kuser_get_tls();
} else if (!strcasecmp(arg, "kuser_cmpxchg")) {
return __kuser_cmpxchg(0, 0, 0);
} else if (!strcasecmp(arg, "kuser_memory_barrier")) {
__kuser_dmb();
} else if (!strcasecmp(arg, "kuser_cmpxchg64")) {
return __kuser_cmpxchg64(0, 0, 0);
#endif
} else if (!strcasecmp(arg, "no_new_privs")) {
if (prctl(PR_SET_NO_NEW_PRIVS, 1) != 0) {
fprintf(stderr, "prctl(PR_SET_NO_NEW_PRIVS, 1) failed: %s\n", strerror(errno));
return EXIT_SUCCESS;
}
abort();
} else {
return usage();
}
fprintf(stderr, "%s: exiting normally!\n", getprogname());
return EXIT_SUCCESS;
}
int main(int argc, char** argv) {
#if defined(STATIC_CRASHER)
debuggerd_callbacks_t callbacks = {
.get_abort_message = []() {
static struct {
size_t size;
char msg[32];
} msg;
msg.size = strlen("dummy abort message");
memcpy(msg.msg, "dummy abort message", strlen("dummy abort message"));
return reinterpret_cast<abort_msg_t*>(&msg);
},
.post_dump = nullptr
};
debuggerd_init(&callbacks);
#endif
if (argc == 1) crash1();
else if (argc == 2) return do_action(argv[1]);
return usage();
}
};
|