summaryrefslogtreecommitdiffstats
blob: 57209aaefeffa4165d375aaadec42a75cc92cfd6 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
/*
 * Copyright 2008, The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *     http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#define LOG_TAG "DEBUG"

#include "utility.h"

#include <errno.h>
#include <signal.h>
#include <string.h>
#include <sys/ptrace.h>
#include <sys/wait.h>
#include <unistd.h>

#include <string>

#include <android-base/stringprintf.h>
#include <backtrace/Backtrace.h>
#include <log/log.h>

// Whitelist output desired in the logcat output.
bool is_allowed_in_logcat(enum logtype ltype) {
  if ((ltype == HEADER)
   || (ltype == REGISTERS)
   || (ltype == BACKTRACE)) {
    return true;
  }
  return false;
}

void _LOG(log_t* log, enum logtype ltype, const char* fmt, ...) {
  bool write_to_tombstone = (log->tfd != -1);
  bool write_to_logcat = is_allowed_in_logcat(ltype)
                      && log->crashed_tid != -1
                      && log->current_tid != -1
                      && (log->crashed_tid == log->current_tid);

  char buf[512];
  va_list ap;
  va_start(ap, fmt);
  vsnprintf(buf, sizeof(buf), fmt, ap);
  va_end(ap);

  size_t len = strlen(buf);
  if (len <= 0) {
    return;
  }

  if (write_to_tombstone) {
    TEMP_FAILURE_RETRY(write(log->tfd, buf, len));
  }

  if (write_to_logcat) {
    __android_log_buf_write(LOG_ID_CRASH, ANDROID_LOG_FATAL, LOG_TAG, buf);
    if (log->amfd_data != nullptr) {
      *log->amfd_data += buf;
    }
  }
}

bool wait_for_signal(pid_t tid, siginfo_t* siginfo) {
  while (true) {
    int status;
    pid_t n = TEMP_FAILURE_RETRY(waitpid(tid, &status, __WALL));
    if (n == -1) {
      ALOGE("waitpid failed: tid %d, %s", tid, strerror(errno));
      return false;
    } else if (n == tid) {
      if (WIFSTOPPED(status)) {
        if (ptrace(PTRACE_GETSIGINFO, tid, nullptr, siginfo) != 0) {
          ALOGE("PTRACE_GETSIGINFO failed: %s", strerror(errno));
          return false;
        }
        return true;
      } else {
        ALOGE("unexpected waitpid response: n=%d, status=%08x\n", n, status);
        // This is the only circumstance under which we can allow a detach
        // to fail with ESRCH, which indicates the tid has exited.
        return false;
      }
    }
  }
}

#define MEMORY_BYTES_TO_DUMP 256
#define MEMORY_BYTES_PER_LINE 16

void dump_memory(log_t* log, Backtrace* backtrace, uintptr_t addr, const char* fmt, ...) {
  std::string log_msg;
  va_list ap;
  va_start(ap, fmt);
  android::base::StringAppendV(&log_msg, fmt, ap);
  va_end(ap);

  // Align the address to sizeof(long) and start 32 bytes before the address.
  addr &= ~(sizeof(long) - 1);
  if (addr >= 4128) {
    addr -= 32;
  }

  // Don't bother if the address looks too low, or looks too high.
  if (addr < 4096 ||
#if defined(__LP64__)
      addr > 0x4000000000000000UL - MEMORY_BYTES_TO_DUMP) {
#else
      addr > 0xffff0000 - MEMORY_BYTES_TO_DUMP) {
#endif
    return;
  }

  _LOG(log, logtype::MEMORY, "\n%s\n", log_msg.c_str());

  // Dump 256 bytes
  uintptr_t data[MEMORY_BYTES_TO_DUMP/sizeof(uintptr_t)];
  memset(data, 0, MEMORY_BYTES_TO_DUMP);
  size_t bytes = backtrace->Read(addr, reinterpret_cast<uint8_t*>(data), sizeof(data));
  if (bytes % sizeof(uintptr_t) != 0) {
    // This should never happen, but just in case.
    ALOGE("Bytes read %zu, is not a multiple of %zu", bytes, sizeof(uintptr_t));
    bytes &= ~(sizeof(uintptr_t) - 1);
  }

  uintptr_t start = 0;
  bool skip_2nd_read = false;
  if (bytes == 0) {
    // In this case, we might want to try another read at the beginning of
    // the next page only if it's within the amount of memory we would have
    // read.
    size_t page_size = sysconf(_SC_PAGE_SIZE);
    start = ((addr + (page_size - 1)) & ~(page_size - 1)) - addr;
    if (start == 0 || start >= MEMORY_BYTES_TO_DUMP) {
      skip_2nd_read = true;
    }
  }

  if (bytes < MEMORY_BYTES_TO_DUMP && !skip_2nd_read) {
    // Try to do one more read. This could happen if a read crosses a map,
    // but the maps do not have any break between them. Or it could happen
    // if reading from an unreadable map, but the read would cross back
    // into a readable map. Only requires one extra read because a map has
    // to contain at least one page, and the total number of bytes to dump
    // is smaller than a page.
    size_t bytes2 = backtrace->Read(addr + start + bytes, reinterpret_cast<uint8_t*>(data) + bytes,
                                    sizeof(data) - bytes - start);
    bytes += bytes2;
    if (bytes2 > 0 && bytes % sizeof(uintptr_t) != 0) {
      // This should never happen, but we'll try and continue any way.
      ALOGE("Bytes after second read %zu, is not a multiple of %zu", bytes, sizeof(uintptr_t));
      bytes &= ~(sizeof(uintptr_t) - 1);
    }
  }

  // Dump the code around memory as:
  //  addr             contents                           ascii
  //  0000000000008d34 ef000000e8bd0090 e1b00000512fff1e  ............../Q
  //  0000000000008d44 ea00b1f9e92d0090 e3a070fcef000000  ......-..p......
  // On 32-bit machines, there are still 16 bytes per line but addresses and
  // words are of course presented differently.
  uintptr_t* data_ptr = data;
  size_t current = 0;
  size_t total_bytes = start + bytes;
  for (size_t line = 0; line < MEMORY_BYTES_TO_DUMP / MEMORY_BYTES_PER_LINE; line++) {
    std::string logline;
    android::base::StringAppendF(&logline, "    %" PRIPTR, addr);

    addr += MEMORY_BYTES_PER_LINE;
    std::string ascii;
    for (size_t i = 0; i < MEMORY_BYTES_PER_LINE / sizeof(uintptr_t); i++) {
      if (current >= start && current + sizeof(uintptr_t) <= total_bytes) {
        android::base::StringAppendF(&logline, " %" PRIPTR, *data_ptr);

        // Fill out the ascii string from the data.
        uint8_t* ptr = reinterpret_cast<uint8_t*>(data_ptr);
        for (size_t val = 0; val < sizeof(uintptr_t); val++, ptr++) {
          if (*ptr >= 0x20 && *ptr < 0x7f) {
            ascii += *ptr;
          } else {
            ascii += '.';
          }
        }
        data_ptr++;
      } else {
        logline += ' ' + std::string(sizeof(uintptr_t) * 2, '-');
        ascii += std::string(sizeof(uintptr_t), '.');
      }
      current += sizeof(uintptr_t);
    }
    _LOG(log, logtype::MEMORY, "%s  %s\n", logline.c_str(), ascii.c_str());
  }
}