1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
|
/*
* Copyright (C) 2018 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include <fcntl.h>
#include <stdint.h>
#include <stdio.h>
#include <sys/ioctl.h>
#include <sys/types.h>
#include <time.h>
#include <unistd.h>
#include <chrono>
#include <ctime>
#include <map>
#include <thread>
#include <android-base/file.h>
#include <android-base/unique_fd.h>
#include <gtest/gtest.h>
#include <libdm/dm.h>
#include <libdm/loop_control.h>
#include "test_util.h"
using namespace std;
using namespace android::dm;
using unique_fd = android::base::unique_fd;
TEST(libdm, HasMinimumTargets) {
DeviceMapper& dm = DeviceMapper::Instance();
vector<DmTargetTypeInfo> targets;
ASSERT_TRUE(dm.GetAvailableTargets(&targets));
map<string, DmTargetTypeInfo> by_name;
for (const auto& target : targets) {
by_name[target.name()] = target;
}
auto iter = by_name.find("linear");
EXPECT_NE(iter, by_name.end());
}
// Helper to ensure that device mapper devices are released.
class TempDevice {
public:
TempDevice(const std::string& name, const DmTable& table)
: dm_(DeviceMapper::Instance()), name_(name), valid_(false) {
valid_ = dm_.CreateDevice(name, table);
}
TempDevice(TempDevice&& other) : dm_(other.dm_), name_(other.name_), valid_(other.valid_) {
other.valid_ = false;
}
~TempDevice() {
if (valid_) {
dm_.DeleteDevice(name_);
}
}
bool Destroy() {
if (!valid_) {
return false;
}
valid_ = false;
return dm_.DeleteDevice(name_);
}
bool WaitForUdev() const {
auto start_time = std::chrono::steady_clock::now();
while (true) {
if (!access(path().c_str(), F_OK)) {
return true;
}
if (errno != ENOENT) {
return false;
}
std::this_thread::sleep_for(50ms);
std::chrono::duration elapsed = std::chrono::steady_clock::now() - start_time;
if (elapsed >= 5s) {
return false;
}
}
}
std::string path() const {
std::string device_path;
if (!dm_.GetDmDevicePathByName(name_, &device_path)) {
return "";
}
return device_path;
}
const std::string& name() const { return name_; }
bool valid() const { return valid_; }
TempDevice(const TempDevice&) = delete;
TempDevice& operator=(const TempDevice&) = delete;
TempDevice& operator=(TempDevice&& other) {
name_ = other.name_;
valid_ = other.valid_;
other.valid_ = false;
return *this;
}
private:
DeviceMapper& dm_;
std::string name_;
bool valid_;
};
TEST(libdm, DmLinear) {
unique_fd tmp1(CreateTempFile("file_1", 4096));
ASSERT_GE(tmp1, 0);
unique_fd tmp2(CreateTempFile("file_2", 4096));
ASSERT_GE(tmp2, 0);
// Create two different files. These will back two separate loop devices.
const char message1[] = "Hello! This is sector 1.";
const char message2[] = "Goodbye. This is sector 2.";
ASSERT_TRUE(android::base::WriteFully(tmp1, message1, sizeof(message1)));
ASSERT_TRUE(android::base::WriteFully(tmp2, message2, sizeof(message2)));
LoopDevice loop_a(tmp1);
ASSERT_TRUE(loop_a.valid());
LoopDevice loop_b(tmp2);
ASSERT_TRUE(loop_b.valid());
// Define a 2-sector device, with each sector mapping to the first sector
// of one of our loop devices.
DmTable table;
ASSERT_TRUE(table.AddTarget(make_unique<DmTargetLinear>(0, 1, loop_a.device(), 0)));
ASSERT_TRUE(table.AddTarget(make_unique<DmTargetLinear>(1, 1, loop_b.device(), 0)));
ASSERT_TRUE(table.valid());
TempDevice dev("libdm-test-dm-linear", table);
ASSERT_TRUE(dev.valid());
ASSERT_FALSE(dev.path().empty());
ASSERT_TRUE(dev.WaitForUdev());
// Note: a scope is needed to ensure that there are no open descriptors
// when we go to close the device.
{
unique_fd dev_fd(open(dev.path().c_str(), O_RDWR));
ASSERT_GE(dev_fd, 0);
// Test that each sector of our device is correctly mapped to each loop
// device.
char sector[512];
ASSERT_TRUE(android::base::ReadFully(dev_fd, sector, sizeof(sector)));
ASSERT_EQ(strncmp(sector, message1, sizeof(message1)), 0);
ASSERT_TRUE(android::base::ReadFully(dev_fd, sector, sizeof(sector)));
ASSERT_EQ(strncmp(sector, message2, sizeof(message2)), 0);
}
// Normally the TestDevice destructor would delete this, but at least one
// test should ensure that device deletion works.
ASSERT_TRUE(dev.Destroy());
}
|