1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
|
//
// Copyright (C) 2018 The Android Open Source Project
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
// http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
//
#ifndef LIBLP_METADATA_BUILDER_H
#define LIBLP_METADATA_BUILDER_H
#include <stddef.h>
#include <stdint.h>
#include <map>
#include <memory>
#include "metadata_format.h"
namespace android {
namespace fs_mgr {
class LinearExtent;
// Abstraction around dm-targets that can be encoded into logical partition tables.
class Extent {
public:
explicit Extent(uint64_t num_sectors) : num_sectors_(num_sectors) {}
virtual ~Extent() {}
virtual void AddTo(LpMetadata* out) const = 0;
virtual LinearExtent* AsLinearExtent() { return nullptr; }
uint64_t num_sectors() const { return num_sectors_; }
void set_num_sectors(uint64_t num_sectors) { num_sectors_ = num_sectors; }
protected:
uint64_t num_sectors_;
};
// This corresponds to a dm-linear target.
class LinearExtent final : public Extent {
public:
LinearExtent(uint64_t num_sectors, uint64_t physical_sector)
: Extent(num_sectors), physical_sector_(physical_sector) {}
void AddTo(LpMetadata* metadata) const override;
LinearExtent* AsLinearExtent() override { return this; }
uint64_t physical_sector() const { return physical_sector_; }
private:
uint64_t physical_sector_;
};
// This corresponds to a dm-zero target.
class ZeroExtent final : public Extent {
public:
explicit ZeroExtent(uint64_t num_sectors) : Extent(num_sectors) {}
void AddTo(LpMetadata* out) const override;
};
class Partition final {
public:
Partition(const std::string& name, const std::string& guid, uint32_t attributes);
// Add a raw extent.
void AddExtent(std::unique_ptr<Extent>&& extent);
// Remove all extents from this partition.
void RemoveExtents();
// Remove and/or shrink extents until the partition is the requested size.
// See MetadataBuilder::ShrinkPartition for more information.
void ShrinkTo(uint64_t requested_size);
const std::string& name() const { return name_; }
uint32_t attributes() const { return attributes_; }
const std::string& guid() const { return guid_; }
const std::vector<std::unique_ptr<Extent>>& extents() const { return extents_; }
uint64_t size() const { return size_; }
private:
std::string name_;
std::string guid_;
std::vector<std::unique_ptr<Extent>> extents_;
uint32_t attributes_;
uint64_t size_;
};
class MetadataBuilder {
public:
// Construct an empty logical partition table builder. The block device size
// and maximum metadata size must be specified, as this will determine which
// areas of the physical partition can be flashed for metadata vs for logical
// partitions.
//
// If the parameters would yield invalid metadata, nullptr is returned. This
// could happen if the block device size is too small to store the metadata
// and backup copies.
static std::unique_ptr<MetadataBuilder> New(uint64_t blockdevice_size,
uint32_t metadata_max_size,
uint32_t metadata_slot_count);
// Import an existing table for modification. If the table is not valid, for
// example it contains duplicate partition names, then nullptr is returned.
static std::unique_ptr<MetadataBuilder> New(const LpMetadata& metadata);
// Export metadata so it can be serialized to an image, to disk, or mounted
// via device-mapper.
std::unique_ptr<LpMetadata> Export();
// Add a partition, returning a handle so it can be sized as needed. If a
// partition with the given name already exists, nullptr is returned.
Partition* AddPartition(const std::string& name, const std::string& guid, uint32_t attributes);
// Delete a partition by name if it exists.
void RemovePartition(const std::string& name);
// Find a partition by name. If no partition is found, nullptr is returned.
Partition* FindPartition(const std::string& name);
// Grow a partition to the requested size. If the partition's size is already
// greater or equal to the requested size, this will return true and the
// partition table will not be changed. Otherwise, a greedy algorithm is
// used to find free gaps in the partition table and allocate them for this
// partition. If not enough space can be allocated, false is returned, and
// the parition table will not be modified.
//
// The size will be rounded UP to the nearest sector.
//
// Note, this is an in-memory operation, and it does not alter the
// underlying filesystem or contents of the partition on disk.
bool GrowPartition(Partition* partition, uint64_t requested_size);
// Shrink a partition to the requested size. If the partition is already
// smaller than the given size, this will return and the partition table
// will not be changed. Otherwise, extents will be removed and/or shrunk
// from the end of the partition until it is the requested size.
//
// The size will be rounded UP to the nearest sector.
//
// Note, this is an in-memory operation, and it does not alter the
// underlying filesystem or contents of the partition on disk.
void ShrinkPartition(Partition* partition, uint64_t requested_size);
// Amount of space that can be allocated to logical partitions.
uint64_t AllocatableSpace() const;
private:
MetadataBuilder();
bool Init(uint64_t blockdevice_size, uint32_t metadata_max_size, uint32_t metadata_slot_count);
bool Init(const LpMetadata& metadata);
LpMetadataGeometry geometry_;
LpMetadataHeader header_;
std::vector<std::unique_ptr<Partition>> partitions_;
};
} // namespace fs_mgr
} // namespace android
#endif /* LIBLP_METADATA_BUILDER_H */
|