summaryrefslogtreecommitdiffstats
blob: 0f96e3a605a553b0f9e175c18526e2b84759f1ba (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
//
// Copyright (C) 2018 The Android Open Source Project
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
//      http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
//

#ifndef LIBLP_METADATA_BUILDER_H
#define LIBLP_METADATA_BUILDER_H

#include <stddef.h>
#include <stdint.h>

#include <map>
#include <memory>

#include "liblp.h"

namespace android {
namespace fs_mgr {

class LinearExtent;

// By default, partitions are aligned on a 1MiB boundary.
static const uint32_t kDefaultPartitionAlignment = 1024 * 1024;

struct BlockDeviceInfo {
    BlockDeviceInfo() : size(0), alignment(0), alignment_offset(0) {}
    BlockDeviceInfo(uint64_t size, uint32_t alignment, uint32_t alignment_offset)
        : size(size), alignment(alignment), alignment_offset(alignment_offset) {}
    // Size of the block device, in bytes.
    uint64_t size;
    // Optimal target alignment, in bytes. Partition extents will be aligned to
    // this value by default. This value must be 0 or a multiple of 512.
    uint32_t alignment;
    // Alignment offset to parent device (if any), in bytes. The sector at
    // |alignment_offset| on the target device is correctly aligned on its
    // parent device. This value must be 0 or a multiple of 512.
    uint32_t alignment_offset;
};

// Abstraction around dm-targets that can be encoded into logical partition tables.
class Extent {
  public:
    explicit Extent(uint64_t num_sectors) : num_sectors_(num_sectors) {}
    virtual ~Extent() {}

    virtual void AddTo(LpMetadata* out) const = 0;
    virtual LinearExtent* AsLinearExtent() { return nullptr; }

    uint64_t num_sectors() const { return num_sectors_; }
    void set_num_sectors(uint64_t num_sectors) { num_sectors_ = num_sectors; }

  protected:
    uint64_t num_sectors_;
};

// This corresponds to a dm-linear target.
class LinearExtent final : public Extent {
  public:
    LinearExtent(uint64_t num_sectors, uint64_t physical_sector)
        : Extent(num_sectors), physical_sector_(physical_sector) {}

    void AddTo(LpMetadata* metadata) const override;
    LinearExtent* AsLinearExtent() override { return this; }

    uint64_t physical_sector() const { return physical_sector_; }

  private:
    uint64_t physical_sector_;
};

// This corresponds to a dm-zero target.
class ZeroExtent final : public Extent {
  public:
    explicit ZeroExtent(uint64_t num_sectors) : Extent(num_sectors) {}

    void AddTo(LpMetadata* out) const override;
};

class Partition final {
  public:
    Partition(const std::string& name, const std::string& guid, uint32_t attributes);

    // Add a raw extent.
    void AddExtent(std::unique_ptr<Extent>&& extent);

    // Remove all extents from this partition.
    void RemoveExtents();

    // Remove and/or shrink extents until the partition is the requested size.
    // See MetadataBuilder::ShrinkPartition for more information.
    void ShrinkTo(uint64_t requested_size);

    const std::string& name() const { return name_; }
    uint32_t attributes() const { return attributes_; }
    const std::string& guid() const { return guid_; }
    const std::vector<std::unique_ptr<Extent>>& extents() const { return extents_; }
    uint64_t size() const { return size_; }

  private:
    std::string name_;
    std::string guid_;
    std::vector<std::unique_ptr<Extent>> extents_;
    uint32_t attributes_;
    uint64_t size_;
};

class MetadataBuilder {
  public:
    // Construct an empty logical partition table builder. The block device size
    // and maximum metadata size must be specified, as this will determine which
    // areas of the physical partition can be flashed for metadata vs for logical
    // partitions.
    //
    // If the parameters would yield invalid metadata, nullptr is returned. This
    // could happen if the block device size is too small to store the metadata
    // and backup copies.
    static std::unique_ptr<MetadataBuilder> New(const BlockDeviceInfo& device_info,
                                                uint32_t metadata_max_size,
                                                uint32_t metadata_slot_count);

    // Import an existing table for modification. This reads metadata off the
    // given block device and imports it. It also adjusts alignment information
    // based on run-time values in the operating system.
    static std::unique_ptr<MetadataBuilder> New(const std::string& block_device,
                                                uint32_t slot_number);

    // Import an existing table for modification. If the table is not valid, for
    // example it contains duplicate partition names, then nullptr is returned.
    // This method is for testing or changing off-line tables.
    static std::unique_ptr<MetadataBuilder> New(const LpMetadata& metadata);

    // Wrapper around New() with a BlockDeviceInfo that only specifies a device
    // size. This is a convenience method for tests.
    static std::unique_ptr<MetadataBuilder> New(uint64_t blockdev_size, uint32_t metadata_max_size,
                                                uint32_t metadata_slot_count) {
        BlockDeviceInfo device_info(blockdev_size, 0, 0);
        return New(device_info, metadata_max_size, metadata_slot_count);
    }

    // Export metadata so it can be serialized to an image, to disk, or mounted
    // via device-mapper.
    std::unique_ptr<LpMetadata> Export();

    // Add a partition, returning a handle so it can be sized as needed. If a
    // partition with the given name already exists, nullptr is returned.
    Partition* AddPartition(const std::string& name, const std::string& guid, uint32_t attributes);

    // Delete a partition by name if it exists.
    void RemovePartition(const std::string& name);

    // Find a partition by name. If no partition is found, nullptr is returned.
    Partition* FindPartition(const std::string& name);

    // Grow or shrink a partition to the requested size. This size will be
    // rounded UP to the nearest block (512 bytes).
    //
    // When growing a partition, a greedy algorithm is used to find free gaps
    // in the partition table and allocate them. If not enough space can be
    // allocated, false is returned, and the parition table will not be
    // modified.
    //
    // Note, this is an in-memory operation, and it does not alter the
    // underlying filesystem or contents of the partition on disk.
    bool ResizePartition(Partition* partition, uint64_t requested_size);

    // Amount of space that can be allocated to logical partitions.
    uint64_t AllocatableSpace() const;

    // Merge new block device information into previous values. Alignment values
    // are only overwritten if the new values are non-zero.
    void set_block_device_info(const BlockDeviceInfo& device_info);
    const BlockDeviceInfo& block_device_info() const { return device_info_; }

  private:
    MetadataBuilder();
    bool Init(const BlockDeviceInfo& info, uint32_t metadata_max_size, uint32_t metadata_slot_count);
    bool Init(const LpMetadata& metadata);
    bool GrowPartition(Partition* partition, uint64_t aligned_size);
    void ShrinkPartition(Partition* partition, uint64_t aligned_size);
    uint64_t AlignSector(uint64_t sector);

    LpMetadataGeometry geometry_;
    LpMetadataHeader header_;
    std::vector<std::unique_ptr<Partition>> partitions_;
    BlockDeviceInfo device_info_;
};

// Read BlockDeviceInfo for a given block device. This always returns false
// for non-Linux operating systems.
bool GetBlockDeviceInfo(const std::string& block_device, BlockDeviceInfo* device_info);

}  // namespace fs_mgr
}  // namespace android

#endif /* LIBLP_METADATA_BUILDER_H */