1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
|
/*
* Copyright (C) 2007 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef ANDROID_CUTILS_ATOMIC_H
#define ANDROID_CUTILS_ATOMIC_H
#include <stdint.h>
#include <sys/types.h>
#include <stdatomic.h>
#ifndef ANDROID_ATOMIC_INLINE
#define ANDROID_ATOMIC_INLINE static inline
#endif
/*
* A handful of basic atomic operations.
* THESE ARE HERE FOR LEGACY REASONS ONLY. AVOID.
*
* PREFERRED ALTERNATIVES:
* - Use C++/C/pthread locks/mutexes whenever there is not a
* convincing reason to do otherwise. Note that very clever and
* complicated, but correct, lock-free code is often slower than
* using locks, especially where nontrivial data structures
* are involved.
* - C11 stdatomic.h.
* - Where supported, C++11 std::atomic<T> .
*
* PLEASE STOP READING HERE UNLESS YOU ARE TRYING TO UNDERSTAND
* OR UPDATE OLD CODE.
*
* The "acquire" and "release" terms can be defined intuitively in terms
* of the placement of memory barriers in a simple lock implementation:
* - wait until compare-and-swap(lock-is-free --> lock-is-held) succeeds
* - barrier
* - [do work]
* - barrier
* - store(lock-is-free)
* In very crude terms, the initial (acquire) barrier prevents any of the
* "work" from happening before the lock is held, and the later (release)
* barrier ensures that all of the work happens before the lock is released.
* (Think of cached writes, cache read-ahead, and instruction reordering
* around the CAS and store instructions.)
*
* The barriers must apply to both the compiler and the CPU. Note it is
* legal for instructions that occur before an "acquire" barrier to be
* moved down below it, and for instructions that occur after a "release"
* barrier to be moved up above it.
*
* The ARM-driven implementation we use here is short on subtlety,
* and actually requests a full barrier from the compiler and the CPU.
* The only difference between acquire and release is in whether they
* are issued before or after the atomic operation with which they
* are associated. To ease the transition to C/C++ atomic intrinsics,
* you should not rely on this, and instead assume that only the minimal
* acquire/release protection is provided.
*
* NOTE: all int32_t* values are expected to be aligned on 32-bit boundaries.
* If they are not, atomicity is not guaranteed.
*/
ANDROID_ATOMIC_INLINE
volatile atomic_int_least32_t* to_atomic_int_least32_t(volatile const int32_t* addr) {
#ifdef __cplusplus
return reinterpret_cast<volatile atomic_int_least32_t*>(const_cast<volatile int32_t*>(addr));
#else
return (volatile atomic_int_least32_t*)addr;
#endif
}
/*
* Basic arithmetic and bitwise operations. These all provide a
* barrier with "release" ordering, and return the previous value.
*
* These have the same characteristics (e.g. what happens on overflow)
* as the equivalent non-atomic C operations.
*/
ANDROID_ATOMIC_INLINE
int32_t android_atomic_inc(volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
/* Int32_t, if it exists, is the same as int_least32_t. */
return atomic_fetch_add_explicit(a, 1, memory_order_release);
}
ANDROID_ATOMIC_INLINE
int32_t android_atomic_dec(volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return atomic_fetch_sub_explicit(a, 1, memory_order_release);
}
ANDROID_ATOMIC_INLINE
int32_t android_atomic_add(int32_t value, volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return atomic_fetch_add_explicit(a, value, memory_order_release);
}
ANDROID_ATOMIC_INLINE
int32_t android_atomic_and(int32_t value, volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return atomic_fetch_and_explicit(a, value, memory_order_release);
}
ANDROID_ATOMIC_INLINE
int32_t android_atomic_or(int32_t value, volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return atomic_fetch_or_explicit(a, value, memory_order_release);
}
/*
* Perform an atomic load with "acquire" or "release" ordering.
*
* Note that the notion of a "release" ordering for a load does not
* really fit into the C11 or C++11 memory model. The extra ordering
* is normally observable only by code using memory_order_relaxed
* atomics, or data races. In the rare cases in which such ordering
* is called for, use memory_order_relaxed atomics and a leading
* atomic_thread_fence (typically with memory_order_acquire,
* not memory_order_release!) instead. If you do not understand
* this comment, you are in the vast majority, and should not be
* using release loads or replacing them with anything other than
* locks or default sequentially consistent atomics.
*/
ANDROID_ATOMIC_INLINE
int32_t android_atomic_acquire_load(volatile const int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return atomic_load_explicit(a, memory_order_acquire);
}
ANDROID_ATOMIC_INLINE
int32_t android_atomic_release_load(volatile const int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
atomic_thread_fence(memory_order_seq_cst);
/* Any reasonable clients of this interface would probably prefer */
/* something weaker. But some remaining clients seem to be */
/* abusing this API in strange ways, e.g. by using it as a fence. */
/* Thus we are conservative until we can get rid of remaining */
/* clients (and this function). */
return atomic_load_explicit(a, memory_order_relaxed);
}
/*
* Perform an atomic store with "acquire" or "release" ordering.
*
* Note that the notion of an "acquire" ordering for a store does not
* really fit into the C11 or C++11 memory model. The extra ordering
* is normally observable only by code using memory_order_relaxed
* atomics, or data races. In the rare cases in which such ordering
* is called for, use memory_order_relaxed atomics and a trailing
* atomic_thread_fence (typically with memory_order_release,
* not memory_order_acquire!) instead.
*/
ANDROID_ATOMIC_INLINE
void android_atomic_acquire_store(int32_t value, volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
atomic_store_explicit(a, value, memory_order_relaxed);
atomic_thread_fence(memory_order_seq_cst);
/* Again overly conservative to accomodate weird clients. */
}
ANDROID_ATOMIC_INLINE
void android_atomic_release_store(int32_t value, volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
atomic_store_explicit(a, value, memory_order_release);
}
/*
* Compare-and-set operation with "acquire" or "release" ordering.
*
* This returns zero if the new value was successfully stored, which will
* only happen when *addr == oldvalue.
*
* (The return value is inverted from implementations on other platforms,
* but matches the ARM ldrex/strex result.)
*
* Implementations that use the release CAS in a loop may be less efficient
* than possible, because we re-issue the memory barrier on each iteration.
*/
ANDROID_ATOMIC_INLINE
int android_atomic_acquire_cas(int32_t oldvalue, int32_t newvalue,
volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return !atomic_compare_exchange_strong_explicit(
a, &oldvalue, newvalue,
memory_order_acquire,
memory_order_acquire);
}
ANDROID_ATOMIC_INLINE
int android_atomic_release_cas(int32_t oldvalue, int32_t newvalue,
volatile int32_t* addr)
{
volatile atomic_int_least32_t* a = to_atomic_int_least32_t(addr);
return !atomic_compare_exchange_strong_explicit(
a, &oldvalue, newvalue,
memory_order_release,
memory_order_relaxed);
}
/*
* Fence primitives.
*/
ANDROID_ATOMIC_INLINE
void android_compiler_barrier(void)
{
__asm__ __volatile__ ("" : : : "memory");
/* Could probably also be: */
/* atomic_signal_fence(memory_order_seq_cst); */
}
ANDROID_ATOMIC_INLINE
void android_memory_barrier(void)
{
atomic_thread_fence(memory_order_seq_cst);
}
/*
* Aliases for code using an older version of this header. These are now
* deprecated and should not be used. The definitions will be removed
* in a future release.
*/
#define android_atomic_write android_atomic_release_store
#define android_atomic_cmpxchg android_atomic_release_cas
#endif // ANDROID_CUTILS_ATOMIC_H
|