summaryrefslogtreecommitdiffstats
blob: a0dd1e0340ed72c7f203e529420902928abd74bb (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
/*
 * Copyright (C) 2012 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LIBS_CUTILS_TRACE_H
#define _LIBS_CUTILS_TRACE_H

#include <sys/cdefs.h>
#include <sys/types.h>
#include <stdint.h>
#include <stdbool.h>
#include <unistd.h>
#include <cutils/compiler.h>

#ifdef ANDROID_SMP
#include <cutils/atomic-inline.h>
#else
#include <cutils/atomic.h>
#endif

__BEGIN_DECLS

/**
 * The ATRACE_TAG macro can be defined before including this header to trace
 * using one of the tags defined below.  It must be defined to one of the
 * following ATRACE_TAG_* macros.  The trace tag is used to filter tracing in
 * userland to avoid some of the runtime cost of tracing when it is not desired.
 *
 * Defining ATRACE_TAG to be ATRACE_TAG_ALWAYS will result in the tracing always
 * being enabled - this should ONLY be done for debug code, as userland tracing
 * has a performance cost even when the trace is not being recorded.  Defining
 * ATRACE_TAG to be ATRACE_TAG_NEVER or leaving ATRACE_TAG undefined will result
 * in the tracing always being disabled.
 *
 * ATRACE_TAG_HAL should be bitwise ORed with the relevant tags for tracing
 * within a hardware module.  For example a camera hardware module would set:
 * #define ATRACE_TAG  (ATRACE_TAG_CAMERA | ATRACE_TAG_HAL)
 *
 * Keep these in sync with frameworks/base/core/java/android/os/Trace.java.
 */
#define ATRACE_TAG_NEVER            0       // This tag is never enabled.
#define ATRACE_TAG_ALWAYS           (1<<0)  // This tag is always enabled.
#define ATRACE_TAG_GRAPHICS         (1<<1)
#define ATRACE_TAG_INPUT            (1<<2)
#define ATRACE_TAG_VIEW             (1<<3)
#define ATRACE_TAG_WEBVIEW          (1<<4)
#define ATRACE_TAG_WINDOW_MANAGER   (1<<5)
#define ATRACE_TAG_ACTIVITY_MANAGER (1<<6)
#define ATRACE_TAG_SYNC_MANAGER     (1<<7)
#define ATRACE_TAG_AUDIO            (1<<8)
#define ATRACE_TAG_VIDEO            (1<<9)
#define ATRACE_TAG_CAMERA           (1<<10)
#define ATRACE_TAG_HAL              (1<<11)
#define ATRACE_TAG_APP              (1<<12)
#define ATRACE_TAG_RESOURCES        (1<<13)
#define ATRACE_TAG_DALVIK           (1<<14)
#define ATRACE_TAG_RS               (1<<15)
#define ATRACE_TAG_LAST             ATRACE_TAG_RS

// Reserved for initialization.
#define ATRACE_TAG_NOT_READY        (1LL<<63)

#define ATRACE_TAG_VALID_MASK ((ATRACE_TAG_LAST - 1) | ATRACE_TAG_LAST)

#ifndef ATRACE_TAG
#define ATRACE_TAG ATRACE_TAG_NEVER
#elif ATRACE_TAG > ATRACE_TAG_VALID_MASK
#error ATRACE_TAG must be defined to be one of the tags defined in cutils/trace.h
#endif

#ifdef HAVE_ANDROID_OS
/**
 * Maximum size of a message that can be logged to the trace buffer.
 * Note this message includes a tag, the pid, and the string given as the name.
 * Names should be kept short to get the most use of the trace buffer.
 */
#define ATRACE_MESSAGE_LENGTH 1024

/**
 * Opens the trace file for writing and reads the property for initial tags.
 * The atrace.tags.enableflags property sets the tags to trace.
 * This function should not be explicitly called, the first call to any normal
 * trace function will cause it to be run safely.
 */
void atrace_setup();

/**
 * If tracing is ready, set atrace_enabled_tags to the system property
 * debug.atrace.tags.enableflags. Can be used as a sysprop change callback.
 */
void atrace_update_tags();

/**
 * Set whether the process is debuggable.  By default the process is not
 * considered debuggable.  If the process is not debuggable then application-
 * level tracing is not allowed unless the ro.debuggable system property is
 * set to '1'.
 */
void atrace_set_debuggable(bool debuggable);

/**
 * Set whether tracing is enabled for the current process.  This is used to
 * prevent tracing within the Zygote process.
 */
void atrace_set_tracing_enabled(bool enabled);

/**
 * Flag indicating whether setup has been completed, initialized to 0.
 * Nonzero indicates setup has completed.
 * Note: This does NOT indicate whether or not setup was successful.
 */
extern volatile int32_t atrace_is_ready;

/**
 * Set of ATRACE_TAG flags to trace for, initialized to ATRACE_TAG_NOT_READY.
 * A value of zero indicates setup has failed.
 * Any other nonzero value indicates setup has succeeded, and tracing is on.
 */
extern uint64_t atrace_enabled_tags;

/**
 * Handle to the kernel's trace buffer, initialized to -1.
 * Any other value indicates setup has succeeded, and is a valid fd for tracing.
 */
extern int atrace_marker_fd;

/**
 * atrace_init readies the process for tracing by opening the trace_marker file.
 * Calling any trace function causes this to be run, so calling it is optional.
 * This can be explicitly run to avoid setup delay on first trace function.
 */
#define ATRACE_INIT() atrace_init()
static inline void atrace_init()
{
    if (CC_UNLIKELY(!android_atomic_acquire_load(&atrace_is_ready))) {
        atrace_setup();
    }
}

/**
 * Get the mask of all tags currently enabled.
 * It can be used as a guard condition around more expensive trace calculations.
 * Every trace function calls this, which ensures atrace_init is run.
 */
#define ATRACE_GET_ENABLED_TAGS() atrace_get_enabled_tags()
static inline uint64_t atrace_get_enabled_tags()
{
    atrace_init();
    return atrace_enabled_tags;
}

/**
 * Test if a given tag is currently enabled.
 * Returns nonzero if the tag is enabled, otherwise zero.
 * It can be used as a guard condition around more expensive trace calculations.
 */
#define ATRACE_ENABLED() atrace_is_tag_enabled(ATRACE_TAG)
static inline uint64_t atrace_is_tag_enabled(uint64_t tag)
{
    return atrace_get_enabled_tags() & tag;
}

/**
 * Trace the beginning of a context.  name is used to identify the context.
 * This is often used to time function execution.
 */
#define ATRACE_BEGIN(name) atrace_begin(ATRACE_TAG, name)
static inline void atrace_begin(uint64_t tag, const char* name)
{
    if (CC_UNLIKELY(atrace_is_tag_enabled(tag))) {
        char buf[ATRACE_MESSAGE_LENGTH];
        size_t len;

        len = snprintf(buf, ATRACE_MESSAGE_LENGTH, "B|%d|%s", getpid(), name);
        write(atrace_marker_fd, buf, len);
    }
}

/**
 * Trace the end of a context.
 * This should match up (and occur after) a corresponding ATRACE_BEGIN.
 */
#define ATRACE_END() atrace_end(ATRACE_TAG)
static inline void atrace_end(uint64_t tag)
{
    if (CC_UNLIKELY(atrace_is_tag_enabled(tag))) {
        char c = 'E';
        write(atrace_marker_fd, &c, 1);
    }
}

/**
 * Trace the beginning of an asynchronous event. Unlike ATRACE_BEGIN/ATRACE_END
 * contexts, asynchronous events do not need to be nested. The name describes
 * the event, and the cookie provides a unique identifier for distinguishing
 * simultaneous events. The name and cookie used to begin an event must be
 * used to end it.
 */
#define ATRACE_ASYNC_BEGIN(name, cookie) \
    atrace_async_begin(ATRACE_TAG, name, cookie)
static inline void atrace_async_begin(uint64_t tag, const char* name,
        int32_t cookie)
{
    if (CC_UNLIKELY(atrace_is_tag_enabled(tag))) {
        char buf[ATRACE_MESSAGE_LENGTH];
        size_t len;

        len = snprintf(buf, ATRACE_MESSAGE_LENGTH, "S|%d|%s|%d", getpid(),
                name, cookie);
        write(atrace_marker_fd, buf, len);
    }
}

/**
 * Trace the end of an asynchronous event.
 * This should have a corresponding ATRACE_ASYNC_BEGIN.
 */
#define ATRACE_ASYNC_END(name, cookie) atrace_async_end(ATRACE_TAG, name, cookie)
static inline void atrace_async_end(uint64_t tag, const char* name,
        int32_t cookie)
{
    if (CC_UNLIKELY(atrace_is_tag_enabled(tag))) {
        char buf[ATRACE_MESSAGE_LENGTH];
        size_t len;

        len = snprintf(buf, ATRACE_MESSAGE_LENGTH, "F|%d|%s|%d", getpid(),
                name, cookie);
        write(atrace_marker_fd, buf, len);
    }
}


/**
 * Traces an integer counter value.  name is used to identify the counter.
 * This can be used to track how a value changes over time.
 */
#define ATRACE_INT(name, value) atrace_int(ATRACE_TAG, name, value)
static inline void atrace_int(uint64_t tag, const char* name, int32_t value)
{
    if (CC_UNLIKELY(atrace_is_tag_enabled(tag))) {
        char buf[ATRACE_MESSAGE_LENGTH];
        size_t len;

        len = snprintf(buf, ATRACE_MESSAGE_LENGTH, "C|%d|%s|%d",
                getpid(), name, value);
        write(atrace_marker_fd, buf, len);
    }
}

#else // not HAVE_ANDROID_OS

#define ATRACE_INIT()
#define ATRACE_GET_ENABLED_TAGS()
#define ATRACE_ENABLED() 0
#define ATRACE_BEGIN(name)
#define ATRACE_END()
#define ATRACE_ASYNC_BEGIN(name, cookie)
#define ATRACE_ASYNC_END(name, cookie)
#define ATRACE_INT(name, value)

#endif // not HAVE_ANDROID_OS

__END_DECLS

#endif // _LIBS_CUTILS_TRACE_H